<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックIs it mandatory to match RTD version between M7_0 Bootloader and M7_0 App?</title>
    <link>https://community.nxp.com/t5/S32G/Is-it-mandatory-to-match-RTD-version-between-M7-0-Bootloader-and/m-p/1958504#M10848</link>
    <description>&lt;P&gt;I am preparing a S32G274A bootloader customization, which operates only the M7_0 core. I mainly referenced two documents 'AN13750' and 'S32G_Bootloader_V2-2022.1024_eng.pdf'&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'd like to customize the bootloader to load the prepared M7_0 App(AUTOSAR SWP) with example work(AN13750 - Integration_Reference_Examples_S32G2_2022_06).&lt;/P&gt;&lt;P&gt;However, I have one doubt regarding RTD.&lt;/P&gt;&lt;P&gt;- In AN13750, Bootloader was made based on 'RTD_4.4_3.0.2'&lt;/P&gt;&lt;P&gt;- The prepared M7_0 App image's RTD version is 'ex. RTD_4.4_4.0.2_P04'&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Q1. Are bootloaders and apps with different RTD version compatible?&lt;/P&gt;&lt;P&gt;Q2. If not, is there a way to change the example bootloader's RTD version to specific RTD version?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Dominic.&lt;/P&gt;</description>
    <pubDate>Fri, 20 Sep 2024 07:37:50 GMT</pubDate>
    <dc:creator>Dominic88</dc:creator>
    <dc:date>2024-09-20T07:37:50Z</dc:date>
    <item>
      <title>Is it mandatory to match RTD version between M7_0 Bootloader and M7_0 App?</title>
      <link>https://community.nxp.com/t5/S32G/Is-it-mandatory-to-match-RTD-version-between-M7-0-Bootloader-and/m-p/1958504#M10848</link>
      <description>&lt;P&gt;I am preparing a S32G274A bootloader customization, which operates only the M7_0 core. I mainly referenced two documents 'AN13750' and 'S32G_Bootloader_V2-2022.1024_eng.pdf'&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'd like to customize the bootloader to load the prepared M7_0 App(AUTOSAR SWP) with example work(AN13750 - Integration_Reference_Examples_S32G2_2022_06).&lt;/P&gt;&lt;P&gt;However, I have one doubt regarding RTD.&lt;/P&gt;&lt;P&gt;- In AN13750, Bootloader was made based on 'RTD_4.4_3.0.2'&lt;/P&gt;&lt;P&gt;- The prepared M7_0 App image's RTD version is 'ex. RTD_4.4_4.0.2_P04'&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Q1. Are bootloaders and apps with different RTD version compatible?&lt;/P&gt;&lt;P&gt;Q2. If not, is there a way to change the example bootloader's RTD version to specific RTD version?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Dominic.&lt;/P&gt;</description>
      <pubDate>Fri, 20 Sep 2024 07:37:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Is-it-mandatory-to-match-RTD-version-between-M7-0-Bootloader-and/m-p/1958504#M10848</guid>
      <dc:creator>Dominic88</dc:creator>
      <dc:date>2024-09-20T07:37:50Z</dc:date>
    </item>
    <item>
      <title>Re: Is it mandatory to match RTD version between M7_0 Bootloader and M7_0 App?</title>
      <link>https://community.nxp.com/t5/S32G/Is-it-mandatory-to-match-RTD-version-between-M7-0-Bootloader-and/m-p/1959393#M10870</link>
      <description>&lt;P&gt;Hello, &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/240856"&gt;@Dominic88&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for you post.&lt;/P&gt;
&lt;P&gt;I suggest using the same RTD during the development.&lt;/P&gt;
&lt;P&gt;Regarding to the bootloader and the corresponding M7 application running on same M7_0, since bootloader fully quits and totally switched to the M7_0 application, it may not impact if different RTD used for bootloader and M7_0 application, but again, I suggest using the same RTD during the development work.&lt;/P&gt;
&lt;P&gt;It is possible to change the RTD used for the bootloader, you may rebuild the bootloader using different RTD, &amp;nbsp;but unlike the version that used in the AN, the other version are not verified and tested, there may be issues that need to be debugged during the integration.&lt;/P&gt;
&lt;P&gt;For bootloader itself, the version that mentioned in the AN is relatively old, there are newer version for your reference which are based with newer version RTD.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Mon, 23 Sep 2024 02:58:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Is-it-mandatory-to-match-RTD-version-between-M7-0-Bootloader-and/m-p/1959393#M10870</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-09-23T02:58:51Z</dc:date>
    </item>
  </channel>
</rss>