<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: S32G3 RDB3 boot from QSPI issue</title>
    <link>https://community.nxp.com/t5/S32G/S32G3-RDB3-boot-from-QSPI-issue/m-p/1953004#M10765</link>
    <description>&lt;P&gt;Hi Chenyin,&lt;/P&gt;&lt;P&gt;Thank you for the dip switch setting.&lt;/P&gt;&lt;P&gt;I tried using the bsp41 pre-built fip.s32-qspi image, and you are correct—it successfully boots. However, the fip.s32-qspi image generated from the fsl-image-auto build(bsp41) does not boot. Do you know if I should be using a different command to generate the correct fip.s32-qspi&amp;nbsp;QSPI image?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;XD&lt;/P&gt;</description>
    <pubDate>Thu, 12 Sep 2024 04:22:25 GMT</pubDate>
    <dc:creator>XD</dc:creator>
    <dc:date>2024-09-12T04:22:25Z</dc:date>
    <item>
      <title>S32G3 RDB3 boot from QSPI issue</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-RDB3-boot-from-QSPI-issue/m-p/1951573#M10697</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using bsp41 to generate QSPI images (fip.s32-qspi and fsl-image-flash-s32g399ardb3.flashimage). However, none of them are able to boot after I used S32flashtool to flash them into QSPI via UART. The command I used is:&lt;/P&gt;&lt;P&gt;S32G3xxx.bin -a MX25UW51245G.bin -fwrite -f fip.s32-qspi -addr 0&lt;/P&gt;&lt;P&gt;I am confused about the RDB3 dip switch settings. I followed the bsp41 user manual (section 4.3.3), changing SW4[3:4] and SW7[6], but it seems that the ON position is opposite from what I expected (top-side down). Another document mentioned setting all switches SW4-7 to OFF, but neither approach has resulted in a successful boot from QSPI. Can you clarify the correct dip switch settings or suggest other possible solutions?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;XD&lt;/P&gt;</description>
      <pubDate>Wed, 11 Sep 2024 02:05:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-RDB3-boot-from-QSPI-issue/m-p/1951573#M10697</guid>
      <dc:creator>XD</dc:creator>
      <dc:date>2024-09-11T02:05:08Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 RDB3 boot from QSPI issue</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-RDB3-boot-from-QSPI-issue/m-p/1952949#M10758</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello, &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235130"&gt;@XD&lt;/a&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Thanks for the post.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I have tested it from my side with pre-built images for QSPI boot, it seems working correct, below please find the switch settings for your reference.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="chenyin_h_0-1726111317025.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/298732iCE8244F01001BE03/image-size/medium?v=v2&amp;amp;px=400" role="button" title="chenyin_h_0-1726111317025.png" alt="chenyin_h_0-1726111317025.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Thu, 12 Sep 2024 03:22:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-RDB3-boot-from-QSPI-issue/m-p/1952949#M10758</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-09-12T03:22:35Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 RDB3 boot from QSPI issue</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-RDB3-boot-from-QSPI-issue/m-p/1953004#M10765</link>
      <description>&lt;P&gt;Hi Chenyin,&lt;/P&gt;&lt;P&gt;Thank you for the dip switch setting.&lt;/P&gt;&lt;P&gt;I tried using the bsp41 pre-built fip.s32-qspi image, and you are correct—it successfully boots. However, the fip.s32-qspi image generated from the fsl-image-auto build(bsp41) does not boot. Do you know if I should be using a different command to generate the correct fip.s32-qspi&amp;nbsp;QSPI image?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;XD&lt;/P&gt;</description>
      <pubDate>Thu, 12 Sep 2024 04:22:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-RDB3-boot-from-QSPI-issue/m-p/1953004#M10765</guid>
      <dc:creator>XD</dc:creator>
      <dc:date>2024-09-12T04:22:25Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 RDB3 boot from QSPI issue</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-RDB3-boot-from-QSPI-issue/m-p/1953135#M10773</link>
      <description>&lt;P&gt;Hi Chenyin,&lt;/P&gt;&lt;P&gt;Please disregard this issue. It turns out that the S32flashtool has a problem on Linux. While it works well for eMMC flashing, it doesn't seem to function properly with QSPI flashing. I have already matched the flash parameters to those used in the Windows version, and the same file successfully booted when flashed using the Windows tool. Thank you for your support.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;XD&lt;/P&gt;</description>
      <pubDate>Thu, 12 Sep 2024 06:50:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-RDB3-boot-from-QSPI-issue/m-p/1953135#M10773</guid>
      <dc:creator>XD</dc:creator>
      <dc:date>2024-09-12T06:50:34Z</dc:date>
    </item>
  </channel>
</rss>