<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックS32DS DRAM U-Boot Code Generation</title>
    <link>https://community.nxp.com/t5/S32G/S32DS-DRAM-U-Boot-Code-Generation/m-p/1950302#M10667</link>
    <description>&lt;P&gt;I am using the S32DS DRAM Tool for profiling my board and am able to generate functional Arm Trusted Firmware code. When I change the setting to instead generate U-Boot code it creates the same code set as used for the ATF. Ive created a clean new project to try to generate U-Boot code but it is not generating. Is this feature functional?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;The AT-F generated code is not compatible with the U-Boot code base as far as I can tell, the files that are generated do not exist in the U-Boot code tree.&lt;/P&gt;</description>
    <pubDate>Mon, 09 Sep 2024 19:07:48 GMT</pubDate>
    <dc:creator>minersrevolt</dc:creator>
    <dc:date>2024-09-09T19:07:48Z</dc:date>
    <item>
      <title>S32DS DRAM U-Boot Code Generation</title>
      <link>https://community.nxp.com/t5/S32G/S32DS-DRAM-U-Boot-Code-Generation/m-p/1950302#M10667</link>
      <description>&lt;P&gt;I am using the S32DS DRAM Tool for profiling my board and am able to generate functional Arm Trusted Firmware code. When I change the setting to instead generate U-Boot code it creates the same code set as used for the ATF. Ive created a clean new project to try to generate U-Boot code but it is not generating. Is this feature functional?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;The AT-F generated code is not compatible with the U-Boot code base as far as I can tell, the files that are generated do not exist in the U-Boot code tree.&lt;/P&gt;</description>
      <pubDate>Mon, 09 Sep 2024 19:07:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32DS-DRAM-U-Boot-Code-Generation/m-p/1950302#M10667</guid>
      <dc:creator>minersrevolt</dc:creator>
      <dc:date>2024-09-09T19:07:48Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS DRAM U-Boot Code Generation</title>
      <link>https://community.nxp.com/t5/S32G/S32DS-DRAM-U-Boot-Code-Generation/m-p/1951716#M10703</link>
      <description>&lt;P&gt;Thanks for the post.&lt;/P&gt;
&lt;P&gt;I have checked the document, and do not find that the u-boot feature is removed from the generated code style with DDR tools.&lt;/P&gt;
&lt;P&gt;But since several year ago, the BSP for S32G has moved the DDR code to TFA&lt;/P&gt;
&lt;P&gt;Instead of the u-boot, as a result, you may have a try with the DDR tools in S32DS3.4, also I suggest referencing the DDR code structure from BSP31 or a little earlier. In which the DDR code are located under u-boot.&lt;/P&gt;
&lt;P&gt;Sorry for your inconvenience.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Wed, 11 Sep 2024 06:08:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32DS-DRAM-U-Boot-Code-Generation/m-p/1951716#M10703</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-09-11T06:08:05Z</dc:date>
    </item>
  </channel>
</rss>