<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32G399A - Is Device Tree Configuration for U-Boot required? in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32G399A-Is-Device-Tree-Configuration-for-U-Boot-required/m-p/1946745#M10605</link>
    <description>&lt;P&gt;Dear NXP fellows,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I see, for example, that in the Release BSP41.0 of U-Boot, there is no specific DTS or DTSI files concerning the S32G399A board in &lt;A href="https://github.com/nxp-auto-linux/u-boot/tree/release/bsp41.0-2022.04/arch/arm/dts" target="_blank"&gt;https://github.com/nxp-auto-linux/u-boot/tree/release/bsp41.0-2022.04/arch/arm/dts&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;The Arm-Trusted Firmware has the DTS files for the S32G boards.&lt;/P&gt;&lt;P&gt;However, I saw one project where the developer patched U-boot for including the configurations required by the S32G boards.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, my question is: Are the DTS configurations in this case managed exclusively by the ATF or I do have to manage the DTS in U-Boot too?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your help,&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Guilherme&lt;/P&gt;</description>
    <pubDate>Wed, 04 Sep 2024 01:55:28 GMT</pubDate>
    <dc:creator>GuilhermeS32G3</dc:creator>
    <dc:date>2024-09-04T01:55:28Z</dc:date>
    <item>
      <title>S32G399A - Is Device Tree Configuration for U-Boot required?</title>
      <link>https://community.nxp.com/t5/S32G/S32G399A-Is-Device-Tree-Configuration-for-U-Boot-required/m-p/1946745#M10605</link>
      <description>&lt;P&gt;Dear NXP fellows,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I see, for example, that in the Release BSP41.0 of U-Boot, there is no specific DTS or DTSI files concerning the S32G399A board in &lt;A href="https://github.com/nxp-auto-linux/u-boot/tree/release/bsp41.0-2022.04/arch/arm/dts" target="_blank"&gt;https://github.com/nxp-auto-linux/u-boot/tree/release/bsp41.0-2022.04/arch/arm/dts&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;The Arm-Trusted Firmware has the DTS files for the S32G boards.&lt;/P&gt;&lt;P&gt;However, I saw one project where the developer patched U-boot for including the configurations required by the S32G boards.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, my question is: Are the DTS configurations in this case managed exclusively by the ATF or I do have to manage the DTS in U-Boot too?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your help,&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Guilherme&lt;/P&gt;</description>
      <pubDate>Wed, 04 Sep 2024 01:55:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G399A-Is-Device-Tree-Configuration-for-U-Boot-required/m-p/1946745#M10605</guid>
      <dc:creator>GuilhermeS32G3</dc:creator>
      <dc:date>2024-09-04T01:55:28Z</dc:date>
    </item>
    <item>
      <title>Re: S32G399A - Is Device Tree Configuration for U-Boot required?</title>
      <link>https://community.nxp.com/t5/S32G/S32G399A-Is-Device-Tree-Configuration-for-U-Boot-required/m-p/1949855#M10659</link>
      <description>&lt;P&gt;Hello, &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/239861"&gt;@GuilhermeS32G3&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for the post&lt;/P&gt;
&lt;P&gt;From BSP's perspective, the dts is managed by ATF, you may not need to modify the files under u-boot.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Mon, 09 Sep 2024 07:46:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G399A-Is-Device-Tree-Configuration-for-U-Boot-required/m-p/1949855#M10659</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-09-09T07:46:24Z</dc:date>
    </item>
    <item>
      <title>Re: S32G399A - Is Device Tree Configuration for U-Boot required?</title>
      <link>https://community.nxp.com/t5/S32G/S32G399A-Is-Device-Tree-Configuration-for-U-Boot-required/m-p/1949856#M10660</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/24163"&gt;@chenyin_h&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much for the answer!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Guilherme&lt;/P&gt;</description>
      <pubDate>Mon, 09 Sep 2024 07:47:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G399A-Is-Device-Tree-Configuration-for-U-Boot-required/m-p/1949856#M10660</guid>
      <dc:creator>GuilhermeS32G3</dc:creator>
      <dc:date>2024-09-09T07:47:45Z</dc:date>
    </item>
  </channel>
</rss>