<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 GoldVip S32G3999A RDB3: Unable to validate NXP example Gateway usecases</title>
    <link>https://community.nxp.com/t5/S32G/GoldVip-S32G3999A-RDB3-Unable-to-validate-NXP-example-Gateway/m-p/1946321#M10599</link>
    <description>&lt;P&gt;1. Followed the instruction of GoldVIP bring up with the S32G3 V 1.12 version.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. The RDB3 is booting from the SD card fine however at the end seeing the following error/warning&lt;/P&gt;&lt;P&gt;[ 33.017785] pfeng-slave 46000000.pfe_slave: ERR: (DRIVER) event 1 - Driver runtime error: [pfeng-slave-drv.c:265] PFE controller UP timed out&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;3. Setup a dcoker container environment as per instructions&lt;/P&gt;&lt;P&gt;4. start the ethernet gateway "A53 slow-path use cases"&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;vip@PTCLAPSUBRAS:~/goldvip$ sudo ./eth-slow-path-host.sh -L 3 -d full -t UDP -l 30 enx24f5a2f0fab0 enx002427884bba&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Creating nw_ns0 and nw_ns1 network namespaces...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Adding enx24f5a2f0fab0 interface to nw_ns0...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Adding enx002427884bba interface to nw_ns1...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;PING 10.0.1.2 (10.0.1.2) 56(84) bytes of data.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;--- 10.0.1.2 ping statistics ---&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;4 packets transmitted, 0 received, 100% packet loss, time 3064ms&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Setting IP 192.168.100.1 to enx24f5a2f0fab0 in nw_ns0...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Setting IP 10.0.1.1 to enx002427884bba in nw_ns1...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Checking network between the network namespaces&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Failed to connect to the network!&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Retrying...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Deleting network namespaces...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Killing iperf3 process...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Creating nw_ns0 and nw_ns1 network namespaces...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Adding enx24f5a2f0fab0 interface to nw_ns0...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Adding enx002427884bba interface to nw_ns1...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;connect: Network is unreachable&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Setting IP 192.168.100.1 to enx24f5a2f0fab0 in nw_ns0...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Setting IP 10.0.1.1 to enx002427884bba in nw_ns1...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Checking network between the network namespaces&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Failed to connect to the network!&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Retrying...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Deleting network namespaces...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Killing iperf3 process...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Creating nw_ns0 and nw_ns1 network namespaces...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Adding enx24f5a2f0fab0 interface to nw_ns0...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Adding enx002427884bba interface to nw_ns1...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;connect: Network is unreachable&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Setting IP 192.168.100.1 to enx24f5a2f0fab0 in nw_ns0...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Setting IP 10.0.1.1 to enx002427884bba in nw_ns1...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Checking network between the network namespaces&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Failed to connect to the network!&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Retrying...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Deleting network namespaces...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Killing iperf3 process...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Creating nw_ns0 and nw_ns1 network namespaces...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Adding enx24f5a2f0fab0 interface to nw_ns0...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Adding enx002427884bba interface to nw_ns1...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;connect: Network is unreachable&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Setting IP 192.168.100.1 to enx24f5a2f0fab0 in nw_ns0...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Setting IP 10.0.1.1 to enx002427884bba in nw_ns1...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Checking network between the network namespaces&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Failed to connect to the network!&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Deleting network namespaces...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Killing iperf3 process...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;vip@PTCLAPSUBRAS:~/goldvip$&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;while the above test is going on from the docker shell, minicom is printing the following….&lt;/P&gt;&lt;P&gt;&lt;EM&gt;root@s32g399ardb3:~# /home/root/eth-gw/eth-cleanup-target.sh&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Device "pfe0sl" does not exist.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;An error occurred in file /home/root/eth-gw/eth-cleanup-target.sh, at line 43&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;root@s32g399ardb3:~# /home/root/eth-gw/eth-slow-path-target.sh -L 3&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Cannot find device "pfe0sl"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;An error occurred in file /home/root/eth-gw/eth-slow-path-target.sh, at line 53&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;root@s32g399ardb3:~# /home/root/eth-gw/eth-cleanup-target.sh&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Device "pfe0sl" does not exist.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;An error occurred in file /home/root/eth-gw/eth-cleanup-target.sh, at line 43&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 03 Sep 2024 13:40:08 GMT</pubDate>
    <dc:creator>senthilnathan_pas</dc:creator>
    <dc:date>2024-09-03T13:40:08Z</dc:date>
    <item>
      <title>GoldVip S32G3999A RDB3: Unable to validate NXP example Gateway usecases</title>
      <link>https://community.nxp.com/t5/S32G/GoldVip-S32G3999A-RDB3-Unable-to-validate-NXP-example-Gateway/m-p/1946321#M10599</link>
      <description>&lt;P&gt;1. Followed the instruction of GoldVIP bring up with the S32G3 V 1.12 version.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. The RDB3 is booting from the SD card fine however at the end seeing the following error/warning&lt;/P&gt;&lt;P&gt;[ 33.017785] pfeng-slave 46000000.pfe_slave: ERR: (DRIVER) event 1 - Driver runtime error: [pfeng-slave-drv.c:265] PFE controller UP timed out&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;3. Setup a dcoker container environment as per instructions&lt;/P&gt;&lt;P&gt;4. start the ethernet gateway "A53 slow-path use cases"&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;vip@PTCLAPSUBRAS:~/goldvip$ sudo ./eth-slow-path-host.sh -L 3 -d full -t UDP -l 30 enx24f5a2f0fab0 enx002427884bba&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Creating nw_ns0 and nw_ns1 network namespaces...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Adding enx24f5a2f0fab0 interface to nw_ns0...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Adding enx002427884bba interface to nw_ns1...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;PING 10.0.1.2 (10.0.1.2) 56(84) bytes of data.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;--- 10.0.1.2 ping statistics ---&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;4 packets transmitted, 0 received, 100% packet loss, time 3064ms&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Setting IP 192.168.100.1 to enx24f5a2f0fab0 in nw_ns0...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Setting IP 10.0.1.1 to enx002427884bba in nw_ns1...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Checking network between the network namespaces&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Failed to connect to the network!&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Retrying...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Deleting network namespaces...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Killing iperf3 process...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Creating nw_ns0 and nw_ns1 network namespaces...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Adding enx24f5a2f0fab0 interface to nw_ns0...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Adding enx002427884bba interface to nw_ns1...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;connect: Network is unreachable&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Setting IP 192.168.100.1 to enx24f5a2f0fab0 in nw_ns0...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Setting IP 10.0.1.1 to enx002427884bba in nw_ns1...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Checking network between the network namespaces&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Failed to connect to the network!&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Retrying...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Deleting network namespaces...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Killing iperf3 process...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Creating nw_ns0 and nw_ns1 network namespaces...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Adding enx24f5a2f0fab0 interface to nw_ns0...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Adding enx002427884bba interface to nw_ns1...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;connect: Network is unreachable&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Setting IP 192.168.100.1 to enx24f5a2f0fab0 in nw_ns0...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Setting IP 10.0.1.1 to enx002427884bba in nw_ns1...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Checking network between the network namespaces&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Failed to connect to the network!&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Retrying...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Deleting network namespaces...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Killing iperf3 process...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Creating nw_ns0 and nw_ns1 network namespaces...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Adding enx24f5a2f0fab0 interface to nw_ns0...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Adding enx002427884bba interface to nw_ns1...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;connect: Network is unreachable&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Setting IP 192.168.100.1 to enx24f5a2f0fab0 in nw_ns0...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Setting IP 10.0.1.1 to enx002427884bba in nw_ns1...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Checking network between the network namespaces&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Failed to connect to the network!&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Deleting network namespaces...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Killing iperf3 process...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;vip@PTCLAPSUBRAS:~/goldvip$&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;while the above test is going on from the docker shell, minicom is printing the following….&lt;/P&gt;&lt;P&gt;&lt;EM&gt;root@s32g399ardb3:~# /home/root/eth-gw/eth-cleanup-target.sh&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Device "pfe0sl" does not exist.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;An error occurred in file /home/root/eth-gw/eth-cleanup-target.sh, at line 43&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;root@s32g399ardb3:~# /home/root/eth-gw/eth-slow-path-target.sh -L 3&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Cannot find device "pfe0sl"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;An error occurred in file /home/root/eth-gw/eth-slow-path-target.sh, at line 53&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;root@s32g399ardb3:~# /home/root/eth-gw/eth-cleanup-target.sh&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Device "pfe0sl" does not exist.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;An error occurred in file /home/root/eth-gw/eth-cleanup-target.sh, at line 43&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Sep 2024 13:40:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/GoldVip-S32G3999A-RDB3-Unable-to-validate-NXP-example-Gateway/m-p/1946321#M10599</guid>
      <dc:creator>senthilnathan_pas</dc:creator>
      <dc:date>2024-09-03T13:40:08Z</dc:date>
    </item>
    <item>
      <title>Re: GoldVip S32G3999A RDB3: Unable to validate NXP example Gateway usecases</title>
      <link>https://community.nxp.com/t5/S32G/GoldVip-S32G3999A-RDB3-Unable-to-validate-NXP-example-Gateway/m-p/1946708#M10603</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/239902"&gt;@senthilnathan_pas&lt;/a&gt;&amp;nbsp;, thanks for contacting NXP support.&lt;/P&gt;
&lt;P&gt;I will try to replicate the behavior you are seeing to check if there is a problem with the examples provided, it may take a little while to setup all the tools needed and then investigate the root cause, so I appreciate your patience.&lt;/P&gt;
&lt;P&gt;I understand that the first error (steps 1 and 2) are from section&amp;nbsp;&lt;STRONG&gt;5&amp;nbsp;GoldVIP Quick Start&lt;/STRONG&gt;&amp;nbsp;and the second error (steps 3 and 4) are from section&amp;nbsp;&lt;STRONG&gt;6 Docker&lt;/STRONG&gt; of the&amp;nbsp;of the&amp;nbsp;&lt;STRONG&gt;S32G Vehicle Integration Platform (GoldVIP) User Manual for S32G3/UM12007&lt;/STRONG&gt;&amp;nbsp;in my case I have &lt;STRONG&gt;Rev. 1.12.0 — 18 June 2024 &lt;/STRONG&gt;(your revision should match, since I'm using GoldVIP 1.12), is my understanding correct?&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 04 Sep 2024 00:13:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/GoldVip-S32G3999A-RDB3-Unable-to-validate-NXP-example-Gateway/m-p/1946708#M10603</guid>
      <dc:creator>alejandro_e</dc:creator>
      <dc:date>2024-09-04T00:13:59Z</dc:date>
    </item>
    <item>
      <title>Re: GoldVip S32G3999A RDB3: Unable to validate NXP example Gateway usecases</title>
      <link>https://community.nxp.com/t5/S32G/GoldVip-S32G3999A-RDB3-Unable-to-validate-NXP-example-Gateway/m-p/1948448#M10630</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/239902"&gt;@senthilnathan_pas&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;While doing some investigation on the topic I found a very similar case, the explanation to the problem is as follows:&lt;/P&gt;
&lt;P&gt;"&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;GoldVIP includes a multi-instance PFE setup, where the PFE master driver is on the Cortex-M7_0 core (GoldVIP Real-time Gateway Application), and the slave instance runs on the Cortex-A53 clusters (Linux). The master instance has to be up and running, so that the slave one could work.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;So, I recommend to follow the steps described in our User Manual and use the NOR Flash boot mode, so that the application running on the Cortex-M7 cores is also loaded and started.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;"&lt;/P&gt;
&lt;P&gt;The steps to enable the examples are in section&amp;nbsp;&lt;STRONG&gt;5 GoldVIP Quick Start&amp;nbsp;&lt;/STRONG&gt;of the&amp;nbsp;&lt;STRONG&gt;S32G Vehicle Integration Platform (GoldVIP) User Manual for S32G3&amp;nbsp;&lt;/STRONG&gt;[Rev. 1.12.0 — 18 June 2024].&lt;/P&gt;
&lt;P&gt;You should see a string similar to "&lt;EM&gt;bootloader 0x2 Application 0 image fragment 0 of size 3145728 was loaded from QSPI, address 0x400000."&amp;nbsp;&amp;nbsp;&lt;/EM&gt;in the boot logs when the bootloader is configured to boot both cores.&lt;/P&gt;
&lt;P&gt;With your current configuration configuration a log like "&lt;EM&gt;M7_0 core is not started, ipc-shm-chdev module will not be inserted"&lt;/EM&gt;&amp;nbsp; should appear right now, indicating the problem with the Real time core.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please let me know if this information was useful.&lt;/P&gt;</description>
      <pubDate>Thu, 05 Sep 2024 17:33:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/GoldVip-S32G3999A-RDB3-Unable-to-validate-NXP-example-Gateway/m-p/1948448#M10630</guid>
      <dc:creator>alejandro_e</dc:creator>
      <dc:date>2024-09-05T17:33:58Z</dc:date>
    </item>
  </channel>
</rss>