<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using the S32g274rdb2 development board to debug the bootloader in S32G</title>
    <link>https://community.nxp.com/t5/S32G/Using-the-S32g274rdb2-development-board-to-debug-the-bootloader/m-p/1939883#M10493</link>
    <description>&lt;P&gt;It stops flashing once entering the kernel.&lt;BR /&gt;I only changed the status of SPI1 for dts in uboot and kernel to disable.The document I refer to is S32G_Bootloader_V2-2022.1024_eng.pdf .&lt;/P&gt;</description>
    <pubDate>Mon, 26 Aug 2024 03:39:01 GMT</pubDate>
    <dc:creator>sdx111</dc:creator>
    <dc:date>2024-08-26T03:39:01Z</dc:date>
    <item>
      <title>Using the S32g274rdb2 development board to debug the bootloader</title>
      <link>https://community.nxp.com/t5/S32G/Using-the-S32g274rdb2-development-board-to-debug-the-bootloader/m-p/1938191#M10457</link>
      <description>&lt;P&gt;&lt;SPAN&gt;With reference to this document, I have changed the state of SPI1 of BSP35 in core A to disable. Why does this GPIO LED still stop flashing after core A loads SPI1 during operation?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="sdx111_0-1724311825912.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/294694i0FC63A0B19E7F86D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="sdx111_0-1724311825912.png" alt="sdx111_0-1724311825912.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="sdx111_1-1724311844342.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/294695i9537F2766BFBD093/image-size/medium?v=v2&amp;amp;px=400" role="button" title="sdx111_1-1724311844342.png" alt="sdx111_1-1724311844342.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 22 Aug 2024 07:48:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Using-the-S32g274rdb2-development-board-to-debug-the-bootloader/m-p/1938191#M10457</guid>
      <dc:creator>sdx111</dc:creator>
      <dc:date>2024-08-22T07:48:56Z</dc:date>
    </item>
    <item>
      <title>Re: Using the S32g274rdb2 development board to debug the bootloader</title>
      <link>https://community.nxp.com/t5/S32G/Using-the-S32g274rdb2-development-board-to-debug-the-bootloader/m-p/1939849#M10492</link>
      <description>&lt;P&gt;Hello, &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231473"&gt;@sdx111&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for the question and sorry for the delay.&lt;/P&gt;
&lt;P&gt;May I know if it stops flashing once entering the uboot or kernel? how you disabling the SPI1?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Mon, 26 Aug 2024 03:03:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Using-the-S32g274rdb2-development-board-to-debug-the-bootloader/m-p/1939849#M10492</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-08-26T03:03:13Z</dc:date>
    </item>
    <item>
      <title>Re: Using the S32g274rdb2 development board to debug the bootloader</title>
      <link>https://community.nxp.com/t5/S32G/Using-the-S32g274rdb2-development-board-to-debug-the-bootloader/m-p/1939883#M10493</link>
      <description>&lt;P&gt;It stops flashing once entering the kernel.&lt;BR /&gt;I only changed the status of SPI1 for dts in uboot and kernel to disable.The document I refer to is S32G_Bootloader_V2-2022.1024_eng.pdf .&lt;/P&gt;</description>
      <pubDate>Mon, 26 Aug 2024 03:39:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Using-the-S32g274rdb2-development-board-to-debug-the-bootloader/m-p/1939883#M10493</guid>
      <dc:creator>sdx111</dc:creator>
      <dc:date>2024-08-26T03:39:01Z</dc:date>
    </item>
    <item>
      <title>Re: Using the S32g274rdb2 development board to debug the bootloader</title>
      <link>https://community.nxp.com/t5/S32G/Using-the-S32g274rdb2-development-board-to-debug-the-bootloader/m-p/1940810#M10500</link>
      <description>&lt;P&gt;Hello, &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231473"&gt;@sdx111&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for the clarification.&lt;/P&gt;
&lt;P&gt;Sorry that I do not see problem from this training document attached,&amp;nbsp; from your test, it is correct under u-boot, right? since there is issue once enter the kernel, would you please try removing the corresponding nodes from kernel DTS?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Tue, 27 Aug 2024 02:41:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Using-the-S32g274rdb2-development-board-to-debug-the-bootloader/m-p/1940810#M10500</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-08-27T02:41:47Z</dc:date>
    </item>
    <item>
      <title>Re: Using the S32g274rdb2 development board to debug the bootloader</title>
      <link>https://community.nxp.com/t5/S32G/Using-the-S32g274rdb2-development-board-to-debug-the-bootloader/m-p/1940910#M10503</link>
      <description>Yes,It is correct under u-boot.&lt;BR /&gt;In addition, please check 4.3 DIO MCAL+Linux test in the training document, which also suggests the A core driver stops after loading SPI.&lt;BR /&gt;I tried to remove the corresponding nodes from kernel DTS earlier. However, I do not know why A core will not start directly. Could you please tell me some detailed operations?</description>
      <pubDate>Tue, 27 Aug 2024 05:14:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Using-the-S32g274rdb2-development-board-to-debug-the-bootloader/m-p/1940910#M10503</guid>
      <dc:creator>sdx111</dc:creator>
      <dc:date>2024-08-27T05:14:57Z</dc:date>
    </item>
    <item>
      <title>Re: Using the S32g274rdb2 development board to debug the bootloader</title>
      <link>https://community.nxp.com/t5/S32G/Using-the-S32g274rdb2-development-board-to-debug-the-bootloader/m-p/1941754#M10507</link>
      <description>&lt;P&gt;Hello, &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231473"&gt;@sdx111&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for the reply.&lt;/P&gt;
&lt;P&gt;I assume that you are using the DIO example as the M core application to flash the LED, right? I remember that only GPIO6 is used in that example.&lt;/P&gt;
&lt;P&gt;If you have disabled the corresponding pin in kernel, it seems odd that the Linux booting is impacted. May I know if your bootloader could boot the A core side properly if not booting the M core side simultaneously?&lt;/P&gt;
&lt;P&gt;Let me summarize the status, correct me if any misunderstanding made, if any, I do apologize.&lt;/P&gt;
&lt;P&gt;1. The LED keep flashing when enter u-boot.&lt;/P&gt;
&lt;P&gt;2. When entering the kernel, if only changed the state of SPI1 in kernel dts to disable, the kernel could boot correctly but the LED stop flashing.&lt;/P&gt;
&lt;P&gt;3. When entering the kernel, if only removing the corresponding nodes from kernel DTS, the kernel could not boot correctly, right? how about the LED status?&lt;/P&gt;
&lt;P&gt;At last, I remeber that the DIO example's code will blink the LED for some time, and do not flash at last, may I know if you were actually using the Dio_ToggleLed_S32G274A_M7 example from which version of RTD?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Wed, 28 Aug 2024 04:30:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Using-the-S32g274rdb2-development-board-to-debug-the-bootloader/m-p/1941754#M10507</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-08-28T04:30:34Z</dc:date>
    </item>
    <item>
      <title>Re: Using the S32g274rdb2 development board to debug the bootloader</title>
      <link>https://community.nxp.com/t5/S32G/Using-the-S32g274rdb2-development-board-to-debug-the-bootloader/m-p/1945306#M10584</link>
      <description>I am using the DIO example as the M core application to flash the LED.&lt;BR /&gt;My bootloader could boot the A core side properly if not booting the M core side simultaneously.&lt;BR /&gt;&lt;BR /&gt;1. The LED keep flashing when enter u-boot.&lt;BR /&gt;Yes&lt;BR /&gt;&lt;BR /&gt;2. When entering the kernel, if only changed the state of SPI1 in kernel dts to disable, the kernel could boot correctly but the LED stop flashing.&lt;BR /&gt;Yes&lt;BR /&gt;&lt;BR /&gt;3. When entering the kernel, if only removing the corresponding nodes from kernel DTS, the kernel could not boot correctly. LED keep flashing.&lt;BR /&gt;&lt;BR /&gt;We changed the DIO example to always flash.</description>
      <pubDate>Mon, 02 Sep 2024 08:28:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Using-the-S32g274rdb2-development-board-to-debug-the-bootloader/m-p/1945306#M10584</guid>
      <dc:creator>sdx111</dc:creator>
      <dc:date>2024-09-02T08:28:39Z</dc:date>
    </item>
    <item>
      <title>Re: Using the S32g274rdb2 development board to debug the bootloader</title>
      <link>https://community.nxp.com/t5/S32G/Using-the-S32g274rdb2-development-board-to-debug-the-bootloader/m-p/1945958#M10593</link>
      <description>&lt;P&gt;Hello, &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231473"&gt;@sdx111&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your reply.&lt;/P&gt;
&lt;P&gt;Well, commonly such A&amp;amp;M booting issue is caused by the resource conflicts, including clock, memory, pinmux, etc. &lt;/P&gt;
&lt;P&gt;Let me try it later to see if it could be reproduced, if any findings made, I will update you, besides, I suggest continue checking any possible conflicts one by one according to your own implementation.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Tue, 03 Sep 2024 06:52:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Using-the-S32g274rdb2-development-board-to-debug-the-bootloader/m-p/1945958#M10593</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-09-03T06:52:58Z</dc:date>
    </item>
  </channel>
</rss>