<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NXP BESS 1.0 reference solution for DBC in Power &amp; Energy</title>
    <link>https://community.nxp.com/t5/Power-Energy/NXP-BESS-1-0-reference-solution-for-DBC/m-p/2355088#M95</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I recently purchased the NXP BESS 1.0 reference solution (BMU/CMU/BJB setup), and I am currently exploring the provided software and communication interfaces.&lt;/P&gt;&lt;P&gt;I have a question regarding CAN communication:&lt;/P&gt;&lt;P&gt;Is it possible to import and use a DBC file within the provided software or reference application?&lt;BR /&gt;For example, is there any built-in support or recommended approach for integrating a DBC-based CAN message definition into the system?&lt;/P&gt;&lt;P&gt;I noticed that the BMU supports CAN-FD communication , but I could not find clear information about DBC usage or tooling support in the software package.&lt;/P&gt;&lt;P&gt;Also, I am relatively new to CAN communication, so any guidance, examples, or best practices would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
    <pubDate>Thu, 23 Apr 2026 08:42:57 GMT</pubDate>
    <dc:creator>JeHwanYoo</dc:creator>
    <dc:date>2026-04-23T08:42:57Z</dc:date>
    <item>
      <title>NXP BESS 1.0 reference solution for DBC</title>
      <link>https://community.nxp.com/t5/Power-Energy/NXP-BESS-1-0-reference-solution-for-DBC/m-p/2355088#M95</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I recently purchased the NXP BESS 1.0 reference solution (BMU/CMU/BJB setup), and I am currently exploring the provided software and communication interfaces.&lt;/P&gt;&lt;P&gt;I have a question regarding CAN communication:&lt;/P&gt;&lt;P&gt;Is it possible to import and use a DBC file within the provided software or reference application?&lt;BR /&gt;For example, is there any built-in support or recommended approach for integrating a DBC-based CAN message definition into the system?&lt;/P&gt;&lt;P&gt;I noticed that the BMU supports CAN-FD communication , but I could not find clear information about DBC usage or tooling support in the software package.&lt;/P&gt;&lt;P&gt;Also, I am relatively new to CAN communication, so any guidance, examples, or best practices would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Thu, 23 Apr 2026 08:42:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Energy/NXP-BESS-1-0-reference-solution-for-DBC/m-p/2355088#M95</guid>
      <dc:creator>JeHwanYoo</dc:creator>
      <dc:date>2026-04-23T08:42:57Z</dc:date>
    </item>
  </channel>
</rss>