<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power &amp; EnergyのトピックRe: iMXRT1170EVKB</title>
    <link>https://community.nxp.com/t5/Power-Energy/iMXRT1170EVKB/m-p/1904945#M70</link>
    <description>&lt;P&gt;It is possible that the system is not powered correctly, if only using the debugger USB then you need to make sure that the jumper is on the correct position so it powers the entire system.&lt;BR /&gt;If everything is properly powered then refer to this post:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/RT-board-recovery-for-debugger-connect-issues/ta-p/1635260" target="_blank"&gt;RT board recovery for debugger connect issues - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Tue, 09 Jul 2024 22:30:27 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2024-07-09T22:30:27Z</dc:date>
    <item>
      <title>iMXRT1170EVKB</title>
      <link>https://community.nxp.com/t5/Power-Energy/iMXRT1170EVKB/m-p/1899397#M63</link>
      <description>&lt;P&gt;In iMX RT 1170 EVKB i got this problem during debugging.&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;P&gt;Probe Firmware: MCU-LINK on-board (r0E2) CMSIS-DAP V2.250 (NXP Semiconductors)&lt;/P&gt;&lt;P&gt;Serial Number: NVUYDXEI5YUN1&lt;/P&gt;&lt;P&gt;VID:PID: 1FC9:0143&lt;/P&gt;&lt;P&gt;USB Path: \\?\hid#vid_1fc9&amp;amp;pid_0143&amp;amp;mi_00#7&amp;amp;38ddcd02&amp;amp;0&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}&lt;/P&gt;&lt;P&gt;connection failed - Em(04). Cannot provide power to DAP bus... Retrying&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Failed on connect: Em(04). Cannot provide power to DAP bus.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Connected&amp;amp;Reset. Was: NotConnected. DpID: 6BA02477. CpuID: 00000000. Info: &amp;lt;None&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Last stub error 0: OK&lt;/P&gt;&lt;P&gt;Last sticky error: 0x0 AIndex: 0&lt;/P&gt;&lt;P&gt;No debug bus (MemAp) selected&lt;/P&gt;&lt;P&gt;DAP Speed test unexecuted or failed&lt;/P&gt;&lt;P&gt;Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can I solve it??&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Thu, 04 Jul 2024 09:22:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Energy/iMXRT1170EVKB/m-p/1899397#M63</guid>
      <dc:creator>KKR231</dc:creator>
      <dc:date>2024-07-04T09:22:41Z</dc:date>
    </item>
    <item>
      <title>Re: iMXRT1170EVKB</title>
      <link>https://community.nxp.com/t5/Power-Energy/iMXRT1170EVKB/m-p/1904945#M70</link>
      <description>&lt;P&gt;It is possible that the system is not powered correctly, if only using the debugger USB then you need to make sure that the jumper is on the correct position so it powers the entire system.&lt;BR /&gt;If everything is properly powered then refer to this post:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/RT-board-recovery-for-debugger-connect-issues/ta-p/1635260" target="_blank"&gt;RT board recovery for debugger connect issues - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Tue, 09 Jul 2024 22:30:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Energy/iMXRT1170EVKB/m-p/1904945#M70</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2024-07-09T22:30:27Z</dc:date>
    </item>
  </channel>
</rss>