<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power &amp; EnergyのトピックRe: esd</title>
    <link>https://community.nxp.com/t5/Power-Energy/esd/m-p/1874570#M59</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;For surge protection in a 10/100M Ethernet application, consider NXP's PESD3V3L1BA or PESD5V0S1BA series surge protectors. These devices offer bidirectional protection with low series resistance (1.4 ohms), minimal channel-to-channel resistance (0.03 ohms max), and fast response time to transition from normal operating state to current limiting state. With a peak impulse voltage&amp;nbsp;&lt;A href="https://www-adpvantage.com" target="_self"&gt;ADPVantage&lt;/A&gt; withstand of up to 40V, they effectively safeguard against excessive voltages and currents during surge events, ensuring protection for high-speed, low-voltage drivers and receivers.&lt;/P&gt;</description>
    <pubDate>Sat, 25 May 2024 04:46:47 GMT</pubDate>
    <dc:creator>kurdt784</dc:creator>
    <dc:date>2024-05-25T04:46:47Z</dc:date>
    <item>
      <title>esd</title>
      <link>https://community.nxp.com/t5/Power-Energy/esd/m-p/1870542#M51</link>
      <description>&lt;DIV class=""&gt;We are looking for the surge protector&amp;nbsp;in unidirectional and bi-directional mode. Can you suggest the part from NXPs portfolio if&amp;nbsp;it matches the technical specifications?&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;High speed protectors&amp;nbsp; are the TVS devices to form an extremely low let-through energy barrier to excessive voltages and currents during surge events which may cause damage to unprotected high-speed, low voltage drivers and receivers. components.&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;STRONG&gt;They are used in multiple applications but we need a 10/100M ethernet application.&lt;/STRONG&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;UL&gt;&lt;LI&gt;Current required for the device to go from operating state to protected state- 750mA&lt;/LI&gt;&lt;LI&gt;Series resistance-1.4Ohms&lt;/LI&gt;&lt;LI&gt;Chanel to channel resistance-0.03ohms max&lt;/LI&gt;&lt;LI&gt;Time for the device to go from normal operating state to current limiting state - 50ns&lt;/LI&gt;&lt;LI&gt;Peak impulse voltage withstand with duration less than 1 ms - 40V max&lt;/LI&gt;&lt;/UL&gt;&lt;/DIV&gt;</description>
      <pubDate>Wed, 22 May 2024 09:20:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Energy/esd/m-p/1870542#M51</guid>
      <dc:creator>smkalim</dc:creator>
      <dc:date>2024-05-22T09:20:37Z</dc:date>
    </item>
    <item>
      <title>Re: esd</title>
      <link>https://community.nxp.com/t5/Power-Energy/esd/m-p/1871469#M53</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;smkalim&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;For the ESD discrete products had already transferred to&amp;nbsp;&lt;A class="" tabindex="0" href="http://www.baidu.com/link?url=jMbDCiy2ePElS4ot5D0Gj1W-hkENZ48lnQsQKwU_HBwV1OmFWp674Tp4uyEpiTcqarY2Xp2F2jWguF68XMfekb7Q2BX87tVM29iskRh6p-y" target="_blank" rel="noopener" data-showurl-highlight="true" data-click="{&amp;quot;F&amp;quot;:&amp;quot;738317EA&amp;quot;,&amp;quot;F1&amp;quot;:&amp;quot;9D73F1E4&amp;quot;,&amp;quot;F2&amp;quot;:&amp;quot;4CA6DE6A&amp;quot;,&amp;quot;F3&amp;quot;:&amp;quot;54E5243F&amp;quot;,&amp;quot;T&amp;quot;:1716430579,&amp;quot;y&amp;quot;:&amp;quot;EB5DF376&amp;quot;}" aria-label=""&gt;Nexperia.&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;You can directly contact with them for getting support！！&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Thu, 23 May 2024 02:17:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Energy/esd/m-p/1871469#M53</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2024-05-23T02:17:10Z</dc:date>
    </item>
    <item>
      <title>Re: esd</title>
      <link>https://community.nxp.com/t5/Power-Energy/esd/m-p/1874570#M59</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;For surge protection in a 10/100M Ethernet application, consider NXP's PESD3V3L1BA or PESD5V0S1BA series surge protectors. These devices offer bidirectional protection with low series resistance (1.4 ohms), minimal channel-to-channel resistance (0.03 ohms max), and fast response time to transition from normal operating state to current limiting state. With a peak impulse voltage&amp;nbsp;&lt;A href="https://www-adpvantage.com" target="_self"&gt;ADPVantage&lt;/A&gt; withstand of up to 40V, they effectively safeguard against excessive voltages and currents during surge events, ensuring protection for high-speed, low-voltage drivers and receivers.&lt;/P&gt;</description>
      <pubDate>Sat, 25 May 2024 04:46:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Energy/esd/m-p/1874570#M59</guid>
      <dc:creator>kurdt784</dc:creator>
      <dc:date>2024-05-25T04:46:47Z</dc:date>
    </item>
  </channel>
</rss>