<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC33730 linear regulators in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/MC33730-linear-regulators/m-p/1032671#M921</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you G.w. Sun,&lt;/P&gt;&lt;P&gt;so there isn't at all the risk to damage the linear regulator or may be the entire chip?, I mean, the stage that should drive the external pass transistor (may be an op amp?) works always in saturation because of the absence of the feedback voltage, I think..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Alessandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 31 Mar 2020 12:59:45 GMT</pubDate>
    <dc:creator>Gelby</dc:creator>
    <dc:date>2020-03-31T12:59:45Z</dc:date>
    <item>
      <title>MC33730 linear regulators</title>
      <link>https://community.nxp.com/t5/Power-Management/MC33730-linear-regulators/m-p/1032670#M920</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;I'm going to use the MC3370 chip in an environment where I need only the 5V and the 3.3V voltages.&lt;/P&gt;&lt;P&gt;I don't need to use any stand by supplies, I know the VKAM is always active (also with the chip in sleep mode) and this is ok for me, I want to use VDDL as 3.3V source and I don't need more.&lt;/P&gt;&lt;P&gt;To save power in stand by, I want to program the VDD3 regulator as 3.3V, not stand by regulator, but I don't need it because I use the VDDL regulator as 3.3V source, here my question, have I to add the external pass NPN transistor and bypass capacitors to the VDD3 circuitry (VDD3_B and VDD3), or can I simply left open these two pins (VDD3_B and VDD3)?&lt;/P&gt;&lt;P&gt;Thanks a lot,&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alessandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Mar 2020 10:06:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/MC33730-linear-regulators/m-p/1032670#M920</guid>
      <dc:creator>Gelby</dc:creator>
      <dc:date>2020-03-30T10:06:45Z</dc:date>
    </item>
    <item>
      <title>Re: MC33730 linear regulators</title>
      <link>https://community.nxp.com/t5/Power-Management/MC33730-linear-regulators/m-p/1032671#M921</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you G.w. Sun,&lt;/P&gt;&lt;P&gt;so there isn't at all the risk to damage the linear regulator or may be the entire chip?, I mean, the stage that should drive the external pass transistor (may be an op amp?) works always in saturation because of the absence of the feedback voltage, I think..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Alessandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Mar 2020 12:59:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/MC33730-linear-regulators/m-p/1032671#M921</guid>
      <dc:creator>Gelby</dc:creator>
      <dc:date>2020-03-31T12:59:45Z</dc:date>
    </item>
    <item>
      <title>Re: MC33730 linear regulators</title>
      <link>https://community.nxp.com/t5/Power-Management/MC33730-linear-regulators/m-p/1032672#M922</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Alessandro&lt;/P&gt;&lt;P&gt;After discussed ,to be on safe consider please add the external pass NPN transistor and bypass capacitors to the VDD3 circuitry (VDD3_B and VDD3) if unused this LDO&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Apr 2020 01:32:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/MC33730-linear-regulators/m-p/1032672#M922</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2020-04-01T01:32:59Z</dc:date>
    </item>
  </channel>
</rss>