<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MC33771 BCC init issue in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/MC33771-BCC-init-issue/m-p/1031889#M916</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sir&lt;/P&gt;&lt;P&gt;I modify the BCC V1.1 connect the 2pcs MC33771, but now&amp;nbsp; the CID2 init seems have problem,&lt;/P&gt;&lt;P&gt;i lost some thing modify?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/100561iDECB78BCA83547D3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Feb 2020 03:31:25 GMT</pubDate>
    <dc:creator>kentseng</dc:creator>
    <dc:date>2020-02-03T03:31:25Z</dc:date>
    <item>
      <title>MC33771 BCC init issue</title>
      <link>https://community.nxp.com/t5/Power-Management/MC33771-BCC-init-issue/m-p/1031889#M916</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sir&lt;/P&gt;&lt;P&gt;I modify the BCC V1.1 connect the 2pcs MC33771, but now&amp;nbsp; the CID2 init seems have problem,&lt;/P&gt;&lt;P&gt;i lost some thing modify?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/100561iDECB78BCA83547D3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Feb 2020 03:31:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/MC33771-BCC-init-issue/m-p/1031889#M916</guid>
      <dc:creator>kentseng</dc:creator>
      <dc:date>2020-02-03T03:31:25Z</dc:date>
    </item>
    <item>
      <title>Re: MC33771 BCC init issue</title>
      <link>https://community.nxp.com/t5/Power-Management/MC33771-BCC-init-issue/m-p/1031890#M917</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tzu,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The driver itself support up to 15 devices in the TPL mode.&lt;/P&gt;&lt;P&gt;The provided example(s) projects are determined for a use case of &lt;STRONG&gt;one BCC device&lt;/STRONG&gt; as it is written in its (/their) documentations.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When more BCC devices are used, &lt;EM style="color: #002060; "&gt;BCC_INIT_CONF&lt;/EM&gt; must be initialized as &lt;EM style="color: #002060; "&gt;[&lt;STRONG&gt;NUMBER OF DEVICES&lt;/STRONG&gt;][BCC_INIT_CONF_REG_CNT]&lt;/EM&gt; with appropriate register values for each BCC device separately.&lt;/P&gt;&lt;P&gt;Another possibility is to &lt;STRONG&gt;keep the second parameter of BCC_Init function NULL&lt;/STRONG&gt; and to initialize the registers by BCC_Reg_Write or BCC_Reg_GlobalWrite operations by yourself.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Feb 2020 11:35:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/MC33771-BCC-init-issue/m-p/1031890#M917</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2020-02-05T11:35:29Z</dc:date>
    </item>
  </channel>
</rss>