<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックRe: KV10 entry VLLS3 and LLWU wakeup question</title>
    <link>https://community.nxp.com/t5/Power-Management/KV10-entry-VLLS3-and-LLWU-wakeup-question/m-p/1013992#M808</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,can you explain more about it ? I don't understand what does it mean. Thank you very much!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Apr 2020 09:16:06 GMT</pubDate>
    <dc:creator>ChandlerY</dc:creator>
    <dc:date>2020-04-30T09:16:06Z</dc:date>
    <item>
      <title>KV10 entry VLLS3 and LLWU wakeup question</title>
      <link>https://community.nxp.com/t5/Power-Management/KV10-entry-VLLS3-and-LLWU-wakeup-question/m-p/1013987#M803</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I now use the low power VLLS3 mode of KV10Z32, using the wakeup function of the LLWU, but the program will not wake up using the PTC3 (LLWU _ P7) and request help. thanks you&lt;/P&gt;&lt;P&gt;the following is the code&lt;/P&gt;&lt;P&gt;void BOARD_InitPins(void)&lt;BR /&gt;{&lt;BR /&gt; /* Port C Clock Gate Control: Clock enabled */&lt;BR /&gt; CLOCK_EnableClock(kCLOCK_PortC);&lt;BR /&gt; /* Port E Clock Gate Control: Clock enabled */&lt;BR /&gt; CLOCK_EnableClock(kCLOCK_PortE);&lt;/P&gt;&lt;P&gt;gpio_pin_config_t PTE16_config = {&lt;BR /&gt; .pinDirection = kGPIO_DigitalOutput,&lt;BR /&gt; .outputLogic = 0U&lt;BR /&gt; };&lt;BR /&gt; /* Initialize GPIO functionality on pin PTE16 (pin 3) */&lt;BR /&gt; GPIO_PinInit(BOARD_INITPINS_PTE16_GPIO, BOARD_INITPINS_PTE16_PIN, &amp;amp;PTE16_config);&lt;/P&gt;&lt;P&gt;/* PORTC3 (pin 24) is configured as LLWU_P7 */&lt;BR /&gt; PORT_SetPinMux(PORTC, 3U, kPORT_MuxAsGpio);&lt;/P&gt;&lt;P&gt;PORTC-&amp;gt;PCR[3] = ((PORTC-&amp;gt;PCR[3] &amp;amp;&lt;BR /&gt; /* Mask bits to zero which are setting */&lt;BR /&gt; (~(PORT_PCR_PS_MASK | PORT_PCR_ISF_MASK)))&lt;/P&gt;&lt;P&gt;/* Pull Select: Internal pulldown resistor is enabled on the corresponding pin, if the&lt;BR /&gt; * corresponding PE field is set. */ &lt;BR /&gt; | PORT_PCR_PS(PCR_PS_0b0));&lt;/P&gt;&lt;P&gt;/* PORTE16 (pin 3) is configured as PTE16 */&lt;BR /&gt; PORT_SetPinMux(BOARD_INITPINS_PTE16_PORT, BOARD_INITPINS_PTE16_PIN, kPORT_MuxAsGpio);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;int main(void)&lt;BR /&gt;{&lt;BR /&gt; smc_power_mode_vlls_config_t vlls_config; /* Local variable for vlls configuration */&lt;BR /&gt; &lt;BR /&gt; /* Init board hardware. */&lt;BR /&gt; PMC_ClearPeriphIOIsolationFlag(PMC);&lt;BR /&gt; BOARD_InitPins(); &lt;BR /&gt; for(uint32_t i = 0; i&amp;lt;0x5FFF;i++)&lt;BR /&gt; { &lt;BR /&gt; delay();&lt;BR /&gt; GPIO_WritePinOutput(GPIOE,16,1); &lt;BR /&gt; delay(); &lt;BR /&gt; GPIO_WritePinOutput(GPIOE,16,0); &lt;BR /&gt; } &lt;BR /&gt; LLWU_SetExternalWakeupPinMode(LLWU,7,kLLWU_ExternalPinRisingEdge); &lt;BR /&gt; &lt;BR /&gt; vlls_config.subMode = kSMC_StopSub3; &lt;BR /&gt; SMC_PreEnterStopModes();&lt;BR /&gt; SMC_SetPowerModeVlls(SMC, &amp;amp;vlls_config);&lt;BR /&gt; PMC-&amp;gt;REGSC = PMC_REGSC_ACKISO_MASK;&lt;BR /&gt; SMC_PostExitStopModes(); &lt;BR /&gt; &lt;BR /&gt; &lt;BR /&gt; while (1)&lt;BR /&gt; {&lt;BR /&gt; for(uint32_t i = 0; i&amp;lt;0x5FFF;i++)&lt;BR /&gt; { &lt;BR /&gt; delay();&lt;BR /&gt; GPIO_WritePinOutput(GPIOE,16,1); &lt;BR /&gt; delay(); &lt;BR /&gt; GPIO_WritePinOutput(GPIOE,16,0); &lt;BR /&gt; } &lt;BR /&gt; &lt;BR /&gt; }&lt;BR /&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Nov 2019 02:36:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/KV10-entry-VLLS3-and-LLWU-wakeup-question/m-p/1013987#M803</guid>
      <dc:creator>胡绍广</dc:creator>
      <dc:date>2019-11-20T02:36:06Z</dc:date>
    </item>
    <item>
      <title>Re: KV10 entry VLLS3 and LLWU wakeup question</title>
      <link>https://community.nxp.com/t5/Power-Management/KV10-entry-VLLS3-and-LLWU-wakeup-question/m-p/1013988#M804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You do not use the signal Multiplexing function.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="2.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/92246i57A3140F21F02418/image-size/large?v=v2&amp;amp;px=999" role="button" title="2.PNG" alt="2.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Nov 2019 01:08:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/KV10-entry-VLLS3-and-LLWU-wakeup-question/m-p/1013988#M804</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2019-11-21T01:08:11Z</dc:date>
    </item>
    <item>
      <title>Re: KV10 entry VLLS3 and LLWU wakeup question</title>
      <link>https://community.nxp.com/t5/Power-Management/KV10-entry-VLLS3-and-LLWU-wakeup-question/m-p/1013989#M805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much for your answer. This problem has been solved. The new problem I encounter now is that the data of SRAM is lost after exiting VLLS3 mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please tell me what I should do now so as not to lose SRAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The development environment I use is Keil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Nov 2019 01:32:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/KV10-entry-VLLS3-and-LLWU-wakeup-question/m-p/1013989#M805</guid>
      <dc:creator>胡绍广</dc:creator>
      <dc:date>2019-11-21T01:32:18Z</dc:date>
    </item>
    <item>
      <title>Re: KV10 entry VLLS3 and LLWU wakeup question</title>
      <link>https://community.nxp.com/t5/Power-Management/KV10-entry-VLLS3-and-LLWU-wakeup-question/m-p/1013990#M806</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class="" data-section="0" style="color: #333333; background-color: #f7f8fa; font-weight: normal; font-size: 14px;"&gt;&lt;SPAN class="" data-group="0-0" data-section="0" data-sentence="0"&gt;Thank you very much for your answer. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="" data-section="0" style="color: #333333; background-color: #f7f8fa; font-weight: normal; font-size: 14px;"&gt;&lt;SPAN class="" data-group="0-0" data-section="0" data-sentence="0"&gt;This problem has been solved. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="" data-section="0" style="color: #333333; background-color: #f7f8fa; font-weight: normal; font-size: 14px;"&gt;&lt;SPAN class="" data-group="0-0" data-section="0" data-sentence="0"&gt;The new problem I encounter now is that the data of SRAM is lost after exiting VLLS3 mode.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="" data-section="1" style="color: #333333; background-color: #f7f8fa; font-weight: normal; font-size: 14px;"&gt;&lt;SPAN class="" data-group="1-0" data-section="1" data-sentence="0"&gt;Please tell me what I should do now so as not to lose SRAM.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="" data-section="2" style="color: #333333; background-color: #f7f8fa; font-weight: normal; font-size: 14px;"&gt;&lt;SPAN class="" data-group="2-0" data-section="2" data-sentence="0"&gt;The development environment I use is Keil&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Nov 2019 02:59:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/KV10-entry-VLLS3-and-LLWU-wakeup-question/m-p/1013990#M806</guid>
      <dc:creator>胡绍广</dc:creator>
      <dc:date>2019-11-21T02:59:44Z</dc:date>
    </item>
    <item>
      <title>Re: KV10 entry VLLS3 and LLWU wakeup question</title>
      <link>https://community.nxp.com/t5/Power-Management/KV10-entry-VLLS3-and-LLWU-wakeup-question/m-p/1013991#M807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Sorry. If you have other's question. Please create a new question.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;------------------------------------------------------------------------------- &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Nov 2019 01:29:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/KV10-entry-VLLS3-and-LLWU-wakeup-question/m-p/1013991#M807</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2019-11-22T01:29:44Z</dc:date>
    </item>
    <item>
      <title>Re: KV10 entry VLLS3 and LLWU wakeup question</title>
      <link>https://community.nxp.com/t5/Power-Management/KV10-entry-VLLS3-and-LLWU-wakeup-question/m-p/1013992#M808</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,can you explain more about it ? I don't understand what does it mean. Thank you very much!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Apr 2020 09:16:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/KV10-entry-VLLS3-and-LLWU-wakeup-question/m-p/1013992#M808</guid>
      <dc:creator>ChandlerY</dc:creator>
      <dc:date>2020-04-30T09:16:06Z</dc:date>
    </item>
    <item>
      <title>Re: KV10 entry VLLS3 and LLWU wakeup question</title>
      <link>https://community.nxp.com/t5/Power-Management/KV10-entry-VLLS3-and-LLWU-wakeup-question/m-p/1013993#M809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The comment shows that we should configure the pin as LLWU. But the next line, the function configure the pin as GPIO.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 May 2020 02:40:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/KV10-entry-VLLS3-and-LLWU-wakeup-question/m-p/1013993#M809</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2020-05-06T02:40:02Z</dc:date>
    </item>
  </channel>
</rss>