<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックRe: Vadc absolute measurement input voltage</title>
    <link>https://community.nxp.com/t5/Power-Management/Vadc-absolute-measurement-input-voltage/m-p/1004561#M754</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The voltage range for GPIOx for either measurement method must be A&lt;SPAN style="font-size: 12px;"&gt;GND&lt;/SPAN&gt; to V&lt;SPAN style="font-size: 12px;"&gt;COM&lt;/SPAN&gt;.&amp;nbsp; The maximum voltage per&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;(MC33771B)/table 7 is as I originally stated and have to be the thresholds for the protection clamp diodes.&amp;nbsp; As I read section &lt;SPAN&gt;(MC33771B)/&lt;/SPAN&gt;9.16.4 I interpret it to mean that ratiometric conversion is only used for temperature measurements.&amp;nbsp; If GPIOx is configured as a ratiometric input then the MC33771 will test the generated digital value against the OT and UT thresholds to qualify for fault conditions.&amp;nbsp; If a GPIOx is configured as absolute then no testing is done on the digital result.&amp;nbsp; However, in both measurement modes V&lt;SPAN style="font-size: 12px;"&gt;COM&lt;/SPAN&gt; is the reference.&amp;nbsp; Why the V&lt;SPAN style="font-size: 12px;"&gt;ADC&lt;/SPAN&gt; specification description adds "...for ratiometric measurements" is confusing.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Mar 2020 02:43:56 GMT</pubDate>
    <dc:creator>noel_lanier</dc:creator>
    <dc:date>2020-03-19T02:43:56Z</dc:date>
    <item>
      <title>Vadc absolute measurement input voltage</title>
      <link>https://community.nxp.com/t5/Power-Management/Vadc-absolute-measurement-input-voltage/m-p/1004555#M748</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does anyone know the maximum Vadc input voltage for absolute measurements? The MC33771 datasheet only specifies the maximum input voltage for ratiometric measurements (AGND..Vcom) #MC33771&amp;nbsp;#Vadc&amp;nbsp;#absolute&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Mar 2020 09:50:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Vadc-absolute-measurement-input-voltage/m-p/1004555#M748</guid>
      <dc:creator>kshitij_dadheka</dc:creator>
      <dc:date>2020-03-09T09:50:05Z</dc:date>
    </item>
    <item>
      <title>Re: Vadc absolute measurement input voltage</title>
      <link>https://community.nxp.com/t5/Power-Management/Vadc-absolute-measurement-input-voltage/m-p/1004556#M749</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I believe the max range for ADC1 for a CTx input can be inferred from the specifications for V&lt;SPAN style="font-size: 12px;"&gt;CT_RNG&lt;/SPAN&gt;.&lt;SPAN style="font-size: 15px;"&gt;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&amp;nbsp;(0 &amp;lt;= V&lt;SPAN style="font-size: 12px;"&gt;CT&lt;/SPAN&gt; &amp;lt;= 4.85)V&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Mar 2020 23:09:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Vadc-absolute-measurement-input-voltage/m-p/1004556#M749</guid>
      <dc:creator>noel_lanier</dc:creator>
      <dc:date>2020-03-09T23:09:04Z</dc:date>
    </item>
    <item>
      <title>Re: Vadc absolute measurement input voltage</title>
      <link>https://community.nxp.com/t5/Power-Management/Vadc-absolute-measurement-input-voltage/m-p/1004557#M750</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do you mean the CTx pin specification?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Mar 2020 06:46:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Vadc-absolute-measurement-input-voltage/m-p/1004557#M750</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2020-03-10T06:46:32Z</dc:date>
    </item>
    <item>
      <title>Re: Vadc absolute measurement input voltage</title>
      <link>https://community.nxp.com/t5/Power-Management/Vadc-absolute-measurement-input-voltage/m-p/1004558#M751</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, I mean the specification for absolute analog measurements on the GPIOx inputs. For ratiometric it is for Vadc specified in the 'General purpose input/output GPIOx' section of the datasheet as between AGND and Vcom, but for absolute measurements no range is specified.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Mar 2020 09:07:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Vadc-absolute-measurement-input-voltage/m-p/1004558#M751</guid>
      <dc:creator>kshitij_dadheka</dc:creator>
      <dc:date>2020-03-10T09:07:03Z</dc:date>
    </item>
    <item>
      <title>Re: Vadc absolute measurement input voltage</title>
      <link>https://community.nxp.com/t5/Power-Management/Vadc-absolute-measurement-input-voltage/m-p/1004559#M752</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;V&lt;SPAN style="font-size: 12px;"&gt;ADC(MAX)&lt;/SPAN&gt; for a GPIOx input is relative to V&lt;SPAN style="font-size: 12px;"&gt;COM&lt;/SPAN&gt;.&amp;nbsp; See Fig 17 in the datasheet.&amp;nbsp; The ADC reference is switched from the internal ADCREF to V&lt;SPAN style="font-size: 12px;"&gt;COM&lt;/SPAN&gt; when using GPIO as analog inputs.&amp;nbsp; V&lt;SPAN style="font-size: 12px;"&gt;GPIOx(ABS MAX)&lt;/SPAN&gt; is (V&lt;SPAN style="font-size: 12px;"&gt;COM&lt;/SPAN&gt;+0.5)V&amp;nbsp; However, if V&lt;SPAN style="font-size: 12px;"&gt;COM&lt;/SPAN&gt; is the reference then anything above that will measure as Full-Scale.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Mar 2020 16:39:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Vadc-absolute-measurement-input-voltage/m-p/1004559#M752</guid>
      <dc:creator>noel_lanier</dc:creator>
      <dc:date>2020-03-10T16:39:30Z</dc:date>
    </item>
    <item>
      <title>Re: Vadc absolute measurement input voltage</title>
      <link>https://community.nxp.com/t5/Power-Management/Vadc-absolute-measurement-input-voltage/m-p/1004560#M753</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Noel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for your reply. However, if I look at table 16 (table 12 for the MC33771C) I see 2 operational modes for the analog modes of any GPIOx: absolute and ratiometric. If Vcom is the reference for both I do not see why the settings for the GPIOx should be different (see table 57 (MC33771B)/table 51 (MC33771C): GPIO_CFG1. If Vcom is the reference for both modes, the fact that the measurement is then absolute or ratiometric is determined by the external circuitry: if it is fed by Vcom it will be ratiometric, if it is fed by an independent source is will be absolute. A different setting in GPIO_CFG1 however implies to me that the ADC is fed with different references (VCOM? ADCREF? other?), hence a different maximum voltage range on the GPIOx inputs. It is this voltage range that I am interested in for an absolute measurement. The voltage range for a ratiometric measurement is explicitly mentioned in table 9 (MC33771B)/table 8 (MC33771C) under 'General purpose input/output GPIOx' -&amp;gt; 'Vadc: Amalog ADC input voltage range for ratiometric measurements'&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Mar 2020 08:42:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Vadc-absolute-measurement-input-voltage/m-p/1004560#M753</guid>
      <dc:creator>kshitij_dadheka</dc:creator>
      <dc:date>2020-03-11T08:42:18Z</dc:date>
    </item>
    <item>
      <title>Re: Vadc absolute measurement input voltage</title>
      <link>https://community.nxp.com/t5/Power-Management/Vadc-absolute-measurement-input-voltage/m-p/1004561#M754</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The voltage range for GPIOx for either measurement method must be A&lt;SPAN style="font-size: 12px;"&gt;GND&lt;/SPAN&gt; to V&lt;SPAN style="font-size: 12px;"&gt;COM&lt;/SPAN&gt;.&amp;nbsp; The maximum voltage per&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;(MC33771B)/table 7 is as I originally stated and have to be the thresholds for the protection clamp diodes.&amp;nbsp; As I read section &lt;SPAN&gt;(MC33771B)/&lt;/SPAN&gt;9.16.4 I interpret it to mean that ratiometric conversion is only used for temperature measurements.&amp;nbsp; If GPIOx is configured as a ratiometric input then the MC33771 will test the generated digital value against the OT and UT thresholds to qualify for fault conditions.&amp;nbsp; If a GPIOx is configured as absolute then no testing is done on the digital result.&amp;nbsp; However, in both measurement modes V&lt;SPAN style="font-size: 12px;"&gt;COM&lt;/SPAN&gt; is the reference.&amp;nbsp; Why the V&lt;SPAN style="font-size: 12px;"&gt;ADC&lt;/SPAN&gt; specification description adds "...for ratiometric measurements" is confusing.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2020 02:43:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Vadc-absolute-measurement-input-voltage/m-p/1004561#M754</guid>
      <dc:creator>noel_lanier</dc:creator>
      <dc:date>2020-03-19T02:43:56Z</dc:date>
    </item>
    <item>
      <title>Re: Vadc absolute measurement input voltage</title>
      <link>https://community.nxp.com/t5/Power-Management/Vadc-absolute-measurement-input-voltage/m-p/1004562#M755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Noel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for this clarification, this was indeed the answer I was looking for!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Mar 2020 09:26:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Vadc-absolute-measurement-input-voltage/m-p/1004562#M755</guid>
      <dc:creator>kshitij_dadheka</dc:creator>
      <dc:date>2020-03-20T09:26:35Z</dc:date>
    </item>
  </channel>
</rss>