<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックRe: MMPF0100F0AEP Power Up</title>
    <link>https://community.nxp.com/t5/Power-Management/MMPF0100F0AEP-Power-Up/m-p/966378#M623</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI&lt;/P&gt;&lt;P&gt;I attached the schematic for your reference about EVB of PF0100.&lt;/P&gt;&lt;P&gt;Please also try below three items configurations especially for Item1 and 2:&lt;/P&gt;&lt;P&gt;1:If VDDOTP = VCOREDIG (1.5 V), the values are loaded from the default configuration.&lt;BR /&gt;2:If VDDOTP = 0.0 V, TBB_POR = 0 and FUSE_POR_XOR = 1, the values are loaded from the fuses. In the MMPF0100, FUSE_POR1, FUSE_POR2, and FUSE_POR3 are XOR’ed into the FUSE_POR_XOR bit. The FUSE_POR_XOR has to be 1 for fuses to be loaded. This can be achieved by setting any one or all of the FUSE_PORx bits. In the MMPF0100A, the XOR function is removed. It is required to set all of the FUSE_PORx bits to be able to load the fuses.&lt;BR /&gt;3:If VDDOTP = 0.0 V, TBB_POR = 0 and FUSE_POR_XOR = 0, the TBBOTP registers remain initialized at zero.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Jun 2019 02:57:56 GMT</pubDate>
    <dc:creator>guoweisun</dc:creator>
    <dc:date>2019-06-12T02:57:56Z</dc:date>
    <item>
      <title>MMPF0100F0AEP Power Up</title>
      <link>https://community.nxp.com/t5/Power-Management/MMPF0100F0AEP-Power-Up/m-p/966377#M622</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Greetings!!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using MMPF0100F0AEP PMIC for a custom board design, i have ordered pre programmed chip with F0 OTP configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And as per the datasheet&amp;nbsp;VDDOTP is connected to GND to enable the OTP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately i am not getting any output voltages, Can you please help me with the power up procedure for this IC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: I have referred- MCIMX6Q-SDB design.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Arif&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Jun 2019 07:09:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/MMPF0100F0AEP-Power-Up/m-p/966377#M622</guid>
      <dc:creator>arif_kanganoll1</dc:creator>
      <dc:date>2019-06-10T07:09:06Z</dc:date>
    </item>
    <item>
      <title>Re: MMPF0100F0AEP Power Up</title>
      <link>https://community.nxp.com/t5/Power-Management/MMPF0100F0AEP-Power-Up/m-p/966378#M623</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI&lt;/P&gt;&lt;P&gt;I attached the schematic for your reference about EVB of PF0100.&lt;/P&gt;&lt;P&gt;Please also try below three items configurations especially for Item1 and 2:&lt;/P&gt;&lt;P&gt;1:If VDDOTP = VCOREDIG (1.5 V), the values are loaded from the default configuration.&lt;BR /&gt;2:If VDDOTP = 0.0 V, TBB_POR = 0 and FUSE_POR_XOR = 1, the values are loaded from the fuses. In the MMPF0100, FUSE_POR1, FUSE_POR2, and FUSE_POR3 are XOR’ed into the FUSE_POR_XOR bit. The FUSE_POR_XOR has to be 1 for fuses to be loaded. This can be achieved by setting any one or all of the FUSE_PORx bits. In the MMPF0100A, the XOR function is removed. It is required to set all of the FUSE_PORx bits to be able to load the fuses.&lt;BR /&gt;3:If VDDOTP = 0.0 V, TBB_POR = 0 and FUSE_POR_XOR = 0, the TBBOTP registers remain initialized at zero.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jun 2019 02:57:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/MMPF0100F0AEP-Power-Up/m-p/966378#M623</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2019-06-12T02:57:56Z</dc:date>
    </item>
  </channel>
</rss>