<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Built In Self Tests in FS85 in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/Built-In-Self-Tests-in-FS85/m-p/964350#M606</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Haby,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, if ABIST1 (ABIST1_OK = 0) or LBIST (LBIST_OK = 0) fails, RSTB and PGOOD are released, but FS0B remains stuck low keeping the application in safe state. The Fail-safe state machine transitions to the INIT_FS state as usual.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As for the ABIST2, during INIT_FS, the MCU configures the ABIST2 coverage with the FS_I_OVUV_SAFE_REACTION1 register, assigning the voltage monitoring to be verified during ABIST2:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;VCOREMON_ABIST2 = 1 to verify VCOREMON comparators during ABIST2&lt;/LI&gt;&lt;LI&gt;VDDIOMON_ABIST2 = 1 to verify VDDIOMON comparators during ABIST2&lt;/LI&gt;&lt;LI&gt;VMONx_ABIST2 = 1 to verify VMONx comparators during ABIST2&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/90504i51BB146C78A7782E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/90708iF08A2C59830782BC/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_5.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/90837i7192EEA74D26AFAC/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As soon as INIT_FS is closed and the latest voltage regulator assigned to ABIST2 is started, ABIST2 is executed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Sep 2019 13:03:39 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2019-09-24T13:03:39Z</dc:date>
    <item>
      <title>Built In Self Tests in FS85</title>
      <link>https://community.nxp.com/t5/Power-Management/Built-In-Self-Tests-in-FS85/m-p/964349#M605</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What will happen when ABIST or LBIST tests fail in FS85. I understand that FS0B pin will be stuck low. How does FS85 behave after this; will watchdog windowing happens and refresh will be accepted by FS85 without shifting to normal mode? or will RSTB pin be asserted?&lt;/P&gt;&lt;P&gt;Also how ABIST2 test&amp;nbsp;is launched&amp;nbsp;via SPI ? Is it done by configuring FS_I_OVUV_SAFE_REACTION1 register during INIT_FS?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Sep 2019 07:35:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Built-In-Self-Tests-in-FS85/m-p/964349#M605</guid>
      <dc:creator>haby_a</dc:creator>
      <dc:date>2019-09-24T07:35:52Z</dc:date>
    </item>
    <item>
      <title>Re: Built In Self Tests in FS85</title>
      <link>https://community.nxp.com/t5/Power-Management/Built-In-Self-Tests-in-FS85/m-p/964350#M606</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Haby,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, if ABIST1 (ABIST1_OK = 0) or LBIST (LBIST_OK = 0) fails, RSTB and PGOOD are released, but FS0B remains stuck low keeping the application in safe state. The Fail-safe state machine transitions to the INIT_FS state as usual.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As for the ABIST2, during INIT_FS, the MCU configures the ABIST2 coverage with the FS_I_OVUV_SAFE_REACTION1 register, assigning the voltage monitoring to be verified during ABIST2:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;VCOREMON_ABIST2 = 1 to verify VCOREMON comparators during ABIST2&lt;/LI&gt;&lt;LI&gt;VDDIOMON_ABIST2 = 1 to verify VDDIOMON comparators during ABIST2&lt;/LI&gt;&lt;LI&gt;VMONx_ABIST2 = 1 to verify VMONx comparators during ABIST2&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/90504i51BB146C78A7782E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/90708iF08A2C59830782BC/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_5.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/90837i7192EEA74D26AFAC/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As soon as INIT_FS is closed and the latest voltage regulator assigned to ABIST2 is started, ABIST2 is executed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Sep 2019 13:03:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Built-In-Self-Tests-in-FS85/m-p/964350#M606</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2019-09-24T13:03:39Z</dc:date>
    </item>
  </channel>
</rss>