<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックPF8200 open drain pull up voltage</title>
    <link>https://community.nxp.com/t5/Power-Management/PF8200-open-drain-pull-up-voltage/m-p/962663#M598</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on a design that uses the PF8200. RESETB_MCU, INTB, PGOOD, and FSOB are all open drain signals that the datasheet recommends pulling up to VDDIO. However, for my application, I would like to pull them to a slightly different voltage. Since these are all open drain outputs, I believe this is acceptable, but I was hoping someone from NXP could provide a little more direction. Here are my questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Does the voltage on VDDIO affect how high I can pull the open drain outputs? For example, if VDDIO is 1.8V, can I pull the open drain outputs to 3.3V and still get proper operation?&lt;/P&gt;&lt;P&gt;2. If VDDIO is 3.3V, can I pull the open drain outputs to 1.8V and still have them work properly?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Aug 2019 20:35:23 GMT</pubDate>
    <dc:creator>adevries</dc:creator>
    <dc:date>2019-08-22T20:35:23Z</dc:date>
    <item>
      <title>PF8200 open drain pull up voltage</title>
      <link>https://community.nxp.com/t5/Power-Management/PF8200-open-drain-pull-up-voltage/m-p/962663#M598</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on a design that uses the PF8200. RESETB_MCU, INTB, PGOOD, and FSOB are all open drain signals that the datasheet recommends pulling up to VDDIO. However, for my application, I would like to pull them to a slightly different voltage. Since these are all open drain outputs, I believe this is acceptable, but I was hoping someone from NXP could provide a little more direction. Here are my questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Does the voltage on VDDIO affect how high I can pull the open drain outputs? For example, if VDDIO is 1.8V, can I pull the open drain outputs to 3.3V and still get proper operation?&lt;/P&gt;&lt;P&gt;2. If VDDIO is 3.3V, can I pull the open drain outputs to 1.8V and still have them work properly?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Aug 2019 20:35:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF8200-open-drain-pull-up-voltage/m-p/962663#M598</guid>
      <dc:creator>adevries</dc:creator>
      <dc:date>2019-08-22T20:35:23Z</dc:date>
    </item>
    <item>
      <title>Re: PF8200 open drain pull up voltage</title>
      <link>https://community.nxp.com/t5/Power-Management/PF8200-open-drain-pull-up-voltage/m-p/962664#M599</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI &lt;/P&gt;&lt;P&gt;Please see comment:&lt;/P&gt;&lt;P&gt;1. Does the voltage on VDDIO affect how high I can pull the open drain outputs? For example, if VDDIO is 1.8V, can I pull the open drain outputs to 3.3V and still get proper operation?&lt;/P&gt;&lt;P&gt;[gw]Yes,you can!&lt;/P&gt;&lt;P&gt;2. If VDDIO is 3.3V, can I pull the open drain outputs to 1.8V and still have them work properly?&lt;/P&gt;&lt;P&gt;[gw]Yes,you can!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Aug 2019 07:50:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF8200-open-drain-pull-up-voltage/m-p/962664#M599</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2019-08-23T07:50:55Z</dc:date>
    </item>
  </channel>
</rss>