<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FRDM33771 BMS not working properly in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/FRDM33771-BMS-not-working-properly/m-p/961863#M597</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;How do you operate about enable MEAS_ISENSE?&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;For the emulator the current sense output voltage can vary from around −150 mV to +150 mV.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;This output is not designed to drive a large current since the current sense input from the MC3377x needs&lt;BR /&gt;as little as 100 nA. If more than 1 μA is pulled from this output, the voltage may drop by a&lt;BR /&gt;few mV.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 Oct 2019 06:58:28 GMT</pubDate>
    <dc:creator>guoweisun</dc:creator>
    <dc:date>2019-10-31T06:58:28Z</dc:date>
    <item>
      <title>FRDM33771 BMS not working properly</title>
      <link>https://community.nxp.com/t5/Power-Management/FRDM33771-BMS-not-working-properly/m-p/961862#M596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the FRDM33771 together with the battery emulator.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to test cell balancing and measure current for SOC however when I enable the cell balancing I see no difference regarding the voltages and the current measurement seems wrong also.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I enable MEAS_ISENSE I can't change the voltage with the emulator and it keeps -157.286 mV.&lt;/P&gt;&lt;P&gt;Do I have to connect an external shunt resistor or is it already inside the emulator.&lt;/P&gt;&lt;P&gt;See the attachment for further information.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Oct 2019 09:52:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FRDM33771-BMS-not-working-properly/m-p/961862#M596</guid>
      <dc:creator>stagiair4</dc:creator>
      <dc:date>2019-10-24T09:52:38Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM33771 BMS not working properly</title>
      <link>https://community.nxp.com/t5/Power-Management/FRDM33771-BMS-not-working-properly/m-p/961863#M597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;How do you operate about enable MEAS_ISENSE?&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;For the emulator the current sense output voltage can vary from around −150 mV to +150 mV.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;This output is not designed to drive a large current since the current sense input from the MC3377x needs&lt;BR /&gt;as little as 100 nA. If more than 1 μA is pulled from this output, the voltage may drop by a&lt;BR /&gt;few mV.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Oct 2019 06:58:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FRDM33771-BMS-not-working-properly/m-p/961863#M597</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2019-10-31T06:58:28Z</dc:date>
    </item>
  </channel>
</rss>