<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Why using a PF0100 instead PF3000? in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/Why-using-a-PF0100-instead-PF3000/m-p/952806#M543</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;BR /&gt;I'm just curious. In an application where power and voltages of pf3000 are enough...why shoulld i chose a pf0200 for a i.mx6 Solo? ( for example)&lt;BR /&gt;&lt;BR /&gt;I'm not in hurry with a project, i'm just curious. I expect that a pf3000 with right OTP configuration should power a Solo processor.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Oct 2019 16:35:03 GMT</pubDate>
    <dc:creator>massimo2</dc:creator>
    <dc:date>2019-10-22T16:35:03Z</dc:date>
    <item>
      <title>Why using a PF0100 instead PF3000?</title>
      <link>https://community.nxp.com/t5/Power-Management/Why-using-a-PF0100-instead-PF3000/m-p/952806#M543</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;BR /&gt;I'm just curious. In an application where power and voltages of pf3000 are enough...why shoulld i chose a pf0200 for a i.mx6 Solo? ( for example)&lt;BR /&gt;&lt;BR /&gt;I'm not in hurry with a project, i'm just curious. I expect that a pf3000 with right OTP configuration should power a Solo processor.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Oct 2019 16:35:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Why-using-a-PF0100-instead-PF3000/m-p/952806#M543</guid>
      <dc:creator>massimo2</dc:creator>
      <dc:date>2019-10-22T16:35:03Z</dc:date>
    </item>
    <item>
      <title>Re: Why using a PF0100 instead PF3000?</title>
      <link>https://community.nxp.com/t5/Power-Management/Why-using-a-PF0100-instead-PF3000/m-p/952807#M544</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you properly mentioned, power and voltages of PF3000 are enough to turn on the i.mx6 Solo, however, I would strongly recommend to use the PF0200 the main reason that this PMIC is already in the i.mx6 Solo BSP plus you can find it in the reference design: &lt;A href="https://www.nxp.com/design/development-boards/i.mx-evaluation-and-development-boards/sabre-board-for-smart-devices-based-on-the-i.mx-6solox-applications-processors:RD-IMX6SX-SABRE"&gt;https://www.nxp.com/design/development-boards/i.mx-evaluation-and-development-boards/sabre-board-for-smart-devices-based-on-the-i.mx-6solox-applications-processors:RD-IMX6SX-SABRE&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The reason of why NXP decided to use the PF0200/PF0100 for the i.MX6 Solo reference design is because the PF3000 was not launched when the i.MX6 Solo was launched. Plus the PF0200 it is a good PMIC to complete all the power requirements of this processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jose&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Oct 2019 23:35:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Why-using-a-PF0100-instead-PF3000/m-p/952807#M544</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2019-10-23T23:35:31Z</dc:date>
    </item>
    <item>
      <title>Re: Why using a PF0100 instead PF3000?</title>
      <link>https://community.nxp.com/t5/Power-Management/Why-using-a-PF0100-instead-PF3000/m-p/952808#M545</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you.&lt;BR /&gt;I already used it for ULL, that is why i asked. PF3000 is quite cheaper expecially if you buy large amount for multiple projects. However i will stay on pf0200 as recommended. (Time to market cleary wins against price differencees)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Oct 2019 07:01:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Why-using-a-PF0100-instead-PF3000/m-p/952808#M545</guid>
      <dc:creator>massimo2</dc:creator>
      <dc:date>2019-10-24T07:01:17Z</dc:date>
    </item>
  </channel>
</rss>