<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックRe: Solution/reference design for bidirectional AC/DC + bidirectional isolated DC/DC system</title>
    <link>https://community.nxp.com/t5/Power-Management/Solution-reference-design-for-bidirectional-AC-DC-bidirectional/m-p/2410116#M5388</link>
    <description>&lt;P&gt;Hello Sahil,&lt;/P&gt;
&lt;P&gt;NXP has two relevant reference designs for the AC/DC front-end:&lt;/P&gt;
&lt;P&gt;800W Bidirectional AC-DC Conversion Solution (BIDIRECTIONAL-AC-DC-REF-DESIGN) — a fully validated, bidirectional AC/DC converter controlled by the MC56F83783 DSC. It supports both AC-to-DC (PFC mode) and DC-to-AC (grid-tied inverter mode) operation with smooth mode transitions. Key specifications: 800W @ 220Vac, wide input range 85–265Vac, 380V DC bus, peak efficiency &amp;gt;97% @ 220Vac, power factor &amp;gt;0.99. Documentation: UG10208, AN14354. Note that this design uses a full-bridge topology with an LCL filter, not a totem-pole; it is the closest available bidirectional AC/DC reference design from NXP.&lt;/P&gt;
&lt;P&gt;Totem-Pole Bridgeless PFC Converter (RDPFC56F82748) — implements totem-pole bridgeless PFC using the MC56F83783 / MC56F82748 DSC, achieving PF &amp;gt;0.99 and THDi &amp;lt;5%. Documentation: AN12618, DRM174. This specific reference design operates in rectifier (AC-to-DC) mode only and is rated at 240W / 12V output. It is useful as a starting point for totem-pole PFC implementation, but does not include the bidirectional (inverter) control path out of the box.&lt;/P&gt;
&lt;P&gt;If bidirectional operation with totem-pole topology is required in the same design, combining the PFC control from RDPFC56F82748 with the bidirectional control framework from BIDIRECTIONAL-AC-DC-REF-DESIGN would be the recommended approach.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
    <pubDate>Tue, 01 Sep 2026 11:25:07 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2026-09-01T11:25:07Z</dc:date>
    <item>
      <title>Solution/reference design for bidirectional AC/DC + bidirectional isolated DC/DC system</title>
      <link>https://community.nxp.com/t5/Power-Management/Solution-reference-design-for-bidirectional-AC-DC-bidirectional/m-p/2409982#M5387</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;We are assessing a bidirectional digital power system and would like to know if reference designs or nxp solutions are available for a setup like this:&lt;/P&gt;&lt;P&gt;Concept of the system:&lt;/P&gt;&lt;P&gt;AC/DC stage that is bidirectional&lt;/P&gt;&lt;P&gt;PFC topology with a totem pole bridgeless&lt;/P&gt;&lt;P&gt;Bidirectional operation (grid-tied inverter mode and PFC mode)&lt;/P&gt;&lt;P&gt;Isolated DC/DC stage in both directions&lt;/P&gt;&lt;P&gt;Topology of Dual Active Bridge (DAB)&lt;/P&gt;&lt;P&gt;Power flow in both directions with digital control&lt;/P&gt;&lt;P&gt;The system is designed for applications such energy storage systems, bidirectional power converters, or comparable industrial power platforms, and the goal power level is in the multi-kW range.&lt;/P&gt;&lt;P&gt;Would you kindly suggest a reference design or solution?&lt;/P&gt;&lt;P&gt;We will begin with a 1.2kW inverter for 4s pack(nominal 12.8V).&lt;/P&gt;</description>
      <pubDate>Tue, 01 Sep 2026 09:18:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Solution-reference-design-for-bidirectional-AC-DC-bidirectional/m-p/2409982#M5387</guid>
      <dc:creator>sahilHastin</dc:creator>
      <dc:date>2026-09-01T09:18:46Z</dc:date>
    </item>
    <item>
      <title>Re: Solution/reference design for bidirectional AC/DC + bidirectional isolated DC/DC system</title>
      <link>https://community.nxp.com/t5/Power-Management/Solution-reference-design-for-bidirectional-AC-DC-bidirectional/m-p/2410116#M5388</link>
      <description>&lt;P&gt;Hello Sahil,&lt;/P&gt;
&lt;P&gt;NXP has two relevant reference designs for the AC/DC front-end:&lt;/P&gt;
&lt;P&gt;800W Bidirectional AC-DC Conversion Solution (BIDIRECTIONAL-AC-DC-REF-DESIGN) — a fully validated, bidirectional AC/DC converter controlled by the MC56F83783 DSC. It supports both AC-to-DC (PFC mode) and DC-to-AC (grid-tied inverter mode) operation with smooth mode transitions. Key specifications: 800W @ 220Vac, wide input range 85–265Vac, 380V DC bus, peak efficiency &amp;gt;97% @ 220Vac, power factor &amp;gt;0.99. Documentation: UG10208, AN14354. Note that this design uses a full-bridge topology with an LCL filter, not a totem-pole; it is the closest available bidirectional AC/DC reference design from NXP.&lt;/P&gt;
&lt;P&gt;Totem-Pole Bridgeless PFC Converter (RDPFC56F82748) — implements totem-pole bridgeless PFC using the MC56F83783 / MC56F82748 DSC, achieving PF &amp;gt;0.99 and THDi &amp;lt;5%. Documentation: AN12618, DRM174. This specific reference design operates in rectifier (AC-to-DC) mode only and is rated at 240W / 12V output. It is useful as a starting point for totem-pole PFC implementation, but does not include the bidirectional (inverter) control path out of the box.&lt;/P&gt;
&lt;P&gt;If bidirectional operation with totem-pole topology is required in the same design, combining the PFC control from RDPFC56F82748 with the bidirectional control framework from BIDIRECTIONAL-AC-DC-REF-DESIGN would be the recommended approach.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
      <pubDate>Tue, 01 Sep 2026 11:25:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Solution-reference-design-for-bidirectional-AC-DC-bidirectional/m-p/2410116#M5388</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2026-09-01T11:25:07Z</dc:date>
    </item>
    <item>
      <title>Re: Solution/reference design for bidirectional AC/DC + bidirectional isolated DC/DC system</title>
      <link>https://community.nxp.com/t5/Power-Management/Solution-reference-design-for-bidirectional-AC-DC-bidirectional/m-p/2410121#M5389</link>
      <description>Totem pole is not a strict requirement, I am flexible with the topology. I am okay with this reference: BIDIRECTIONAL-AC-DC-REF-DESIGN&lt;BR /&gt;&lt;BR /&gt;Can you also suggest for DC-DC stage, even DAB is not a strict requirement. So if you can suggest a reference for DC-DC stage, it would be very helpful</description>
      <pubDate>Tue, 01 Sep 2026 11:29:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Solution-reference-design-for-bidirectional-AC-DC-bidirectional/m-p/2410121#M5389</guid>
      <dc:creator>sahilHastin</dc:creator>
      <dc:date>2026-09-01T11:29:30Z</dc:date>
    </item>
  </channel>
</rss>