<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic TPL+33664+33774 in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/TPL-33664-33774/m-p/2393380#M5292</link>
    <description>&lt;DIV&gt;&lt;DIV&gt;I have been working on a BMS project recently and encountered the following issues.&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;The publicly available MC33664 datasheet downloaded from NXP’s official website does not contain any register descriptions for the MC33664 transceiver. In addition, the official demo code package I downloaded also lacks any routines for accessing and operating MC33664 internal registers.&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;Does TPL3 communication require read/write access to MC33664’s registers?&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;If register operations are mandatory, could anyone share a complete MC33664 datasheet with full register specifications, as well as a sample demo project that implements MC33664 register read/write logic? Many thanks!&lt;/DIV&gt;&lt;/DIV&gt;</description>
    <pubDate>Fri, 10 Jul 2026 03:55:34 GMT</pubDate>
    <dc:creator>zqing</dc:creator>
    <dc:date>2026-07-10T03:55:34Z</dc:date>
    <item>
      <title>TPL+33664+33774</title>
      <link>https://community.nxp.com/t5/Power-Management/TPL-33664-33774/m-p/2393380#M5292</link>
      <description>&lt;DIV&gt;&lt;DIV&gt;I have been working on a BMS project recently and encountered the following issues.&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;The publicly available MC33664 datasheet downloaded from NXP’s official website does not contain any register descriptions for the MC33664 transceiver. In addition, the official demo code package I downloaded also lacks any routines for accessing and operating MC33664 internal registers.&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;Does TPL3 communication require read/write access to MC33664’s registers?&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;If register operations are mandatory, could anyone share a complete MC33664 datasheet with full register specifications, as well as a sample demo project that implements MC33664 register read/write logic? Many thanks!&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Fri, 10 Jul 2026 03:55:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/TPL-33664-33774/m-p/2393380#M5292</guid>
      <dc:creator>zqing</dc:creator>
      <dc:date>2026-07-10T03:55:34Z</dc:date>
    </item>
    <item>
      <title>Re: TPL+33664+33774</title>
      <link>https://community.nxp.com/t5/Power-Management/TPL-33664-33774/m-p/2393480#M5294</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The datasheet you have downloaded is already the complete, full document. The MC33664 does not contain any internal registers and therefore does not require register read/write operations for TPL communication.&lt;/P&gt;
&lt;P&gt;The device acts as a transparent TPL physical-layer transceiver. It converts the MCU SPI transmit stream into TPL pulse-encoded signals and converts received TPL traffic back into SPI signals. As a result, communication with devices on the TPL network is performed by sending and receiving TPL frames through the SPI interface.&lt;/P&gt;
&lt;P&gt;You may be referring to the newer MC33665A gateway device, which does include internal registers, message queues, routing functions and a register-access protocol. The MC33665A full datasheet (available as a Secure file under NDA) therefore contains extensive register descriptions.&lt;/P&gt;
&lt;P&gt;We have SW device drivers available for both the MC33664 and MC33665 as part of the &lt;A href="https://www.nxp.com/design/design-center/software/embedded-software/nxp-battery-management-software-development-kit-and-toolchain:BMS-SW" target="_self"&gt;Gen1 SDK&lt;/A&gt;. As for the MC33664, the CDD layer on&amp;nbsp;the MCU handles tasks such as pin timing to execute&amp;nbsp;a wake-up sequence,&amp;nbsp;configuring and managing two independent SPI blocks on the MCU simultaneously, interrupt routing etc.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
      <pubDate>Fri, 10 Jul 2026 07:04:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/TPL-33664-33774/m-p/2393480#M5294</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2026-07-10T07:04:11Z</dc:date>
    </item>
  </channel>
</rss>