<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC33879 initialization voltage abnormality and slow initialization in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/MC33879-initialization-voltage-abnormality-and-slow/m-p/2380448#M5236</link>
    <description>&lt;P&gt;分享一下您的原理图。&lt;/P&gt;</description>
    <pubDate>Fri, 12 Jun 2026 00:05:43 GMT</pubDate>
    <dc:creator>guoweisun</dc:creator>
    <dc:date>2026-06-12T00:05:43Z</dc:date>
    <item>
      <title>MC33879 initialization voltage abnormality and slow initialization</title>
      <link>https://community.nxp.com/t5/Power-Management/MC33879-initialization-voltage-abnormality-and-slow/m-p/2379230#M5233</link>
      <description>&lt;P&gt;After supplying power to mc33879, enable the en pin and connect a 12V power to the D1 pin of mc33879. Without giving the command, measure the voltage at the S1 pin, which is 12.45V, slightly higher than 12V. Is this normal?&lt;BR /&gt;Similarly, D1 is connected to a 12V power supply, and S1 is connected to a CAB 500-C current sensor. After I power it on, I control the EN pin high level. According to the manual, after stabilizing at 100us, the command can be issued. However, I need to issue the command 10ms later for the function to be turned on properly because my SPI command has an open/short circuit command detection. The second time I issue the same command every 10ms, the SPI data will display the current channel fault. The third time I issue the same command every 10ms, and the fault will disappear. What's going on?&lt;/P&gt;</description>
      <pubDate>Wed, 10 Jun 2026 01:52:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/MC33879-initialization-voltage-abnormality-and-slow/m-p/2379230#M5233</guid>
      <dc:creator>zuozuo</dc:creator>
      <dc:date>2026-06-10T01:52:06Z</dc:date>
    </item>
    <item>
      <title>Re: MC33879 initialization voltage abnormality and slow initialization</title>
      <link>https://community.nxp.com/t5/Power-Management/MC33879-initialization-voltage-abnormality-and-slow/m-p/2379530#M5234</link>
      <description>&lt;P&gt;It seems there are fault for open or short circuit. You may need to double check your schematics with&amp;nbsp;&lt;SPAN&gt;mc33879 application diagram&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Does VDD connect with 5V instead of 12V?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 10 Jun 2026 12:20:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/MC33879-initialization-voltage-abnormality-and-slow/m-p/2379530#M5234</guid>
      <dc:creator>db16122</dc:creator>
      <dc:date>2026-06-10T12:20:22Z</dc:date>
    </item>
    <item>
      <title>Re: MC33879 initialization voltage abnormality and slow initialization</title>
      <link>https://community.nxp.com/t5/Power-Management/MC33879-initialization-voltage-abnormality-and-slow/m-p/2379884#M5235</link>
      <description>VDD is 5V</description>
      <pubDate>Thu, 11 Jun 2026 06:10:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/MC33879-initialization-voltage-abnormality-and-slow/m-p/2379884#M5235</guid>
      <dc:creator>zuozuo</dc:creator>
      <dc:date>2026-06-11T06:10:16Z</dc:date>
    </item>
    <item>
      <title>Re: MC33879 initialization voltage abnormality and slow initialization</title>
      <link>https://community.nxp.com/t5/Power-Management/MC33879-initialization-voltage-abnormality-and-slow/m-p/2380448#M5236</link>
      <description>&lt;P&gt;分享一下您的原理图。&lt;/P&gt;</description>
      <pubDate>Fri, 12 Jun 2026 00:05:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/MC33879-initialization-voltage-abnormality-and-slow/m-p/2380448#M5236</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2026-06-12T00:05:43Z</dc:date>
    </item>
  </channel>
</rss>