<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Clarifications required in SBCFS26 VPRE Regulator Voltage Range in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/Clarifications-required-in-SBCFS26-VPRE-Regulator-Voltage-Range/m-p/2338166#M5085</link>
    <description>Thank you RafaR for providing the clarifications.</description>
    <pubDate>Tue, 24 Mar 2026 06:50:41 GMT</pubDate>
    <dc:creator>Sivahari</dc:creator>
    <dc:date>2026-03-24T06:50:41Z</dc:date>
    <item>
      <title>Clarifications required in SBCFS26 VPRE Regulator Voltage Range</title>
      <link>https://community.nxp.com/t5/Power-Management/Clarifications-required-in-SBCFS26-VPRE-Regulator-Voltage-Range/m-p/2257234#M4858</link>
      <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;I need clarifications in SBCFS26 VPRE Regulator. I had analysis on MFS2613AMDA6 Datasheet for VPRE Voltage regulator. It is mentioned as FS26 is unable to provide power rails when the supply voltage range is below the VPRE_IN minimum Limit.&amp;nbsp;&lt;/P&gt;&lt;P&gt;As per the datasheet, it's minimum voltage range is 4.75V. If this is the case, then whether VMONPRE will trigger VPRE Undervoltage fault since its threshold value is 90% of VPRE monitoring voltage 6V?&lt;/P&gt;&lt;P&gt;And also, please clarify in which use case i could expect VPRE Undervoltage fault?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for understanding.&lt;/P&gt;</description>
      <pubDate>Mon, 08 Dec 2025 14:27:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Clarifications-required-in-SBCFS26-VPRE-Regulator-Voltage-Range/m-p/2257234#M4858</guid>
      <dc:creator>Sivahari</dc:creator>
      <dc:date>2025-12-08T14:27:29Z</dc:date>
    </item>
    <item>
      <title>Re: Clarifications required in SBCFS26 VPRE Regulator Voltage Range</title>
      <link>https://community.nxp.com/t5/Power-Management/Clarifications-required-in-SBCFS26-VPRE-Regulator-Voltage-Range/m-p/2257438#M4859</link>
      <description>&lt;P&gt;Hello Sivahari&lt;/P&gt;
&lt;P&gt;Good Day!&lt;/P&gt;
&lt;P&gt;1.-&lt;/P&gt;
&lt;P&gt;Yes, but only when VPRE is expected to be ON and regulated. If the device is in a mode where VPRE is enabled and regulating ( Normal mode or Standby mode with VPRE active), and the effective VPRE output falls below the VMONPRE UV threshold, the FS26’s safety monitor can flag a VPRE undervoltage fault after the internal deglitch time&lt;/P&gt;
&lt;P&gt;2.- Some cases in which VPRE Undervoltage fault can occur are:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Battery sag / cranking&lt;/LI&gt;
&lt;LI&gt;VSUP falling below the VPRE input minimum&lt;/LI&gt;
&lt;LI&gt;Excessive load step or short on the VPRE rail&lt;/LI&gt;
&lt;LI&gt;Misconfiguration of front‑end vs. direct‑battery topology (OTP dependent)&lt;/LI&gt;
&lt;LI&gt;Thermal or internal protection interactions&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope this information has helped you, please let me know if you need help with anything else.&lt;/P&gt;
&lt;P&gt;Have a great day and best of luck.&lt;/P&gt;</description>
      <pubDate>Mon, 08 Dec 2025 21:04:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Clarifications-required-in-SBCFS26-VPRE-Regulator-Voltage-Range/m-p/2257438#M4859</guid>
      <dc:creator>RafaR</dc:creator>
      <dc:date>2025-12-08T21:04:05Z</dc:date>
    </item>
    <item>
      <title>Re: Clarifications required in SBCFS26 VPRE Regulator Voltage Range</title>
      <link>https://community.nxp.com/t5/Power-Management/Clarifications-required-in-SBCFS26-VPRE-Regulator-Voltage-Range/m-p/2338166#M5085</link>
      <description>Thank you RafaR for providing the clarifications.</description>
      <pubDate>Tue, 24 Mar 2026 06:50:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Clarifications-required-in-SBCFS26-VPRE-Regulator-Voltage-Range/m-p/2338166#M5085</guid>
      <dc:creator>Sivahari</dc:creator>
      <dc:date>2026-03-24T06:50:41Z</dc:date>
    </item>
  </channel>
</rss>