<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックRe: GD3160</title>
    <link>https://community.nxp.com/t5/Power-Management/GD3160/m-p/2332114#M5068</link>
    <description>&lt;P&gt;The &lt;STRONG&gt;24 V&lt;/STRONG&gt; is the stable output from the SMPS power supply for the first step test. However, the real system will be replaced with a battery one. I would like to confirm which supply voltage range is most suitable for the &lt;STRONG&gt;GD3160&lt;/STRONG&gt;.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Since the device includes an internal regulator from &lt;STRONG&gt;VSUP to 5 V&lt;/STRONG&gt;, operating at &lt;STRONG&gt;24 V&lt;/STRONG&gt; will result in higher power dissipation compared to &lt;STRONG&gt;12 V&lt;/STRONG&gt; due to the larger voltage drop across the internal regulator.&lt;/P&gt;&lt;P&gt;Could you please confirm whether using &lt;STRONG&gt;24 V as VSUP&lt;/STRONG&gt; is acceptable from a thermal and reliability standpoint, or if &lt;STRONG&gt;12 V would be a better operating condition&lt;/STRONG&gt; for this device?&lt;/P&gt;</description>
    <pubDate>Fri, 13 Mar 2026 02:39:00 GMT</pubDate>
    <dc:creator>phanit</dc:creator>
    <dc:date>2026-03-13T02:39:00Z</dc:date>
    <item>
      <title>GD3160</title>
      <link>https://community.nxp.com/t5/Power-Management/GD3160/m-p/2332057#M5066</link>
      <description>&lt;P&gt;Hello, I buy and use the GD3160, I used to design with 24V support for pin Vsup. Somehow, it is should recommend 12V support; it is better than 24V, right? Can you explain which one is better? Since this IC allows support up to 40V.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 13 Mar 2026 01:45:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/GD3160/m-p/2332057#M5066</guid>
      <dc:creator>phanit</dc:creator>
      <dc:date>2026-03-13T01:45:39Z</dc:date>
    </item>
    <item>
      <title>Re: GD3160</title>
      <link>https://community.nxp.com/t5/Power-Management/GD3160/m-p/2332108#M5067</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Your 24V input is stable value or typical value when you use GD3160?&lt;/P&gt;</description>
      <pubDate>Fri, 13 Mar 2026 02:34:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/GD3160/m-p/2332108#M5067</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2026-03-13T02:34:17Z</dc:date>
    </item>
    <item>
      <title>Re: GD3160</title>
      <link>https://community.nxp.com/t5/Power-Management/GD3160/m-p/2332114#M5068</link>
      <description>&lt;P&gt;The &lt;STRONG&gt;24 V&lt;/STRONG&gt; is the stable output from the SMPS power supply for the first step test. However, the real system will be replaced with a battery one. I would like to confirm which supply voltage range is most suitable for the &lt;STRONG&gt;GD3160&lt;/STRONG&gt;.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Since the device includes an internal regulator from &lt;STRONG&gt;VSUP to 5 V&lt;/STRONG&gt;, operating at &lt;STRONG&gt;24 V&lt;/STRONG&gt; will result in higher power dissipation compared to &lt;STRONG&gt;12 V&lt;/STRONG&gt; due to the larger voltage drop across the internal regulator.&lt;/P&gt;&lt;P&gt;Could you please confirm whether using &lt;STRONG&gt;24 V as VSUP&lt;/STRONG&gt; is acceptable from a thermal and reliability standpoint, or if &lt;STRONG&gt;12 V would be a better operating condition&lt;/STRONG&gt; for this device?&lt;/P&gt;</description>
      <pubDate>Fri, 13 Mar 2026 02:39:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/GD3160/m-p/2332114#M5068</guid>
      <dc:creator>phanit</dc:creator>
      <dc:date>2026-03-13T02:39:00Z</dc:date>
    </item>
    <item>
      <title>Re: GD3160</title>
      <link>https://community.nxp.com/t5/Power-Management/GD3160/m-p/2332116#M5069</link>
      <description>&lt;P&gt;The&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;24 V&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;is the stable output from the SMPS power supply for the first step test. However, the real system will be replaced with a battery one. I would like to confirm which supply voltage range is most suitable for the&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;GD3160&lt;/STRONG&gt;.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Since the device includes an internal regulator from&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;VSUP to 5 V&lt;/STRONG&gt;, operating at&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;24 V&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;will result in higher power dissipation compared to&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;12 V&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;due to the larger voltage drop across the internal regulator.&lt;/P&gt;&lt;P&gt;Could you please confirm whether using&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;24 V as VSUP&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;is acceptable from a thermal and reliability standpoint, or if&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;12 V would be a better operating condition&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;for this device?&lt;/P&gt;</description>
      <pubDate>Fri, 13 Mar 2026 02:40:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/GD3160/m-p/2332116#M5069</guid>
      <dc:creator>phanit</dc:creator>
      <dc:date>2026-03-13T02:40:50Z</dc:date>
    </item>
    <item>
      <title>Re: GD3160</title>
      <link>https://community.nxp.com/t5/Power-Management/GD3160/m-p/2332122#M5070</link>
      <description>&lt;P&gt;It can be used in 24V but as you said 12V is more suitable.&lt;/P&gt;</description>
      <pubDate>Fri, 13 Mar 2026 02:51:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/GD3160/m-p/2332122#M5070</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2026-03-13T02:51:10Z</dc:date>
    </item>
  </channel>
</rss>