<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FS4500 Watchdog Disable for Reprogramming in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/FS4500-Watchdog-Disable-for-Reprogramming/m-p/2315783#M4992</link>
    <description>&lt;P&gt;Hi Gowoon,&lt;/P&gt;
&lt;P&gt;1.&amp;nbsp;Your current sequence is correct:&lt;/P&gt;
&lt;P&gt;Enter INIT_FS by asserting RSTB_REQ&lt;BR /&gt;Set WD_WINDOW = 0b0000 to disable the watchdog (valid only in INIT_FS)&lt;BR /&gt;Perform one correct watchdog refresh within 256ms&lt;/P&gt;
&lt;P&gt;We also recommend disabling FCCU monitoring to prevent unintended FCCU error detection during programming. This is done by writing IO_23_FS = 0 in the INIT_FSSM register.&lt;/P&gt;
&lt;P&gt;Once programming is complete, issue another RSTB_REQ reset so that the new software starts and the watchdog becomes active again.&lt;/P&gt;
&lt;P&gt;2.&amp;nbsp;Yes, the entire sequence can be repeated at any time.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
    <pubDate>Tue, 10 Feb 2026 17:03:19 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2026-02-10T17:03:19Z</dc:date>
    <item>
      <title>FS4500 Watchdog Disable for Reprogramming</title>
      <link>https://community.nxp.com/t5/Power-Management/FS4500-Watchdog-Disable-for-Reprogramming/m-p/2315546#M4990</link>
      <description>&lt;P&gt;Hi NXP Team,&lt;/P&gt;&lt;P&gt;We are using FS4500 with TC3xx Series.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For using reprogramming, we understand that Watchdog Disable is needed.&lt;/P&gt;&lt;P&gt;Below is the procedure we used.&lt;/P&gt;&lt;P&gt;First, call FS65_RequestReset (setting RSTB_REQ of SF_OUTPUT_REQUEST).&lt;/P&gt;&lt;P&gt;And, send WD_WINDOW to 0000(Disable, in INIT phase only).&lt;/P&gt;&lt;P&gt;Finally, Watchdog Refresh within 256ms.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Question 1: Are there any additional steps required?&lt;/P&gt;&lt;P&gt;Question 2: There are cases where MCU reset is necessary during the reprogramming procedure. In this case, can I use those Steps again?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;GGL.&lt;/P&gt;</description>
      <pubDate>Tue, 10 Feb 2026 11:23:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS4500-Watchdog-Disable-for-Reprogramming/m-p/2315546#M4990</guid>
      <dc:creator>GGLee</dc:creator>
      <dc:date>2026-02-10T11:23:28Z</dc:date>
    </item>
    <item>
      <title>Re: FS4500 Watchdog Disable for Reprogramming</title>
      <link>https://community.nxp.com/t5/Power-Management/FS4500-Watchdog-Disable-for-Reprogramming/m-p/2315783#M4992</link>
      <description>&lt;P&gt;Hi Gowoon,&lt;/P&gt;
&lt;P&gt;1.&amp;nbsp;Your current sequence is correct:&lt;/P&gt;
&lt;P&gt;Enter INIT_FS by asserting RSTB_REQ&lt;BR /&gt;Set WD_WINDOW = 0b0000 to disable the watchdog (valid only in INIT_FS)&lt;BR /&gt;Perform one correct watchdog refresh within 256ms&lt;/P&gt;
&lt;P&gt;We also recommend disabling FCCU monitoring to prevent unintended FCCU error detection during programming. This is done by writing IO_23_FS = 0 in the INIT_FSSM register.&lt;/P&gt;
&lt;P&gt;Once programming is complete, issue another RSTB_REQ reset so that the new software starts and the watchdog becomes active again.&lt;/P&gt;
&lt;P&gt;2.&amp;nbsp;Yes, the entire sequence can be repeated at any time.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
      <pubDate>Tue, 10 Feb 2026 17:03:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS4500-Watchdog-Disable-for-Reprogramming/m-p/2315783#M4992</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2026-02-10T17:03:19Z</dc:date>
    </item>
  </channel>
</rss>