<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックRe: MC33772B's EPAD</title>
    <link>https://community.nxp.com/t5/Power-Management/MC33772B-s-EPAD/m-p/2315015#M4988</link>
    <description>&lt;P&gt;I already know your answer, but what I really want to understand is why the opened metal area on the bottom side of the MC33772 is 5.4 mm.&lt;/P&gt;&lt;P&gt;According to the application note, the solder opening area is 3.7 mm, but the device’s bottom-side metal area is 5.4 mm. Why is there a difference?&lt;/P&gt;&lt;P&gt;According to the datasheet, the 3.7 mm to 5.4 mm region is specified as a routing keep-out zone.&lt;/P&gt;&lt;P&gt;Given that, I would like to understand why this same 3.7–5.4 mm area is exposed as open metal on the bottom side of the device.&lt;/P&gt;</description>
    <pubDate>Tue, 10 Feb 2026 00:27:09 GMT</pubDate>
    <dc:creator>JakeJung</dc:creator>
    <dc:date>2026-02-10T00:27:09Z</dc:date>
    <item>
      <title>MC33772B's EPAD</title>
      <link>https://community.nxp.com/t5/Power-Management/MC33772B-s-EPAD/m-p/2304316#M4974</link>
      <description>&lt;P&gt;On the bottom side of the MC33772B, there is a 5.4 mm × 5.4 mm exposed metal area.&lt;/P&gt;&lt;P&gt;However, the PCB design guide recommends a solder mask opening of only 3.7–3.8 mm, which suggests an EPAD size of about 3.7 mm.&lt;/P&gt;&lt;P&gt;In actual inspection, the exposed metal area on the IC bottom is 5.4 mm, which is larger than the recommended PCB opening.&lt;/P&gt;&lt;P&gt;According to the datasheet, the region from 3.7 mm (min) to 5.4 mm (max) is specified as a PCB routing keep-out area.&lt;/P&gt;&lt;P&gt;If 3.7 mm is the recommended EPAD size and the 3.7–5.4 mm region is defined as a PCB routing keep-out area, what is the reason that this whole region is designed as exposed metal on the bottom side of the package?&lt;/P&gt;</description>
      <pubDate>Mon, 02 Feb 2026 00:37:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/MC33772B-s-EPAD/m-p/2304316#M4974</guid>
      <dc:creator>JakeJung</dc:creator>
      <dc:date>2026-02-02T00:37:55Z</dc:date>
    </item>
    <item>
      <title>Re: MC33772B's EPAD</title>
      <link>https://community.nxp.com/t5/Power-Management/MC33772B-s-EPAD/m-p/2304364#M4975</link>
      <description>&lt;P&gt;You can read more PCB design for exposed pad from page 12 below link file.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true" target="_blank"&gt;AN4388: Quad Flat Package (QFP) – Application Note&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;5.2 Solder stencil and solder paste&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 02 Feb 2026 03:18:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/MC33772B-s-EPAD/m-p/2304364#M4975</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2026-02-02T03:18:35Z</dc:date>
    </item>
    <item>
      <title>Re: MC33772B's EPAD</title>
      <link>https://community.nxp.com/t5/Power-Management/MC33772B-s-EPAD/m-p/2315015#M4988</link>
      <description>&lt;P&gt;I already know your answer, but what I really want to understand is why the opened metal area on the bottom side of the MC33772 is 5.4 mm.&lt;/P&gt;&lt;P&gt;According to the application note, the solder opening area is 3.7 mm, but the device’s bottom-side metal area is 5.4 mm. Why is there a difference?&lt;/P&gt;&lt;P&gt;According to the datasheet, the 3.7 mm to 5.4 mm region is specified as a routing keep-out zone.&lt;/P&gt;&lt;P&gt;Given that, I would like to understand why this same 3.7–5.4 mm area is exposed as open metal on the bottom side of the device.&lt;/P&gt;</description>
      <pubDate>Tue, 10 Feb 2026 00:27:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/MC33772B-s-EPAD/m-p/2315015#M4988</guid>
      <dc:creator>JakeJung</dc:creator>
      <dc:date>2026-02-10T00:27:09Z</dc:date>
    </item>
  </channel>
</rss>