<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FS26 VPRE, VBOS malfunction in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/FS26-VPRE-VBOS-malfunction/m-p/2195236#M4760</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;we made a design for a customer with the FS26 and the S32K344. Everything worked and we passed the EMI tests. But now during tests in the field, we have FS26 PMICs that have a&amp;nbsp;malfunction and as a result, the uC doesn't work anymore. We use it in a 24V System and have a TVS Diode and an Ideal Diode Controller to protect the input from spikes.&lt;/P&gt;&lt;P&gt;On several boards we see that the VPRE regulator has a malfunction and the voltage just reaches between 4,2V to 4,7V, but it must be 6V. Also VBOS has a too low voltage. In the picture you can see the startup of the VPRE buck converter at 24V, which looks very different to a good PMIC, and the resulting voltage of about 4,2V at the end.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We thought that the damage comes from voltage spikes on the input voltage, but after some measurements it looks like no spike passes the protection circuits.&lt;/P&gt;&lt;P&gt;It could also be that the VPRE voltage is too low, because the internal LDO for VBOS (4,1V) is destroyed and is the result of the defect VBOS LDO.&lt;/P&gt;&lt;P&gt;We have a 1uF capacitor on the VBOS output, which is smaller than the recommended size (4,7uF), but 1uF is also used in some reference designs.&lt;/P&gt;&lt;P&gt;I will also attach a part of the PMIC circuit, maybe we made something wrong there.&lt;/P&gt;&lt;P&gt;Do you have any idea what could be the cause for the issue or have you seen any comparable issues?&lt;/P&gt;&lt;P&gt;We also replaced the PMIC on one board, to be sure that the error comes from the PMIC and afterwards the system booted normal.&lt;/P&gt;&lt;P&gt;Thanks for your help!&lt;/P&gt;</description>
    <pubDate>Wed, 29 Oct 2025 15:49:49 GMT</pubDate>
    <dc:creator>__markus__</dc:creator>
    <dc:date>2025-10-29T15:49:49Z</dc:date>
    <item>
      <title>FS26 VPRE, VBOS malfunction</title>
      <link>https://community.nxp.com/t5/Power-Management/FS26-VPRE-VBOS-malfunction/m-p/2195236#M4760</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;we made a design for a customer with the FS26 and the S32K344. Everything worked and we passed the EMI tests. But now during tests in the field, we have FS26 PMICs that have a&amp;nbsp;malfunction and as a result, the uC doesn't work anymore. We use it in a 24V System and have a TVS Diode and an Ideal Diode Controller to protect the input from spikes.&lt;/P&gt;&lt;P&gt;On several boards we see that the VPRE regulator has a malfunction and the voltage just reaches between 4,2V to 4,7V, but it must be 6V. Also VBOS has a too low voltage. In the picture you can see the startup of the VPRE buck converter at 24V, which looks very different to a good PMIC, and the resulting voltage of about 4,2V at the end.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We thought that the damage comes from voltage spikes on the input voltage, but after some measurements it looks like no spike passes the protection circuits.&lt;/P&gt;&lt;P&gt;It could also be that the VPRE voltage is too low, because the internal LDO for VBOS (4,1V) is destroyed and is the result of the defect VBOS LDO.&lt;/P&gt;&lt;P&gt;We have a 1uF capacitor on the VBOS output, which is smaller than the recommended size (4,7uF), but 1uF is also used in some reference designs.&lt;/P&gt;&lt;P&gt;I will also attach a part of the PMIC circuit, maybe we made something wrong there.&lt;/P&gt;&lt;P&gt;Do you have any idea what could be the cause for the issue or have you seen any comparable issues?&lt;/P&gt;&lt;P&gt;We also replaced the PMIC on one board, to be sure that the error comes from the PMIC and afterwards the system booted normal.&lt;/P&gt;&lt;P&gt;Thanks for your help!&lt;/P&gt;</description>
      <pubDate>Wed, 29 Oct 2025 15:49:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS26-VPRE-VBOS-malfunction/m-p/2195236#M4760</guid>
      <dc:creator>__markus__</dc:creator>
      <dc:date>2025-10-29T15:49:49Z</dc:date>
    </item>
    <item>
      <title>Re: FS26 VPRE, VBOS malfunction</title>
      <link>https://community.nxp.com/t5/Power-Management/FS26-VPRE-VBOS-malfunction/m-p/2199176#M4762</link>
      <description>&lt;P&gt;Hello __markus__&lt;/P&gt;
&lt;P&gt;Good day!&lt;/P&gt;
&lt;P&gt;I'm working on finding the error; I'll contact you soon as I determine the reason for the failure.&lt;/P&gt;
&lt;P&gt;Have a great day and best of luck.&lt;/P&gt;</description>
      <pubDate>Wed, 05 Nov 2025 16:15:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS26-VPRE-VBOS-malfunction/m-p/2199176#M4762</guid>
      <dc:creator>RafaR</dc:creator>
      <dc:date>2025-11-05T16:15:43Z</dc:date>
    </item>
    <item>
      <title>Re: FS26 VPRE, VBOS malfunction</title>
      <link>https://community.nxp.com/t5/Power-Management/FS26-VPRE-VBOS-malfunction/m-p/2201037#M4764</link>
      <description>&lt;P&gt;Hello __markus__&lt;/P&gt;
&lt;P&gt;Good day!&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I apologize for the delay.&lt;/P&gt;
&lt;P&gt;Are you using the FS26 at 24V system with only a TVS protection and without a DCDC in front, right ?&amp;nbsp; If yes, this is not recommended, please see below in AN13850, a DCDC is must for 24V application as FS26 is a 12V SBC, whose nominal voltage range is 18V max. it is not recommended to use FS26 working at 24V for a long time.&lt;/P&gt;
&lt;P&gt;VBOS normal voltage output is 5V, 4.1V is too low. I suppose VBOS has external overstress. 4.7uF VBOS output capacitor is must for VBOS.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;In addition, can you check boot_pre capacitor used in the board ? 100nF is preferred.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="RafaR_0-1762544509170.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/364489i82612C9B0DCC196A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="RafaR_0-1762544509170.png" alt="RafaR_0-1762544509170.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;RafaR_0-1762544509170.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope this information has helped you, please let me know if you need help with anything else.&lt;/P&gt;
&lt;P&gt;Have a great day and best of luck.&lt;/P&gt;</description>
      <pubDate>Fri, 07 Nov 2025 19:42:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS26-VPRE-VBOS-malfunction/m-p/2201037#M4764</guid>
      <dc:creator>RafaR</dc:creator>
      <dc:date>2025-11-07T19:42:28Z</dc:date>
    </item>
    <item>
      <title>Re: FS26 VPRE, VBOS malfunction</title>
      <link>https://community.nxp.com/t5/Power-Management/FS26-VPRE-VBOS-malfunction/m-p/2299326#M4968</link>
      <description>&lt;P&gt;Hello RafaR,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks for the feedback. We are making a redesign and are implementing a buck converter in front of the PMIC.&lt;/P&gt;&lt;P&gt;As we still want to use the boost converter in a front-end configuration, is there a solution to use both, front-end converter and the buck converter on the input?&lt;/P&gt;&lt;P&gt;E.g. by using a diode to protect the buck converter or what is the exact reason, why this is not possible?&lt;/P&gt;&lt;P&gt;I've seen the hint in the AN that it must be used in back-end, but maybe there exists a solution.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And are there any other thinks we have to take care of when using the PMIC in a 24V system?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your help and best regards,&lt;/P&gt;&lt;P&gt;Markus&lt;/P&gt;</description>
      <pubDate>Fri, 23 Jan 2026 14:23:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS26-VPRE-VBOS-malfunction/m-p/2299326#M4968</guid>
      <dc:creator>__markus__</dc:creator>
      <dc:date>2026-01-23T14:23:06Z</dc:date>
    </item>
    <item>
      <title>Re: FS26 VPRE, VBOS malfunction</title>
      <link>https://community.nxp.com/t5/Power-Management/FS26-VPRE-VBOS-malfunction/m-p/2301309#M4971</link>
      <description>&lt;P&gt;For clarification, we want to use the ECU for 12V and 24V Systems, that's the reason why the cold crank feature with the front-end boost converter for 12V should still be available. We don't have enough space to use a buck-boost in front of the PMIC and also the changes in the layout would be severe.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Markus&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jan 2026 11:30:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS26-VPRE-VBOS-malfunction/m-p/2301309#M4971</guid>
      <dc:creator>__markus__</dc:creator>
      <dc:date>2026-01-27T11:30:24Z</dc:date>
    </item>
  </channel>
</rss>