<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: AN1902 QFN Footprint Guidelines in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/AN1902-QFN-Footprint-Guidelines/m-p/2192625#M4757</link>
    <description>&lt;P&gt;Hello JimBKHS&lt;/P&gt;
&lt;P&gt;Good day!&lt;/P&gt;
&lt;P&gt;Yes, your analysis sounds good. As you mentioned, it may vary depending on the component, process used, etc.&lt;/P&gt;
&lt;P&gt;But I think you've captured the most important points to consider.&lt;/P&gt;
&lt;P&gt;Have a great day and best of luck.&lt;/P&gt;</description>
    <pubDate>Fri, 24 Oct 2025 15:36:05 GMT</pubDate>
    <dc:creator>RafaR</dc:creator>
    <dc:date>2025-10-24T15:36:05Z</dc:date>
    <item>
      <title>AN1902 QFN Footprint Guidelines</title>
      <link>https://community.nxp.com/t5/Power-Management/AN1902-QFN-Footprint-Guidelines/m-p/2188416#M4745</link>
      <description>&lt;P&gt;I'm reviewing &lt;A href="https://www.nxp.com/docs/en/application-note/AN1902.pdf" target="_self"&gt;AN1902&lt;/A&gt; on QFN and SON package assembly guidelines and had a specific question about thermal via recommendations. I'm specifically reviewing what to do with thermal vias placed within the exposed pads of these package footprints.&lt;/P&gt;&lt;P&gt;I always thought it was best to UNTENT thermal vias placed within the exposed die pad on the opposite solder mask side, as tenting them would realistically trap a void of air within the via itself and lead to PCB damage during thermal cycles of the assembly. However, page 16 of the app note recommends this:&lt;BR /&gt;&lt;BR /&gt;"If the copper plating does not plug the vias, then the thermal vias can be “tented” with&lt;BR /&gt;solder mask on the top surface of the PCB to avoid solder wicking inside the via during&lt;BR /&gt;assembly. The solder mask diameter should be at least 0.10 mm larger than the via&lt;BR /&gt;diameter."&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So it sounds like the primary goal is to tent the back side of the thermal vias to limit solder reflow into these vias, but with the vias tented won't a void of air (albeit small) be trapped in the via itself? Can't this cause other issues?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 17 Oct 2025 16:01:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/AN1902-QFN-Footprint-Guidelines/m-p/2188416#M4745</guid>
      <dc:creator>JimBKHS</dc:creator>
      <dc:date>2025-10-17T16:01:23Z</dc:date>
    </item>
    <item>
      <title>Re: AN1902 QFN Footprint Guidelines</title>
      <link>https://community.nxp.com/t5/Power-Management/AN1902-QFN-Footprint-Guidelines/m-p/2192038#M4755</link>
      <description>&lt;P&gt;Hello JimBKHS&lt;/P&gt;
&lt;P&gt;Good day!&lt;/P&gt;
&lt;P&gt;The recommendation in AN1902 to tent thermal vias on the top side (component side) is primarily to prevent solder wicking during reflow.&lt;/P&gt;
&lt;P&gt;Your concern about trapped air in shielded vias is valid. However, modern solder mask materials and via shielding techniques are designed to minimize this risk. The void is typically very small and unlikely to cause damage unless the via is large or the board is under extreme thermal stress.&lt;/P&gt;
&lt;P&gt;Usually, each company that manufactures PCB already has its own methods and practices to minimize this risk.&lt;/P&gt;
&lt;P&gt;As extra note:&lt;/P&gt;
&lt;P&gt;If possible, use via fill and cap plating (IPC-4761 Type VII) to completely seal the via. This avoids both solder wicking and air entrapment.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope this information has helped you, please let me know if you need help with anything else.&lt;/P&gt;
&lt;P&gt;Have a great day and best of luck.&lt;/P&gt;</description>
      <pubDate>Fri, 24 Oct 2025 00:15:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/AN1902-QFN-Footprint-Guidelines/m-p/2192038#M4755</guid>
      <dc:creator>RafaR</dc:creator>
      <dc:date>2025-10-24T00:15:20Z</dc:date>
    </item>
    <item>
      <title>Re: AN1902 QFN Footprint Guidelines</title>
      <link>https://community.nxp.com/t5/Power-Management/AN1902-QFN-Footprint-Guidelines/m-p/2192583#M4756</link>
      <description>&lt;P&gt;Thanks&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242156"&gt;@RafaR&lt;/a&gt;&amp;nbsp;I think I was misunderstanding the via tenting, and thought the app note was suggesting tenting on the OPPOSITE of component side, which would definitely trap air voids.&lt;/P&gt;&lt;P&gt;So it looks like the overall thermal via recommendation from this app note is (obviously component, supplier recommendation and process dependent)&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Use a 1.2mm grid array of vias&lt;/LI&gt;&lt;LI&gt;Which are sized 0.3 to 0.33mm in hole diameter&lt;/LI&gt;&lt;LI&gt;Plated to 1oz copper&lt;/LI&gt;&lt;LI&gt;And optionally tented on the component side with mask at a diameter +0.1mm larger than the hole size&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Correct?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 24 Oct 2025 14:09:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/AN1902-QFN-Footprint-Guidelines/m-p/2192583#M4756</guid>
      <dc:creator>JimBKHS</dc:creator>
      <dc:date>2025-10-24T14:09:22Z</dc:date>
    </item>
    <item>
      <title>Re: AN1902 QFN Footprint Guidelines</title>
      <link>https://community.nxp.com/t5/Power-Management/AN1902-QFN-Footprint-Guidelines/m-p/2192625#M4757</link>
      <description>&lt;P&gt;Hello JimBKHS&lt;/P&gt;
&lt;P&gt;Good day!&lt;/P&gt;
&lt;P&gt;Yes, your analysis sounds good. As you mentioned, it may vary depending on the component, process used, etc.&lt;/P&gt;
&lt;P&gt;But I think you've captured the most important points to consider.&lt;/P&gt;
&lt;P&gt;Have a great day and best of luck.&lt;/P&gt;</description>
      <pubDate>Fri, 24 Oct 2025 15:36:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/AN1902-QFN-Footprint-Guidelines/m-p/2192625#M4757</guid>
      <dc:creator>RafaR</dc:creator>
      <dc:date>2025-10-24T15:36:05Z</dc:date>
    </item>
  </channel>
</rss>