<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックPF5030 read I2C while all output lost</title>
    <link>https://community.nxp.com/t5/Power-Management/PF5030-read-I2C-while-all-output-lost/m-p/2174180#M4700</link>
    <description>&lt;P&gt;Hi, when a fatal error occurs, all outputs of the PF5030 are lost while the input power remains present. Is there any way to retrieve detailed fault information via I2C?&lt;/P&gt;&lt;P&gt;The VDDIO is supplied from one of its outputs. In this situation, VDDIO is lost, so the I2C interface may not function. But what if I provide an external VDDIO after the fatal error occurs?&lt;/P&gt;&lt;P&gt;Will the error message still be retained or will it already be lost? Can I retrieve the error reason by supplying external VDDIO after the error happened and attempting I2C communication?&lt;/P&gt;</description>
    <pubDate>Tue, 23 Sep 2025 09:26:44 GMT</pubDate>
    <dc:creator>Pony_Ma</dc:creator>
    <dc:date>2025-09-23T09:26:44Z</dc:date>
    <item>
      <title>PF5030 read I2C while all output lost</title>
      <link>https://community.nxp.com/t5/Power-Management/PF5030-read-I2C-while-all-output-lost/m-p/2174180#M4700</link>
      <description>&lt;P&gt;Hi, when a fatal error occurs, all outputs of the PF5030 are lost while the input power remains present. Is there any way to retrieve detailed fault information via I2C?&lt;/P&gt;&lt;P&gt;The VDDIO is supplied from one of its outputs. In this situation, VDDIO is lost, so the I2C interface may not function. But what if I provide an external VDDIO after the fatal error occurs?&lt;/P&gt;&lt;P&gt;Will the error message still be retained or will it already be lost? Can I retrieve the error reason by supplying external VDDIO after the error happened and attempting I2C communication?&lt;/P&gt;</description>
      <pubDate>Tue, 23 Sep 2025 09:26:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF5030-read-I2C-while-all-output-lost/m-p/2174180#M4700</guid>
      <dc:creator>Pony_Ma</dc:creator>
      <dc:date>2025-09-23T09:26:44Z</dc:date>
    </item>
    <item>
      <title>Re: PF5030 read I2C while all output lost</title>
      <link>https://community.nxp.com/t5/Power-Management/PF5030-read-I2C-while-all-output-lost/m-p/2174255#M4702</link>
      <description>&lt;P&gt;&lt;FONT size="3"&gt;Hi Pony,&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;FONT size="3"&gt;When a fatal error occurs (e.g., watchdog failure, overvoltage on monitored rails, or fault counter overflow), the PF5030 transitions into DEEP-FS state.&lt;/FONT&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;FONT size="3"&gt;In DEEP-FS, all regulators are turned off.&amp;nbsp;&lt;/FONT&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;FONT size="3"&gt;The fail-safe logic remains powered internally from VIN&lt;/FONT&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;FONT size="3"&gt;The I²C interface is in the fail-safe domain and becomes functional again once VDDIO is present (1.71 V to 5.25 V range).&lt;/FONT&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;FONT size="3"&gt;as long as VIN remains above the POR threshold and the device has not been power-cycled, the fail-safe registers (e.g., &lt;CODE&gt;FS_GRL_FLAGS&lt;/CODE&gt;, &lt;CODE&gt;FS_OVUVREG_STATUS1&lt;/CODE&gt;, &lt;CODE&gt;FS_DIAG_SAFETY&lt;/CODE&gt;, &lt;CODE&gt;FS_STATES&lt;/CODE&gt;) will still contain:&lt;/FONT&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;FONT size="3"&gt;Which voltage monitor triggered (OV/UV flags)&lt;/FONT&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;FONT size="3"&gt;Watchdog error flags&lt;/FONT&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;FONT size="3"&gt;Fault counters and state machine status&lt;/FONT&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;/LI&gt;
&lt;LI&gt;&lt;FONT size="3"&gt;These registers are cleared only by POR or explicit writes, not by entering DEEP-FS&lt;/FONT&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;FONT size="3"&gt;&lt;CODE&gt;FS_GRL_FLAGS&lt;/CODE&gt; (general fault summary)&lt;/FONT&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;FONT size="3"&gt;&lt;CODE&gt;FS_OVUVREG_STATUS1&lt;/CODE&gt; (which VMON triggered)&lt;/FONT&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;FONT size="3"&gt;&lt;CODE&gt;FS_DIAG_SAFETY&lt;/CODE&gt; (watchdog, CRC, BIST status)&lt;/FONT&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;FONT size="3"&gt;&lt;CODE&gt;FS_STATES&lt;/CODE&gt; (current fail-safe state)&lt;/FONT&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;FONT size="3"&gt;You can recover detailed fault information after a fatal error by externally powering VDDIO, provided VIN was never lost. If VIN drops below POR, all volatile registers are cleared.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Sep 2025 10:38:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF5030-read-I2C-while-all-output-lost/m-p/2174255#M4702</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2025-09-23T10:38:27Z</dc:date>
    </item>
  </channel>
</rss>