<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SDA pull down in PF4210 &amp; PF0100   in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/SDA-pull-down-in-PF4210-PF0100/m-p/936996#M469</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ws&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;I have no access to look through the internal circuit, &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/anandkumarbalakrishnan"&gt;anandkumarbalakrishnan&lt;/A&gt;‌, do you have any idea about this "issue"?&lt;/P&gt;&lt;P&gt;BRs&lt;/P&gt;&lt;P&gt;jinyu&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Aug 2019 02:00:40 GMT</pubDate>
    <dc:creator>jinyuzhang</dc:creator>
    <dc:date>2019-08-13T02:00:40Z</dc:date>
    <item>
      <title>SDA pull down in PF4210 &amp; PF0100</title>
      <link>https://community.nxp.com/t5/Power-Management/SDA-pull-down-in-PF4210-PF0100/m-p/936993#M466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Team, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Customer found SDA pin of PMIC PF4210 keep in low status&amp;nbsp;when&amp;nbsp;VDDIO&amp;nbsp;is supplied (VDDIO =3.3V) but&amp;nbsp;without VIN (VIN = 0V).&amp;nbsp;There is no&amp;nbsp;such issue in SCL pin and it can pull up with VDDIO only.&amp;nbsp;Both SCL and&amp;nbsp;SDA pin&amp;nbsp;are pull up to VDDIO with 4.7K resistors.&amp;nbsp;If&amp;nbsp;VIN&amp;nbsp;is supplied (3.3V), the SDA status can&amp;nbsp;pull up&amp;nbsp;to VDDIO level and that status&amp;nbsp;can keep &amp;nbsp;even after&amp;nbsp;VIN&amp;nbsp;is turn off.&amp;nbsp;Same result can be&amp;nbsp;found in both PF4210 EVK and customer board. &amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That issue&amp;nbsp;affect other slave devices on the same I2C bus cannot&amp;nbsp;be&amp;nbsp;communicate if supply does not provide to PMIC VIN. &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Similar&amp;nbsp;symptom can also be&amp;nbsp;measured in PF0100 EVB.&amp;nbsp;Is that symptom normal?&amp;nbsp;&amp;nbsp;Does VIN must power for the I2C interface/SDA level stable setup to open-drain pull up?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the application that other slave devices need share&amp;nbsp;the I2C interface/bus with the PMIC (but no need PMIC to work), customer try workaround&amp;nbsp;by&amp;nbsp;power&amp;nbsp;up VIN once, then power it down&amp;nbsp;and only keep VDDIO supply.&amp;nbsp;Is that workaround reliable and&amp;nbsp;What is the suitable&amp;nbsp;workaround for that issue case? &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can we&amp;nbsp;share the&amp;nbsp;internal block diagram of the I2C interface of PMIC&amp;nbsp;to explain that symptom. &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Best Regards,&lt;/P&gt;&lt;P&gt;WS&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Aug 2019 06:03:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/SDA-pull-down-in-PF4210-PF0100/m-p/936993#M466</guid>
      <dc:creator>wswong</dc:creator>
      <dc:date>2019-08-01T06:03:35Z</dc:date>
    </item>
    <item>
      <title>Re: SDA pull down in PF4210 &amp; PF0100</title>
      <link>https://community.nxp.com/t5/Power-Management/SDA-pull-down-in-PF4210-PF0100/m-p/936994#M467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ws&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I have checked on EVB , and the result is the same to you. this is not a good&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;symptom, but we can't regard it as a bug. as when there is no VIn ,Vdig has no output and there is no voltage to control the internal MOS, most of circuit is Floating status, and then if there is a pull up for SDA , the Open Drain mos of SDA may be turned on. I test the leakage current , it is about 600uA, and it seems like the MOS is turned on.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;nbsp; &amp;nbsp; The thing we can do just recommend customer to keep VIN on when VDDIO is on,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;BRs&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;jinyu&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Aug 2019 06:44:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/SDA-pull-down-in-PF4210-PF0100/m-p/936994#M467</guid>
      <dc:creator>jinyuzhang</dc:creator>
      <dc:date>2019-08-12T06:44:04Z</dc:date>
    </item>
    <item>
      <title>Re: SDA pull down in PF4210 &amp; PF0100</title>
      <link>https://community.nxp.com/t5/Power-Management/SDA-pull-down-in-PF4210-PF0100/m-p/936995#M468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jinyu,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your update and we can recommend customer to keep VIN on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any internal block/circuit diagram can help us descript that operation?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Best Regards,&lt;/P&gt;&lt;P&gt;WS&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Aug 2019 13:48:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/SDA-pull-down-in-PF4210-PF0100/m-p/936995#M468</guid>
      <dc:creator>wswong</dc:creator>
      <dc:date>2019-08-12T13:48:38Z</dc:date>
    </item>
    <item>
      <title>Re: SDA pull down in PF4210 &amp; PF0100</title>
      <link>https://community.nxp.com/t5/Power-Management/SDA-pull-down-in-PF4210-PF0100/m-p/936996#M469</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ws&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;I have no access to look through the internal circuit, &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/anandkumarbalakrishnan"&gt;anandkumarbalakrishnan&lt;/A&gt;‌, do you have any idea about this "issue"?&lt;/P&gt;&lt;P&gt;BRs&lt;/P&gt;&lt;P&gt;jinyu&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Aug 2019 02:00:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/SDA-pull-down-in-PF4210-PF0100/m-p/936996#M469</guid>
      <dc:creator>jinyuzhang</dc:creator>
      <dc:date>2019-08-13T02:00:40Z</dc:date>
    </item>
  </channel>
</rss>