<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FS6500 Watchdog in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/FS6500-Watchdog/m-p/2166067#M4680</link>
    <description>&lt;P&gt;If the duty cycle is not 50% then how will be the window period duration looks like when compared to "Table 18. WD_WINDOW". For example, if we set 0011b in WD_WINDOW then the Window period duration can be as low as 2.7ms and as high as 3.3ms when duty cycle is not 50%. In this case does the OPEN &amp;amp; CLOSED windows is still equally divided? A bit confused with the FS CLK accuracy image it seems like the red and blue period is having equal open &amp;amp; closed window period.&lt;/P&gt;</description>
    <pubDate>Tue, 09 Sep 2025 17:08:09 GMT</pubDate>
    <dc:creator>Nixon66</dc:creator>
    <dc:date>2025-09-09T17:08:09Z</dc:date>
    <item>
      <title>FS6500 Watchdog</title>
      <link>https://community.nxp.com/t5/Power-Management/FS6500-Watchdog/m-p/1187901#M1259</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using FS6500 in out project application. Could you please let me know the timing parameters of watchdog signal. Is it entirely software configurable?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 24 Nov 2020 06:23:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS6500-Watchdog/m-p/1187901#M1259</guid>
      <dc:creator>AnneVilasini</dc:creator>
      <dc:date>2020-11-24T06:23:24Z</dc:date>
    </item>
    <item>
      <title>Re: FS6500 Watchdog</title>
      <link>https://community.nxp.com/t5/Power-Management/FS6500-Watchdog/m-p/1188070#M1260</link>
      <description>&lt;P&gt;Hi Anne,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The Watchdog Window Period is configurable by SW. Not only during the INIT_FS phase (first 256ms after RSTB is released), but also later during the Normal mode.&lt;/P&gt;
&lt;P&gt;By default, WD Window duration is 3ms&amp;nbsp; which is in alignment with an FTTI below 10ms.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="WD WINDOW.JPG" style="width: 710px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/130838iB125CAA585251D98/image-size/large?v=v2&amp;amp;px=999" role="button" title="WD WINDOW.JPG" alt="WD WINDOW.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The Watchdog Window Duty Cycle is set to 50% ±10% and is not modifiable.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="WD Refresh Slot.JPG" style="width: 461px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/130841i5E5259FE95E20090/image-size/large?v=v2&amp;amp;px=999" role="button" title="WD Refresh Slot.JPG" alt="WD Refresh Slot.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;</description>
      <pubDate>Tue, 24 Nov 2020 09:49:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS6500-Watchdog/m-p/1188070#M1260</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2020-11-24T09:49:20Z</dc:date>
    </item>
    <item>
      <title>Re: FS6500 Watchdog</title>
      <link>https://community.nxp.com/t5/Power-Management/FS6500-Watchdog/m-p/1190725#M1266</link>
      <description>&lt;P&gt;Thank you Tomas!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you please let me know the following data :&lt;/P&gt;&lt;P&gt;1. Time taken by the watchdog timer to detect a rising and falling edge&lt;/P&gt;&lt;P&gt;2. Reset time and reset cycle duration&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 30 Nov 2020 07:48:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS6500-Watchdog/m-p/1190725#M1266</guid>
      <dc:creator>AnneVilasini</dc:creator>
      <dc:date>2020-11-30T07:48:52Z</dc:date>
    </item>
    <item>
      <title>Re: FS6500 Watchdog</title>
      <link>https://community.nxp.com/t5/Power-Management/FS6500-Watchdog/m-p/2166067#M4680</link>
      <description>&lt;P&gt;If the duty cycle is not 50% then how will be the window period duration looks like when compared to "Table 18. WD_WINDOW". For example, if we set 0011b in WD_WINDOW then the Window period duration can be as low as 2.7ms and as high as 3.3ms when duty cycle is not 50%. In this case does the OPEN &amp;amp; CLOSED windows is still equally divided? A bit confused with the FS CLK accuracy image it seems like the red and blue period is having equal open &amp;amp; closed window period.&lt;/P&gt;</description>
      <pubDate>Tue, 09 Sep 2025 17:08:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS6500-Watchdog/m-p/2166067#M4680</guid>
      <dc:creator>Nixon66</dc:creator>
      <dc:date>2025-09-09T17:08:09Z</dc:date>
    </item>
  </channel>
</rss>