<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Over Temperature Issue on 50XS4200 in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/Over-Temperature-Issue-on-50XS4200/m-p/2130513#M4482</link>
    <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;I am Working on MC50XS4200 High-side switch. I am trying to implement auto retry function as I am getting hit with over current issue. The Auto retry is also keep on failing. Current limit is 15. Upon further investigation I found it to be Overtemperature fault setting in added to that. According to data sheet OT will set only when Junction temperature is above 175 degrees. I could see the OT = OD2 setting in. But I am not sure the junction temperature will be that much to hit OT. So I wanted to check is it any other way this OT can set in.&lt;/P&gt;&lt;P&gt;1. Like because of retries or any other factor.&lt;/P&gt;&lt;P&gt;2. Also wanted to understand can it be caused due to Over current. if so, is there any value for that eg. Over current XX A at XX sec can cause the issue.&lt;/P&gt;&lt;P&gt;3. Is there any current and time graph you have related to this if over current can cause this issue.&lt;/P&gt;</description>
    <pubDate>Wed, 09 Jul 2025 02:50:03 GMT</pubDate>
    <dc:creator>GuruPrakashR</dc:creator>
    <dc:date>2025-07-09T02:50:03Z</dc:date>
    <item>
      <title>Over Temperature Issue on 50XS4200</title>
      <link>https://community.nxp.com/t5/Power-Management/Over-Temperature-Issue-on-50XS4200/m-p/2130513#M4482</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;I am Working on MC50XS4200 High-side switch. I am trying to implement auto retry function as I am getting hit with over current issue. The Auto retry is also keep on failing. Current limit is 15. Upon further investigation I found it to be Overtemperature fault setting in added to that. According to data sheet OT will set only when Junction temperature is above 175 degrees. I could see the OT = OD2 setting in. But I am not sure the junction temperature will be that much to hit OT. So I wanted to check is it any other way this OT can set in.&lt;/P&gt;&lt;P&gt;1. Like because of retries or any other factor.&lt;/P&gt;&lt;P&gt;2. Also wanted to understand can it be caused due to Over current. if so, is there any value for that eg. Over current XX A at XX sec can cause the issue.&lt;/P&gt;&lt;P&gt;3. Is there any current and time graph you have related to this if over current can cause this issue.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jul 2025 02:50:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Over-Temperature-Issue-on-50XS4200/m-p/2130513#M4482</guid>
      <dc:creator>GuruPrakashR</dc:creator>
      <dc:date>2025-07-09T02:50:03Z</dc:date>
    </item>
    <item>
      <title>Re: Over Temperature Issue on 50XS4200</title>
      <link>https://community.nxp.com/t5/Power-Management/Over-Temperature-Issue-on-50XS4200/m-p/2130575#M4483</link>
      <description>&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;Your MC50XS4200 high-side switch is likely hitting an overtemperature (OT) fault, even if the steady-state junction temperature isn't usually 175°C, because repeated overcurrent auto-retries cause significant power dissipation, leading to a cumulative rise in junction temperature. Each retry generates heat (I&lt;BR /&gt;2&lt;BR /&gt;×R&lt;BR /&gt;DS(on)&lt;BR /&gt;​&lt;BR /&gt;), and insufficient cool-down time between attempts can quickly push the die temperature past the OT threshold. Overcurrent is the primary cause of this heating; while there's no fixed "XX A at XX sec" value due to varying thermal impedances and ambient conditions, the datasheet's thermal characteristics (like R&lt;BR /&gt;thJA&lt;BR /&gt;​&lt;BR /&gt;, R&lt;BR /&gt;thJC&lt;BR /&gt;​&lt;BR /&gt;, and transient thermal impedance curves) are crucial for understanding this dynamic, as they explain how current spikes translate into rapid temperature increases.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jul 2025 05:03:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Over-Temperature-Issue-on-50XS4200/m-p/2130575#M4483</guid>
      <dc:creator>Bonnie219Bailey</dc:creator>
      <dc:date>2025-07-09T05:03:20Z</dc:date>
    </item>
    <item>
      <title>Re: Over Temperature Issue on 50XS4200</title>
      <link>https://community.nxp.com/t5/Power-Management/Over-Temperature-Issue-on-50XS4200/m-p/2130668#M4486</link>
      <description>Understood. In that case how to mitigate this problem. Is there any solution. where can i access any material or detail regarding this. Because of this OT I couldn't make auto retry work. Then system is goes offline totally.</description>
      <pubDate>Wed, 09 Jul 2025 06:59:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Over-Temperature-Issue-on-50XS4200/m-p/2130668#M4486</guid>
      <dc:creator>GuruPrakashR</dc:creator>
      <dc:date>2025-07-09T06:59:03Z</dc:date>
    </item>
  </channel>
</rss>