<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TEA2016  LLC-Half-bridge failure in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/TEA2016-LLC-Half-bridge-failure/m-p/2095247#M4348</link>
    <description>Hi&lt;BR /&gt;May I have a look at your schematic diagram and PCB layout.&lt;BR /&gt;At that time, my problem was caused by the feedback loop and the SNSCAP loop.</description>
    <pubDate>Mon, 12 May 2025 07:18:22 GMT</pubDate>
    <dc:creator>JuVen</dc:creator>
    <dc:date>2025-05-12T07:18:22Z</dc:date>
    <item>
      <title>TEA2016  LLC-Half-bridge failure</title>
      <link>https://community.nxp.com/t5/Power-Management/TEA2016-LLC-Half-bridge-failure/m-p/1995724#M3918</link>
      <description>&lt;P&gt;Hi Sir：&lt;/P&gt;&lt;P&gt;I have a Li-ion battery charger project that uses the TEA2016 . It need to outputs 28V to 42V.&lt;/P&gt;&lt;P&gt;The scenarios that need to be applied are 28V to 41.5V constant 5A current .&lt;/P&gt;&lt;P&gt;when battery is 42V ,It need constant voltage.&lt;/P&gt;&lt;P&gt;At present, 42V constant voltage output, current 0A to 5A adjustable, the test is OK.&lt;/P&gt;&lt;P&gt;But, when the constant current 5A output and the voltage is adjusted from 28V to 41.5V, It happen a question LLC-GANMOS Half bridge damaged .&lt;/P&gt;&lt;P&gt;lower bridge and the half-bridge damaged.&lt;/P&gt;&lt;P&gt;I tested a report that the voltage can be output from 28V to 42V when the current loop is limited to a constant 2A output.&lt;/P&gt;&lt;P&gt;But, TEA2016 will automatically adjust the HP-LP mode, and the resonant current waveform and half-bridge voltage waveform in LP mode are confused.&lt;/P&gt;&lt;P&gt;At present, it is speculated that the 5A output in LP mode will disturb GANMOS-GS.（see pg1）&lt;/P&gt;&lt;P&gt;There is also a case where the current loop limits 5A constant current output, and when the load machine adjusts 7Ω in CR mode, the theoretical output voltage is at this moment: 5A*7Ω=35V. In reality, however, the TEA2016 chip stopped working. （see pg2）&lt;/P&gt;&lt;P&gt;See attachment for pictures of current loop 2A limitation（see pg3-pg6）&lt;/P&gt;&lt;P&gt;SCH see PDF,During the test, in order to avoid the instability of the operation amplifier power supply, 13V is an independent power supply&lt;/P&gt;&lt;P&gt;I have asked for the technical support of the agent, but there is no solution at present. I was hoping you could help.&lt;/P&gt;</description>
      <pubDate>Sat, 16 Nov 2024 06:12:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/TEA2016-LLC-Half-bridge-failure/m-p/1995724#M3918</guid>
      <dc:creator>JuVen</dc:creator>
      <dc:date>2024-11-16T06:12:03Z</dc:date>
    </item>
    <item>
      <title>Re: TEA2016  LLC-Half-bridge failure</title>
      <link>https://community.nxp.com/t5/Power-Management/TEA2016-LLC-Half-bridge-failure/m-p/1997068#M3920</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;A id="link_6" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243421" target="_self" aria-label="View Profile of JuVen"&gt;&lt;SPAN class=""&gt;JuVen&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;我想问下您有没有用过附件的计算表格，假如没有的话我还是建议您先review一下原理图根据这个计算表格，调整下里面不一样的具体参数。&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks&lt;BR /&gt;BR&lt;/P&gt;</description>
      <pubDate>Tue, 19 Nov 2024 10:04:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/TEA2016-LLC-Half-bridge-failure/m-p/1997068#M3920</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2024-11-19T10:04:50Z</dc:date>
    </item>
    <item>
      <title>Re: TEA2016  LLC-Half-bridge failure</title>
      <link>https://community.nxp.com/t5/Power-Management/TEA2016-LLC-Half-bridge-failure/m-p/2094083#M4334</link>
      <description>&lt;P&gt;您好，我在使用tea2016调试过程中也遇到与您类似的问题，请问您是否解决？可否提供帮助，谢谢！&lt;/P&gt;</description>
      <pubDate>Fri, 09 May 2025 01:57:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/TEA2016-LLC-Half-bridge-failure/m-p/2094083#M4334</guid>
      <dc:creator>zjhzjhzjhzjh</dc:creator>
      <dc:date>2025-05-09T01:57:27Z</dc:date>
    </item>
    <item>
      <title>Re: TEA2016  LLC-Half-bridge failure</title>
      <link>https://community.nxp.com/t5/Power-Management/TEA2016-LLC-Half-bridge-failure/m-p/2095247#M4348</link>
      <description>Hi&lt;BR /&gt;May I have a look at your schematic diagram and PCB layout.&lt;BR /&gt;At that time, my problem was caused by the feedback loop and the SNSCAP loop.</description>
      <pubDate>Mon, 12 May 2025 07:18:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/TEA2016-LLC-Half-bridge-failure/m-p/2095247#M4348</guid>
      <dc:creator>JuVen</dc:creator>
      <dc:date>2025-05-12T07:18:22Z</dc:date>
    </item>
  </channel>
</rss>