<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Pause FS6500 watchdog in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/Pause-FS6500-watchdog/m-p/781765#M42</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As the title say, because of the flash erase operation, we need to pause the watchdog in FS6500; but this mode only can set in INIT phase.What can i do?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Oct 2018 07:35:06 GMT</pubDate>
    <dc:creator>yangyulong</dc:creator>
    <dc:date>2018-10-30T07:35:06Z</dc:date>
    <item>
      <title>Pause FS6500 watchdog</title>
      <link>https://community.nxp.com/t5/Power-Management/Pause-FS6500-watchdog/m-p/781765#M42</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As the title say, because of the flash erase operation, we need to pause the watchdog in FS6500; but this mode only can set in INIT phase.What can i do?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Oct 2018 07:35:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Pause-FS6500-watchdog/m-p/781765#M42</guid>
      <dc:creator>yangyulong</dc:creator>
      <dc:date>2018-10-30T07:35:06Z</dc:date>
    </item>
    <item>
      <title>Re: Pause FS6500 watchdog</title>
      <link>https://community.nxp.com/t5/Power-Management/Pause-FS6500-watchdog/m-p/781766#M43</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Yang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes,&amp;nbsp; WD can only be disabled in INIT_FS. If you want to refresh MCU when SBC is in Normal mode, You can send an SPI command(RSTB_REQ bit in SF_OUTPUT_REQUEST Register) to reset SBC, then SBC will go to INIT_FS, you can disable WD and refresh MCU then.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Br,&lt;/P&gt;&lt;P&gt;Dennis&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Oct 2018 03:20:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Pause-FS6500-watchdog/m-p/781766#M43</guid>
      <dc:creator>DennisZeng</dc:creator>
      <dc:date>2018-10-31T03:20:11Z</dc:date>
    </item>
    <item>
      <title>Re: Pause FS6500 watchdog</title>
      <link>https://community.nxp.com/t5/Power-Management/Pause-FS6500-watchdog/m-p/781767#M44</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yang,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me just add to Dennis' response that the corresponding SPI command that sets the&amp;nbsp;RSTB_REQ bit in the&amp;nbsp;SF_OUTPUT_REQUEST register is 0xD618. Then you can disable the watchdog (WD_WINDOW_3:0 = 0b0000) during&amp;nbsp;the&amp;nbsp;INIT_FS phase by sending 0xCE0C.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Oct 2018 09:16:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Pause-FS6500-watchdog/m-p/781767#M44</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2018-10-31T09:16:35Z</dc:date>
    </item>
    <item>
      <title>Re: Pause FS6500 watchdog</title>
      <link>https://community.nxp.com/t5/Power-Management/Pause-FS6500-watchdog/m-p/781768#M45</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Tomas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your answer.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a query related to this.&lt;/P&gt;&lt;P&gt;I am trying to change the config of INIT_SF_IMPACT after few wrong watchdog refresh. The RSTB goes LOW and i see SBC staying in normal mode, when MCU initiates the communication again with the SBC.&lt;BR /&gt;&lt;BR /&gt;Any hints regarding this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jul 2019 17:01:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Pause-FS6500-watchdog/m-p/781768#M45</guid>
      <dc:creator>shashi_be1234</dc:creator>
      <dc:date>2019-07-30T17:01:40Z</dc:date>
    </item>
    <item>
      <title>Re: Pause FS6500 watchdog</title>
      <link>https://community.nxp.com/t5/Power-Management/Pause-FS6500-watchdog/m-p/1265056#M1447</link>
      <description>&lt;P&gt;Hello Tomas,&lt;/P&gt;&lt;P&gt;When set the RSTB_REQ bit, MCU will reset from init.&lt;/P&gt;&lt;P&gt;If what I understand is right, can the following action be implemented?&lt;/P&gt;</description>
      <pubDate>Tue, 20 Apr 2021 10:07:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Pause-FS6500-watchdog/m-p/1265056#M1447</guid>
      <dc:creator>xupei</dc:creator>
      <dc:date>2021-04-20T10:07:46Z</dc:date>
    </item>
  </channel>
</rss>