<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックRe: PMIC PF1550 is not working as expected</title>
    <link>https://community.nxp.com/t5/Power-Management/PMIC-PF1550-is-not-working-as-expected/m-p/781664#M41</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Could you please send your schematic?&lt;/P&gt;&lt;P&gt;When you try to change some setting value of PF1550,do you test your send IIC command corresponding ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Dec 2018 13:06:06 GMT</pubDate>
    <dc:creator>guoweisun</dc:creator>
    <dc:date>2018-12-13T13:06:06Z</dc:date>
    <item>
      <title>PMIC PF1550 is not working as expected</title>
      <link>https://community.nxp.com/t5/Power-Management/PMIC-PF1550-is-not-working-as-expected/m-p/781663#M40</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Design with iMX6ULL processor and powering using PMIC PF1550,&lt;/P&gt;&lt;P&gt;At start up PMIC is Up and running with the default voltages and current limits&lt;/P&gt;&lt;P&gt;few functions of PMIC are not working as expected,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Battery charging indication LED is not glowing but battery is getting charged slowly. do i need to configure anything using I2C to indicate the battery charging.&amp;nbsp;&lt;/P&gt;&lt;P&gt;2.&amp;nbsp; I am trying to change the battery charging current limit (100mA default) to 500mA, I could update the register value using I2C but battery charging current is not increasing.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;3.&amp;nbsp; I am trying to put PMIC into standby mode, I could update the register value using I2C and verified written value by reading it back, PMIC did not enter the standby mode instead it was in the active state. am i missing any steps here ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I verified the I2C communication between iMX and PMIC and it is working.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;sharad&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Dec 2018 14:43:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PMIC-PF1550-is-not-working-as-expected/m-p/781663#M40</guid>
      <dc:creator>sharadsathvik</dc:creator>
      <dc:date>2018-12-11T14:43:25Z</dc:date>
    </item>
    <item>
      <title>Re: PMIC PF1550 is not working as expected</title>
      <link>https://community.nxp.com/t5/Power-Management/PMIC-PF1550-is-not-working-as-expected/m-p/781664#M41</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Could you please send your schematic?&lt;/P&gt;&lt;P&gt;When you try to change some setting value of PF1550,do you test your send IIC command corresponding ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Dec 2018 13:06:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PMIC-PF1550-is-not-working-as-expected/m-p/781664#M41</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2018-12-13T13:06:06Z</dc:date>
    </item>
  </channel>
</rss>