<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックPCA9617　Distance: 10m</title>
    <link>https://community.nxp.com/t5/Power-Management/PCA9617-Distance-10m/m-p/2030934#M4095</link>
    <description>&lt;P&gt;I'm thinking of using two PCA9617A, with a master-slave distance of 10m. Is this ok according to the specs?&lt;BR /&gt;One PCA9617 will be connected directly to the master board, and the other one will be placed very close to the slave board.&lt;/P&gt;</description>
    <pubDate>Tue, 21 Jan 2025 01:01:50 GMT</pubDate>
    <dc:creator>yuji0935</dc:creator>
    <dc:date>2025-01-21T01:01:50Z</dc:date>
    <item>
      <title>PCA9617　Distance: 10m</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9617-Distance-10m/m-p/2030934#M4095</link>
      <description>&lt;P&gt;I'm thinking of using two PCA9617A, with a master-slave distance of 10m. Is this ok according to the specs?&lt;BR /&gt;One PCA9617 will be connected directly to the master board, and the other one will be placed very close to the slave board.&lt;/P&gt;</description>
      <pubDate>Tue, 21 Jan 2025 01:01:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9617-Distance-10m/m-p/2030934#M4095</guid>
      <dc:creator>yuji0935</dc:creator>
      <dc:date>2025-01-21T01:01:50Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9617　Distance: 10m</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9617-Distance-10m/m-p/2030974#M4097</link>
      <description>&lt;P&gt;HI&amp;nbsp;&lt;SPAN&gt;yuji0935&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;For the high speed 10m I recommend the differential I2C-bus buffer&amp;nbsp; PCA9614/9615&lt;/P&gt;</description>
      <pubDate>Tue, 21 Jan 2025 02:11:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9617-Distance-10m/m-p/2030974#M4097</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2025-01-21T02:11:31Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9617　Distance: 10m</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9617-Distance-10m/m-p/2030977#M4098</link>
      <description>Thank you for recommending PCA9614/9615 for high speed. However, this time I'm limiting the communication speed to 100kHz. In that case, can I use PCA9617?</description>
      <pubDate>Tue, 21 Jan 2025 02:15:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9617-Distance-10m/m-p/2030977#M4098</guid>
      <dc:creator>yuji0935</dc:creator>
      <dc:date>2025-01-21T02:15:48Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9617　Distance: 10m</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9617-Distance-10m/m-p/2030990#M4100</link>
      <description>&lt;P&gt;The typical blue Cat5e communication cable is about 46 pF/m&lt;/P&gt;
&lt;P&gt;Your usage 10m&amp;nbsp;capacitance + PCA9617 Cio should be less 4000pF,if low speed should be OK.&lt;/P&gt;
&lt;P&gt;---&lt;/P&gt;
&lt;P&gt;2 channel, bidirectional buffer isolates capacitance and allows 540 pF on either side of &lt;BR /&gt;the device at 1 MHz and up to 4000 pF at lower speeds&lt;/P&gt;
&lt;P&gt;---&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Tue, 21 Jan 2025 02:29:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9617-Distance-10m/m-p/2030990#M4100</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2025-01-21T02:29:31Z</dc:date>
    </item>
  </channel>
</rss>