<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PCA9617 waveform in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/PCA9617-waveform/m-p/2028589#M4079</link>
    <description>&lt;P&gt;This circuit works fine with the PCA9600, but to reduce costs, I modified the board to use a PCA9617 and checked the waveform.&lt;BR /&gt;Looking at the clock waveform, there is no particular distortion,&lt;BR /&gt;so there doesn't seem to be a problem, but at the point where the data waveform is outputting Low,&lt;BR /&gt;I observed a waveform that was pulled High at the falling edge of the clock.&lt;/P&gt;&lt;P&gt;I wonder if this is due to crosstalk between the clock and data (there is no problem when the PCA9600DPZ is installed),&lt;BR /&gt;or is it an effect of modifying the board pattern (pattern cutting/cable soldering)?&lt;BR /&gt;I would appreciate your opinions.&lt;/P&gt;</description>
    <pubDate>Thu, 16 Jan 2025 00:35:16 GMT</pubDate>
    <dc:creator>yuji0935</dc:creator>
    <dc:date>2025-01-16T00:35:16Z</dc:date>
    <item>
      <title>PCA9617 waveform</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9617-waveform/m-p/2028589#M4079</link>
      <description>&lt;P&gt;This circuit works fine with the PCA9600, but to reduce costs, I modified the board to use a PCA9617 and checked the waveform.&lt;BR /&gt;Looking at the clock waveform, there is no particular distortion,&lt;BR /&gt;so there doesn't seem to be a problem, but at the point where the data waveform is outputting Low,&lt;BR /&gt;I observed a waveform that was pulled High at the falling edge of the clock.&lt;/P&gt;&lt;P&gt;I wonder if this is due to crosstalk between the clock and data (there is no problem when the PCA9600DPZ is installed),&lt;BR /&gt;or is it an effect of modifying the board pattern (pattern cutting/cable soldering)?&lt;BR /&gt;I would appreciate your opinions.&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jan 2025 00:35:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9617-waveform/m-p/2028589#M4079</guid>
      <dc:creator>yuji0935</dc:creator>
      <dc:date>2025-01-16T00:35:16Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9617 waveform</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9617-waveform/m-p/2028672#M4080</link>
      <description>&lt;P&gt;HI&amp;nbsp;&lt;A id="link_6" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245628" target="_self" aria-label="View Profile of yuji0935"&gt;&lt;SPAN class=""&gt;yuji0935&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;I think it's an effect of modifying the board pattern &amp;nbsp;(pattern cutting/cable soldering)about this glitch.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jan 2025 03:26:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9617-waveform/m-p/2028672#M4080</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2025-01-16T03:26:48Z</dc:date>
    </item>
  </channel>
</rss>