<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックRe: PF8121 in TBB mode</title>
    <link>https://community.nxp.com/t5/Power-Management/PF8121-in-TBB-mode/m-p/912334#M402</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jinyu,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way for the PMIC to hold its TBB register values after a power cycle?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Right now on the evaluation board, I have J21 open to allow MCU to control TBB EN pin.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I set J21 in&amp;nbsp;2-3 -&amp;gt; TBB mode enabled, will it hold the register values after power cycle?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Juhi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Oct 2019 18:33:50 GMT</pubDate>
    <dc:creator>juhi_pandey</dc:creator>
    <dc:date>2019-10-15T18:33:50Z</dc:date>
    <item>
      <title>PF8121 in TBB mode</title>
      <link>https://community.nxp.com/t5/Power-Management/PF8121-in-TBB-mode/m-p/912328#M396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Platform:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; i.MX 8M-Mini + PF8121&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using PF8121(F2) in an upcoming board design(using IMX8-M mini) and working on PMIC TBB mode configuration using KITPF8121FRDMEVM and Flex GUI right now. On the KITPF8121FRDMEVM board, I have the jumper J20 open and J21 in 2-3 -&amp;gt;TBB mode( described on Page 11 of the datasheet&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/user-guide/UM11214.pdf" title="https://www.nxp.com/docs/en/user-guide/UM11214.pdf"&gt;https://www.nxp.com/docs/en/user-guide/UM11214.pdf&lt;/A&gt;&amp;nbsp;).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The output configuration I need for switchers and LDO is :&lt;/P&gt;&lt;P&gt;SW1 - 0.8V&lt;BR /&gt;SW2 - 0.9V&lt;BR /&gt;SW3 - 0.95V&lt;BR /&gt;SW4 - 1.1V&lt;BR /&gt;SW5 - 1.35V&lt;BR /&gt;SW6 - 1.8V&lt;BR /&gt;SW7 - 3.3V&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;LDO1/LDO2 - Unused&lt;BR /&gt;LDO3 - 2.5V&lt;BR /&gt;LDO4 - 1.8V&lt;BR /&gt;SNVS- 1.8V&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you help on how to disable LDO1/LDO2 in the attached excel sheet?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you confirm if I can use the attached excel sheet to load the registers in the Flex GUI?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Juhi&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Sep 2019 23:41:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF8121-in-TBB-mode/m-p/912328#M396</guid>
      <dc:creator>juhi_pandey</dc:creator>
      <dc:date>2019-09-25T23:41:26Z</dc:date>
    </item>
    <item>
      <title>Re: PF8121 in TBB mode</title>
      <link>https://community.nxp.com/t5/Power-Management/PF8121-in-TBB-mode/m-p/912329#M397</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Juhi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you help on how to disable LDO1/LDO2 in the attached excel sheet?&lt;/P&gt;&lt;P&gt;[A] To disable the LDO1 and LDO2 in the excel sheet, you just need to set the OTP_LDO1_SEQ and OTP_LDO1_SEQ to OFF.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you confirm if I can use the attached excel sheet to load the registers in the Flex GUI?&lt;/P&gt;&lt;P&gt;[A] Yes, You can use the attached excel sheet to generate a script file (using EXPORT CONFIG FILE) to be able to load the registers in the FlexGUI. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Sep 2019 15:47:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF8121-in-TBB-mode/m-p/912329#M397</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2019-09-26T15:47:30Z</dc:date>
    </item>
    <item>
      <title>Re: PF8121 in TBB mode</title>
      <link>https://community.nxp.com/t5/Power-Management/PF8121-in-TBB-mode/m-p/912330#M398</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Thanks&amp;nbsp;Jose. I made changes to the excel sheet as suggested by you.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;When I export the script(using export Config file) and load it into the Flex GUI, I see the following error :&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/82055iA3198907509602E9/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Can you help resolve this?&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Thanks,&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Juhi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Sep 2019 16:50:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF8121-in-TBB-mode/m-p/912330#M398</guid>
      <dc:creator>juhi_pandey</dc:creator>
      <dc:date>2019-09-30T16:50:14Z</dc:date>
    </item>
    <item>
      <title>Re: PF8121 in TBB mode</title>
      <link>https://community.nxp.com/t5/Power-Management/PF8121-in-TBB-mode/m-p/912331#M399</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Juhi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is your KL25Z MCU firmware up to date?&lt;/P&gt;&lt;P&gt;I ask this because the KL25Z MCU provides the FlexGUI firmware in charge of converting the USB communication into MCU instructions to control digital I/Os as well as I2C communication to the PMIC.&lt;/P&gt;&lt;P&gt;If the FRDM-KL25Z is not loaded with the correct firmware, the firmware can be updated in few simple steps as you can see in section 5.4 on pages 16, 17 and 18 of the boards user guide: &lt;A href="https://www.nxp.com/docs/en/user-guide/UM11214.pdf"&gt;https://www.nxp.com/docs/en/user-guide/UM11214.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the KL25Z firmware is up to date, then other possibility is the script generated from the excel.&lt;/P&gt;&lt;P&gt;When filling the excel, make sure to fill all required fields marked with a * to enable file generation. When generating a TBB script, it is important to match the device name with the device name in the FlexGUI to ensure proper generation of the script commands.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jose&lt;/P&gt;&lt;P&gt;NXP Semiconductors&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Oct 2019 14:31:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF8121-in-TBB-mode/m-p/912331#M399</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2019-10-02T14:31:09Z</dc:date>
    </item>
    <item>
      <title>Re: PF8121 in TBB mode</title>
      <link>https://community.nxp.com/t5/Power-Management/PF8121-in-TBB-mode/m-p/912332#M400</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Jose.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My main issue was with the KL25Z Firmware. I updated the bootloader version and that fixed my problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After that I was able to verify TBB configuration on the evaluation board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your support.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Juhi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Oct 2019 20:23:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF8121-in-TBB-mode/m-p/912332#M400</guid>
      <dc:creator>juhi_pandey</dc:creator>
      <dc:date>2019-10-03T20:23:47Z</dc:date>
    </item>
    <item>
      <title>Re: PF8121 in TBB mode</title>
      <link>https://community.nxp.com/t5/Power-Management/PF8121-in-TBB-mode/m-p/912333#M401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Juhi&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;Good to see that, and you should use the "Generate Output file " to generate the script, and the yellow button should be choosen TBB . the script should be:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/95799i106374554F487AD2/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;then when you load and run the script , it will work in TBB mode.&lt;/P&gt;&lt;P&gt;BRs&lt;/P&gt;&lt;P&gt;jinyu&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Oct 2019 00:35:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF8121-in-TBB-mode/m-p/912333#M401</guid>
      <dc:creator>jinyuzhang</dc:creator>
      <dc:date>2019-10-07T00:35:58Z</dc:date>
    </item>
    <item>
      <title>Re: PF8121 in TBB mode</title>
      <link>https://community.nxp.com/t5/Power-Management/PF8121-in-TBB-mode/m-p/912334#M402</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jinyu,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way for the PMIC to hold its TBB register values after a power cycle?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Right now on the evaluation board, I have J21 open to allow MCU to control TBB EN pin.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I set J21 in&amp;nbsp;2-3 -&amp;gt; TBB mode enabled, will it hold the register values after power cycle?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Juhi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Oct 2019 18:33:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF8121-in-TBB-mode/m-p/912334#M402</guid>
      <dc:creator>juhi_pandey</dc:creator>
      <dc:date>2019-10-15T18:33:50Z</dc:date>
    </item>
    <item>
      <title>Re: PF8121 in TBB mode</title>
      <link>https://community.nxp.com/t5/Power-Management/PF8121-in-TBB-mode/m-p/912335#M403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Juhi&lt;/P&gt;&lt;P&gt;When OPEN J21 and use MCU to keep TBBEN is high or set J21 in 2-3 to&amp;nbsp;let TBBEN is high, the TBB mode is enable. &lt;BR /&gt;In this time, if you just control PWRON to power off and power on, the TBB register values will be hold after a power cycle. But if you let vin is 0V, the TBB register values won't be hold.&lt;/P&gt;&lt;P&gt;BRs&lt;/P&gt;&lt;P&gt;jinyu&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Oct 2019 03:12:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF8121-in-TBB-mode/m-p/912335#M403</guid>
      <dc:creator>jinyuzhang</dc:creator>
      <dc:date>2019-10-17T03:12:53Z</dc:date>
    </item>
  </channel>
</rss>