<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FS5613 DEBUG mode low VCCA voltage in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/FS5613-DEBUG-mode-low-VCCA-voltage/m-p/2007471#M3964</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;It is high possibility due to overcurrent after VCCA. Vcca 5V should be stable no matter device powerup or normal running.&lt;/P&gt;</description>
    <pubDate>Wed, 04 Dec 2024 21:33:02 GMT</pubDate>
    <dc:creator>ErikaC</dc:creator>
    <dc:date>2024-12-04T21:33:02Z</dc:date>
    <item>
      <title>FS5613 DEBUG mode low VCCA voltage</title>
      <link>https://community.nxp.com/t5/Power-Management/FS5613-DEBUG-mode-low-VCCA-voltage/m-p/2005206#M3954</link>
      <description>&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;After entering DEBUG mode we can observe VPRE, VCORE, VAUX (5V) being of correct value, however VCCA which should be 5V is instead 3V. After programming the microcontroller and running the code on it, the voltage reaches expected 5V. Select resistor is 12k. VCCA is used to power on uC pins, and VAUX is used to power ADC. What could be the reason behind that?&lt;/P&gt;</description>
      <pubDate>Mon, 02 Dec 2024 14:55:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS5613-DEBUG-mode-low-VCCA-voltage/m-p/2005206#M3954</guid>
      <dc:creator>mrajzr</dc:creator>
      <dc:date>2024-12-02T14:55:54Z</dc:date>
    </item>
    <item>
      <title>Re: FS5613 DEBUG mode low VCCA voltage</title>
      <link>https://community.nxp.com/t5/Power-Management/FS5613-DEBUG-mode-low-VCCA-voltage/m-p/2005379#M3956</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Just to confirm, are you using FS56 or FS65?&lt;/P&gt;</description>
      <pubDate>Mon, 02 Dec 2024 19:12:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS5613-DEBUG-mode-low-VCCA-voltage/m-p/2005379#M3956</guid>
      <dc:creator>ErikaC</dc:creator>
      <dc:date>2024-12-02T19:12:22Z</dc:date>
    </item>
    <item>
      <title>Re: FS5613 DEBUG mode low VCCA voltage</title>
      <link>https://community.nxp.com/t5/Power-Management/FS5613-DEBUG-mode-low-VCCA-voltage/m-p/2005770#M3960</link>
      <description>&lt;P&gt;Hello, yes I meant&amp;nbsp;&lt;SPAN&gt;FS65.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Dec 2024 07:12:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS5613-DEBUG-mode-low-VCCA-voltage/m-p/2005770#M3960</guid>
      <dc:creator>mrajzr</dc:creator>
      <dc:date>2024-12-03T07:12:16Z</dc:date>
    </item>
    <item>
      <title>Re: FS5613 DEBUG mode low VCCA voltage</title>
      <link>https://community.nxp.com/t5/Power-Management/FS5613-DEBUG-mode-low-VCCA-voltage/m-p/2007471#M3964</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;It is high possibility due to overcurrent after VCCA. Vcca 5V should be stable no matter device powerup or normal running.&lt;/P&gt;</description>
      <pubDate>Wed, 04 Dec 2024 21:33:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS5613-DEBUG-mode-low-VCCA-voltage/m-p/2007471#M3964</guid>
      <dc:creator>ErikaC</dc:creator>
      <dc:date>2024-12-04T21:33:02Z</dc:date>
    </item>
    <item>
      <title>Re: FS5613 DEBUG mode low VCCA voltage</title>
      <link>https://community.nxp.com/t5/Power-Management/FS5613-DEBUG-mode-low-VCCA-voltage/m-p/2011895#M3978</link>
      <description>&lt;P&gt;Hi ErikaC, thank you for the hint, it was in fact debugger drawing too much current through one of its pins&lt;/P&gt;</description>
      <pubDate>Wed, 11 Dec 2024 10:03:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS5613-DEBUG-mode-low-VCCA-voltage/m-p/2011895#M3978</guid>
      <dc:creator>mrajzr</dc:creator>
      <dc:date>2024-12-11T10:03:43Z</dc:date>
    </item>
  </channel>
</rss>