<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power Management中的主题 Application note for implementing TEA1721AT in design</title>
    <link>https://community.nxp.com/t5/Power-Management/Application-note-for-implementing-TEA1721AT-in-design/m-p/1982066#M3843</link>
    <description>&lt;P&gt;I need to build a fly-back converter with 2 isolated outputs and with an input range of 19 - 150Vdc. It also needs to have a VERY no-load consumption.&lt;/P&gt;&lt;P&gt;I was therefore looking at the TEA1721 family.&lt;/P&gt;&lt;P&gt;Is there a tool or application note that can help me with this design?&lt;/P&gt;</description>
    <pubDate>Fri, 25 Oct 2024 13:28:21 GMT</pubDate>
    <dc:creator>tkoha</dc:creator>
    <dc:date>2024-10-25T13:28:21Z</dc:date>
    <item>
      <title>Application note for implementing TEA1721AT in design</title>
      <link>https://community.nxp.com/t5/Power-Management/Application-note-for-implementing-TEA1721AT-in-design/m-p/1982066#M3843</link>
      <description>&lt;P&gt;I need to build a fly-back converter with 2 isolated outputs and with an input range of 19 - 150Vdc. It also needs to have a VERY no-load consumption.&lt;/P&gt;&lt;P&gt;I was therefore looking at the TEA1721 family.&lt;/P&gt;&lt;P&gt;Is there a tool or application note that can help me with this design?&lt;/P&gt;</description>
      <pubDate>Fri, 25 Oct 2024 13:28:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Application-note-for-implementing-TEA1721AT-in-design/m-p/1982066#M3843</guid>
      <dc:creator>tkoha</dc:creator>
      <dc:date>2024-10-25T13:28:21Z</dc:date>
    </item>
    <item>
      <title>Re: Application note for implementing TEA1721AT in design</title>
      <link>https://community.nxp.com/t5/Power-Management/Application-note-for-implementing-TEA1721AT-in-design/m-p/1982544#M3844</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;That's not easy for design this&amp;nbsp; by use one stage power solution because the input range is more special.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;You can use one stage BOOST to improve input voltage into 150V or above,then second stage use the normal fly-back or QR FLYBACK controller to get the isolation solution.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;You can calculate by following attached calculate sheet. for QR FLY-BACK&amp;nbsp; topology.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Hope this could help！&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 28 Oct 2024 01:52:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Application-note-for-implementing-TEA1721AT-in-design/m-p/1982544#M3844</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2024-10-28T01:52:57Z</dc:date>
    </item>
  </channel>
</rss>