<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power Managementのトピック回复： FS2400 CAN wake up</title>
    <link>https://community.nxp.com/t5/Power-Management/FS2400-CAN-wake-up/m-p/1971177#M3820</link>
    <description>&lt;P&gt;I have&amp;nbsp; also tried write the whole reg to 0x0 and write CAN_WU_I bit to 0, the flag can not be cleared.&lt;/P&gt;&lt;P&gt;fs2400_write_register(&amp;amp;l_xDev, FS2400_REG_M_WU1_FLG, 0x0)&lt;/P&gt;&lt;P&gt;fs2400_write_bit(&amp;amp;l_xDev, FS2400_REG_M_WU1_FLG, FS2400_REG_M_WU1_FLG_CAN_WU_I, 0)&lt;/P&gt;&lt;P&gt;Any other registers should be re-init after a CAN wake-up pattern?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 10 Oct 2024 08:33:32 GMT</pubDate>
    <dc:creator>kk211911</dc:creator>
    <dc:date>2024-10-10T08:33:32Z</dc:date>
    <item>
      <title>FS2400 CAN wake up</title>
      <link>https://community.nxp.com/t5/Power-Management/FS2400-CAN-wake-up/m-p/1971030#M3818</link>
      <description>&lt;P&gt;Hello, the fs2400 works as Debug mode. when&amp;nbsp; i wake up it via CAN from LPOFF mode,&amp;nbsp; can doesn't work.&amp;nbsp; I tried to clear the CAN_WU_I flag following the data sheet, but it can not take effect.&amp;nbsp;&amp;nbsp;How to clear the CAN_WU_I flag?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kk211911_0-1728541432007.png" style="width: 621px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/303938i8F08D07B69BE40BE/image-dimensions/621x45?v=v2" width="621" height="45" role="button" title="kk211911_0-1728541432007.png" alt="kk211911_0-1728541432007.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;kk211911_0-1728541432007.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;After i dId power reset , CAN works.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Oct 2024 06:33:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS2400-CAN-wake-up/m-p/1971030#M3818</guid>
      <dc:creator>kk211911</dc:creator>
      <dc:date>2024-10-10T06:33:37Z</dc:date>
    </item>
    <item>
      <title>Re: FS2400 CAN wake up</title>
      <link>https://community.nxp.com/t5/Power-Management/FS2400-CAN-wake-up/m-p/1971160#M3819</link>
      <description>&lt;P&gt;Hello Kun,&lt;/P&gt;
&lt;P&gt;When the FS2400 is in Debug mode, the CAN transceiver is active regardless of the CAN_MODE[1:0] bits state of the M_CAN register.&lt;/P&gt;
&lt;P&gt;To clear the&amp;nbsp;&lt;SPAN&gt;CAN_WU_I flag, write 0 to bit 0 of the&amp;nbsp;M_WU1_FLG register.&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BRs, Tomas&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Oct 2024 08:24:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS2400-CAN-wake-up/m-p/1971160#M3819</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2024-10-10T08:24:08Z</dc:date>
    </item>
    <item>
      <title>回复： FS2400 CAN wake up</title>
      <link>https://community.nxp.com/t5/Power-Management/FS2400-CAN-wake-up/m-p/1971177#M3820</link>
      <description>&lt;P&gt;I have&amp;nbsp; also tried write the whole reg to 0x0 and write CAN_WU_I bit to 0, the flag can not be cleared.&lt;/P&gt;&lt;P&gt;fs2400_write_register(&amp;amp;l_xDev, FS2400_REG_M_WU1_FLG, 0x0)&lt;/P&gt;&lt;P&gt;fs2400_write_bit(&amp;amp;l_xDev, FS2400_REG_M_WU1_FLG, FS2400_REG_M_WU1_FLG_CAN_WU_I, 0)&lt;/P&gt;&lt;P&gt;Any other registers should be re-init after a CAN wake-up pattern?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Oct 2024 08:33:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS2400-CAN-wake-up/m-p/1971177#M3820</guid>
      <dc:creator>kk211911</dc:creator>
      <dc:date>2024-10-10T08:33:32Z</dc:date>
    </item>
  </channel>
</rss>