<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PF3000 unused outputs in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/PF3000-unused-outputs/m-p/758406#M37</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hazar,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are no disadvantages, unused LDO outputs can be left floating and inputs can be connected to GND if not shared with other LDOs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jose&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Feb 2019 21:48:12 GMT</pubDate>
    <dc:creator>reyes</dc:creator>
    <dc:date>2019-02-05T21:48:12Z</dc:date>
    <item>
      <title>PF3000 unused outputs</title>
      <link>https://community.nxp.com/t5/Power-Management/PF3000-unused-outputs/m-p/758403#M34</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the PF3000 as the primary PMIC to power my MX7 based hardware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the first demo version of the board the 5V output was used for testing purposes, but it is not needed any longer.&lt;/P&gt;&lt;P&gt;May I cut some of the parts connected to the boost regulator? (Diode+Caps+Inductor ~ 50ct cost per device)&lt;/P&gt;&lt;P&gt;Or does the circuit need to be connected? In this case I could probably lower the capacitance values (currently 2x22uF+100nF+4.7uF).&lt;/P&gt;&lt;P&gt;Some LDOs are not used as well, simply using a small capacitor here&amp;nbsp;should be the best option?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Lars&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jan 2018 15:58:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF3000-unused-outputs/m-p/758403#M34</guid>
      <dc:creator>demoniacmilk</dc:creator>
      <dc:date>2018-01-03T15:58:35Z</dc:date>
    </item>
    <item>
      <title>Re: PF3000 unused outputs</title>
      <link>https://community.nxp.com/t5/Power-Management/PF3000-unused-outputs/m-p/758404#M35</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lars,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;U&lt;SPAN&gt;nused boost switching regulator should be connected as follows: &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Pins SWBSTLX and SWBSTFB should be unconnected and Pin VIN2 should be connected to VIN with a 0.1uF bypass capacitor.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;And unused LDO regulators should be connected as follows:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Input pins of the LDOs should be connected to output of a regulator with voltage lower than 3.4V with a 1.0uF decoupling capacitor and the output pins should be unconnected.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jose&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jan 2018 18:20:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF3000-unused-outputs/m-p/758404#M35</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2018-01-04T18:20:56Z</dc:date>
    </item>
    <item>
      <title>Re: PF3000 unused outputs</title>
      <link>https://community.nxp.com/t5/Power-Management/PF3000-unused-outputs/m-p/758405#M36</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Alberto,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the PF3000 datasheet, notes on Figure 36, states that:&lt;/P&gt;&lt;P&gt;Unused LDO: output can be left floating. Connect input pin to GND if not shared with other LDOs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any disadvantage of connecting input of unused LDOs to GND instead of output of a regulator with voltage lower than 3.4V as you suggested?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Hazar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Feb 2019 14:09:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF3000-unused-outputs/m-p/758405#M36</guid>
      <dc:creator>hazar_mutgan</dc:creator>
      <dc:date>2019-02-04T14:09:17Z</dc:date>
    </item>
    <item>
      <title>Re: PF3000 unused outputs</title>
      <link>https://community.nxp.com/t5/Power-Management/PF3000-unused-outputs/m-p/758406#M37</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hazar,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are no disadvantages, unused LDO outputs can be left floating and inputs can be connected to GND if not shared with other LDOs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jose&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Feb 2019 21:48:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF3000-unused-outputs/m-p/758406#M37</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2019-02-05T21:48:12Z</dc:date>
    </item>
  </channel>
</rss>