<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: s32k3 enable PMIC MCU handshark function in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/s32k3-enable-PMIC-MCU-handshark-function/m-p/1906997#M3618</link>
    <description>&lt;P&gt;Hi Jimmy,&lt;/P&gt;
&lt;P&gt;Which PMIC/SBC are you using?&lt;/P&gt;
&lt;P&gt;If FS26,&amp;nbsp;a VCORE_PGOOD signal is available through GPIO2 pin. When&amp;nbsp;GPIO2 is configured as VCORE_PGOOD using the GPIO2_VCORE_PGOOD_OTP bit, GPIO2 is connected to&amp;nbsp;the HS switch (connected internally to VPRE).&lt;/P&gt;
&lt;P&gt;VCORE_PGOOD signal may be connected to the WKPU signal of the MCU which requires a 3.3 V level. A resistor divider is needed to adapt the voltage level.&lt;/P&gt;
&lt;P&gt;• When VCORE is in the good voltage range, VCORE_PGOOD is High logic level.&lt;BR /&gt;• When VCORE is not in the good voltage range or is disabled, VCORE_PGOOD is Low logic level.&lt;/P&gt;
&lt;P&gt;During Standby mode, in case of a reset from the MCU, its RESET pin must be connected to the FS26 RSTB pin but also to the FS26 WAKE1 pin, which is configured as a low-level wake-up source, to wake up the SBC.&lt;/P&gt;
&lt;P&gt;The total capacitance on the RSTB line should not exceed 1nF.&lt;/P&gt;
&lt;P&gt;The MCU EXTWKPU pin must be connected to the FS26 WAKE2 pin, configured as a high-level wake-up&amp;nbsp;source.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture.JPG" style="width: 643px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/288318i68CEAB7E7A1A04F3/image-dimensions/643x508?v=v2" width="643" height="508" role="button" title="Capture.JPG" alt="Capture.JPG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Capture.JPG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
    <pubDate>Fri, 12 Jul 2024 09:49:56 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2024-07-12T09:49:56Z</dc:date>
    <item>
      <title>s32k3 enable PMIC MCU handshark function</title>
      <link>https://community.nxp.com/t5/Power-Management/s32k3-enable-PMIC-MCU-handshark-function/m-p/1905984#M3615</link>
      <description>&lt;P&gt;how can i enable PGOOD PMIC MCU handshark function?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jimmy623_0-1720684017651.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/288061i4F86179A1DF321D3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jimmy623_0-1720684017651.png" alt="jimmy623_0-1720684017651.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;jimmy623_0-1720684017651.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32k3-power-on-reset-issue/td-p/1887078" target="_blank"&gt;S32k3 power on reset issue - NXP Community&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jul 2024 07:49:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/s32k3-enable-PMIC-MCU-handshark-function/m-p/1905984#M3615</guid>
      <dc:creator>jimmy623</dc:creator>
      <dc:date>2024-07-11T07:49:02Z</dc:date>
    </item>
    <item>
      <title>回复： s32k3 enable PMIC MCU handshark function</title>
      <link>https://community.nxp.com/t5/Power-Management/s32k3-enable-PMIC-MCU-handshark-function/m-p/1906945#M3617</link>
      <description>&lt;P&gt;Hi，&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;In S32K358 project we encounter a issue :&amp;nbsp; system boot 5 times&amp;nbsp;&lt;SPAN&gt;Every time when starting from Pflash.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I&amp;nbsp;follow&amp;nbsp; Sbc_fs26_example_HLD_S32K344 example ,enable fs26 in s32k358 to solve the problem.but&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;The problem has not been resolved&lt;/SPAN&gt;&amp;nbsp;.&lt;/P&gt;&lt;P&gt;i try POR_WDG disable:&amp;nbsp;&amp;nbsp;IP_DCM_GPR-&amp;gt;DCMRWP1 |= 0x00000100;&amp;nbsp;&lt;/P&gt;&lt;P&gt;failed !&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;IN RF,&amp;nbsp;&amp;nbsp; PMIC_PGOOD handshake with&amp;nbsp; PMIC,&amp;nbsp;If PGOOD assertion does not arrive within the configured time, POR WDOG will issue a reset to the MCU.&amp;nbsp;how can i enable PGOOD PMIC MCU handshark function?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jimmy623_0-1720773564923.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/288302i410C61FCC26CF3DC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jimmy623_0-1720773564923.png" alt="jimmy623_0-1720773564923.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;jimmy623_0-1720773564923.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jimmy623_1-1720775067764.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/288306i7216D3C318BD0098/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jimmy623_1-1720775067764.png" alt="jimmy623_1-1720775067764.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;jimmy623_1-1720775067764.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 12 Jul 2024 09:04:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/s32k3-enable-PMIC-MCU-handshark-function/m-p/1906945#M3617</guid>
      <dc:creator>jimmy623</dc:creator>
      <dc:date>2024-07-12T09:04:34Z</dc:date>
    </item>
    <item>
      <title>Re: s32k3 enable PMIC MCU handshark function</title>
      <link>https://community.nxp.com/t5/Power-Management/s32k3-enable-PMIC-MCU-handshark-function/m-p/1906997#M3618</link>
      <description>&lt;P&gt;Hi Jimmy,&lt;/P&gt;
&lt;P&gt;Which PMIC/SBC are you using?&lt;/P&gt;
&lt;P&gt;If FS26,&amp;nbsp;a VCORE_PGOOD signal is available through GPIO2 pin. When&amp;nbsp;GPIO2 is configured as VCORE_PGOOD using the GPIO2_VCORE_PGOOD_OTP bit, GPIO2 is connected to&amp;nbsp;the HS switch (connected internally to VPRE).&lt;/P&gt;
&lt;P&gt;VCORE_PGOOD signal may be connected to the WKPU signal of the MCU which requires a 3.3 V level. A resistor divider is needed to adapt the voltage level.&lt;/P&gt;
&lt;P&gt;• When VCORE is in the good voltage range, VCORE_PGOOD is High logic level.&lt;BR /&gt;• When VCORE is not in the good voltage range or is disabled, VCORE_PGOOD is Low logic level.&lt;/P&gt;
&lt;P&gt;During Standby mode, in case of a reset from the MCU, its RESET pin must be connected to the FS26 RSTB pin but also to the FS26 WAKE1 pin, which is configured as a low-level wake-up source, to wake up the SBC.&lt;/P&gt;
&lt;P&gt;The total capacitance on the RSTB line should not exceed 1nF.&lt;/P&gt;
&lt;P&gt;The MCU EXTWKPU pin must be connected to the FS26 WAKE2 pin, configured as a high-level wake-up&amp;nbsp;source.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture.JPG" style="width: 643px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/288318i68CEAB7E7A1A04F3/image-dimensions/643x508?v=v2" width="643" height="508" role="button" title="Capture.JPG" alt="Capture.JPG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Capture.JPG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
      <pubDate>Fri, 12 Jul 2024 09:49:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/s32k3-enable-PMIC-MCU-handshark-function/m-p/1906997#M3618</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2024-07-12T09:49:56Z</dc:date>
    </item>
    <item>
      <title>回复： s32k3 enable PMIC MCU handshark function</title>
      <link>https://community.nxp.com/t5/Power-Management/s32k3-enable-PMIC-MCU-handshark-function/m-p/1910394#M3624</link>
      <description>&lt;P&gt;Hi ,&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;s32k358+fs2613, in fs26 init function Sbc_fs26_InitDevice()&amp;nbsp; / Sbc_fs26_CheckRegAndOTPCorrupt ，&lt;/P&gt;&lt;P&gt;I got REG_CORRUPT fail .&amp;nbsp;xRxData.u16ReadData = 0x280a.&lt;/P&gt;&lt;P&gt;how can i fix this issue?&lt;/P&gt;&lt;P&gt;Thanks!&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jimmy623_1-1721202638897.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/288910i73A8B2073A628579/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jimmy623_1-1721202638897.png" alt="jimmy623_1-1721202638897.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;jimmy623_1-1721202638897.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jimmy623_0-1721202621662.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/288909i168F73A4099BEA3A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jimmy623_0-1721202621662.png" alt="jimmy623_0-1721202621662.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;jimmy623_0-1721202621662.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jul 2024 07:56:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/s32k3-enable-PMIC-MCU-handshark-function/m-p/1910394#M3624</guid>
      <dc:creator>jimmy623</dc:creator>
      <dc:date>2024-07-17T07:56:01Z</dc:date>
    </item>
  </channel>
</rss>