<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TEA19161 in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/TEA19161/m-p/1876118#M3529</link>
    <description>Then may I ask if it can be achieved? I just want to learn about the working state of the LLC circuit through TEA19161. If it is possible, could you provide the circuit diagram</description>
    <pubDate>Tue, 28 May 2024 08:25:51 GMT</pubDate>
    <dc:creator>shouyumi</dc:creator>
    <dc:date>2024-05-28T08:25:51Z</dc:date>
    <item>
      <title>TEA19161</title>
      <link>https://community.nxp.com/t5/Power-Management/TEA19161/m-p/1875159#M3525</link>
      <description>&lt;P&gt;&lt;SPAN&gt;TEA19161T能否在不与TEA19162合作的情况下实现直接的DC-DC转换？&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 27 May 2024 04:35:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/TEA19161/m-p/1875159#M3525</guid>
      <dc:creator>shouyumi</dc:creator>
      <dc:date>2024-05-27T04:35:21Z</dc:date>
    </item>
    <item>
      <title>Re: TEA19161</title>
      <link>https://community.nxp.com/t5/Power-Management/TEA19161/m-p/1875244#M3527</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The TEA19161 is not designed to achieve direct DC-DC conversion without the TEA19162. They are intended to work together to provide a complete and efficient power conversion solution.&lt;/P&gt;
&lt;P&gt;We also do not recommend using the TEA19161 with another PFC controller. The TEA19162 is designed to operate in close cooperation with the TEA19161 to ensure optimal burst-mode operation and complementary protection functions.&lt;/P&gt;
&lt;P&gt;BR, Tomas&lt;/P&gt;</description>
      <pubDate>Mon, 27 May 2024 06:36:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/TEA19161/m-p/1875244#M3527</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2024-05-27T06:36:43Z</dc:date>
    </item>
    <item>
      <title>Re: TEA19161</title>
      <link>https://community.nxp.com/t5/Power-Management/TEA19161/m-p/1876114#M3528</link>
      <description>&lt;P&gt;&lt;SPAN&gt;那我能问一下能不能实现呢？我只想通过TEA19161了解 LLC 电路的工作状态。如果可能的话，你能提供电路图吗？&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 28 May 2024 08:23:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/TEA19161/m-p/1876114#M3528</guid>
      <dc:creator>shouyumi</dc:creator>
      <dc:date>2024-05-28T08:23:53Z</dc:date>
    </item>
    <item>
      <title>Re: TEA19161</title>
      <link>https://community.nxp.com/t5/Power-Management/TEA19161/m-p/1876118#M3529</link>
      <description>Then may I ask if it can be achieved? I just want to learn about the working state of the LLC circuit through TEA19161. If it is possible, could you provide the circuit diagram</description>
      <pubDate>Tue, 28 May 2024 08:25:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/TEA19161/m-p/1876118#M3529</guid>
      <dc:creator>shouyumi</dc:creator>
      <dc:date>2024-05-28T08:25:51Z</dc:date>
    </item>
    <item>
      <title>Re: TEA19161</title>
      <link>https://community.nxp.com/t5/Power-Management/TEA19161/m-p/1876121#M3531</link>
      <description>Thank you very much !</description>
      <pubDate>Tue, 28 May 2024 08:28:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/TEA19161/m-p/1876121#M3531</guid>
      <dc:creator>shouyumi</dc:creator>
      <dc:date>2024-05-28T08:28:52Z</dc:date>
    </item>
  </channel>
</rss>