<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックRe: How to enable CAN on MC33665A?</title>
    <link>https://community.nxp.com/t5/Power-Management/How-to-enable-CAN-on-MC33665A/m-p/1847882#M3436</link>
    <description>&lt;P&gt;Hi Jimmie,&lt;/P&gt;
&lt;P&gt;Here are some hints:.&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;The DBC files are meant to be used with the CAN-based CMU board directly. We actually have an example with documentation (based on the MC33775) published on the &lt;A href="https://www.nxp.com/products/power-management/battery-management/battery-communication-ics/general-purpose-bms-communication-tpl-transceiver-and-can-fd-gateway:MC33665A" target="_blank"&gt;MC33665 webpage&lt;/A&gt;.&lt;/LI&gt;
&lt;LI&gt;There is a CAN-based example code for the BMU available at:&amp;nbsp;&lt;A href="https://nxp.flexnetoperations.com/control/frse/product?child_plneID=860927" target="_blank"&gt;https://nxp.flexnetoperations.com/control/frse/product?child_plneID=860927&lt;/A&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture.jpg" style="width: 657px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/273963i9FCC6A062D79E94E/image-dimensions/657x229?v=v2" width="657" height="229" role="button" title="Capture.jpg" alt="Capture.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope it helps.&lt;/P&gt;
&lt;P&gt;BR, Tomas&lt;/P&gt;</description>
    <pubDate>Tue, 16 Apr 2024 08:33:38 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2024-04-16T08:33:38Z</dc:date>
    <item>
      <title>How to enable CAN on MC33665A?</title>
      <link>https://community.nxp.com/t5/Power-Management/How-to-enable-CAN-on-MC33665A/m-p/1846904#M3433</link>
      <description>&lt;P&gt;Hi NXP forum!&lt;/P&gt;&lt;P&gt;We purchased NXP’s 800 V Battery Management System (BMS) Reference Designs Using ETPL (&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/800-v-battery-management-system-bms-reference-designs-using-etpl:RD-HVBMSCT800BUN" target="_blank" rel="nofollow noopener noreferrer"&gt;https://www.nxp.com/design/design-center/development-boards-and-designs/800-v-battery-management-sys...&lt;/A&gt;) since we wanted a proper BMS to validate and test our battery emulator against.&lt;/P&gt;&lt;P&gt;Works great, currently we have been using FreeMaster and the example that exists for the reference design, referring to HVBMS_800_StartUp_FreeMASTER.pmpx, all measurements done by the BMS looks spot-on and as expected, same with the temperatures that we emulate through another board we have developed.&lt;/P&gt;&lt;P&gt;We have received a CAN database from support at NXP that we were told would work with the reference design BMU, see screenshot below, we have used the NXP_BMS_QPHY_V1.dbc. You can download the files here:&amp;nbsp;&lt;A href="https://www.nxp.com/products/power-management/battery-management/battery-communication-ics/general-purpose-bms-communication-tpl-transceiver-and-can-fd-gateway:MC33665A?tid=vanMC33665A" target="_blank"&gt;MC33665A: Isolated Network High Speed Transceiver and CAN FD Gateway | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JWA74_0-1713167910596.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/273700i7110658DD5F21D4A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JWA74_0-1713167910596.png" alt="JWA74_0-1713167910596.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We have connected our external CAN to the VCU_CAN port (that supports partial networking wake-up) on the RD-K358BMU using the DSUB connector that was included on the J1 connector cabling, according to the manual, to enable the VCU_CAN one can achieve it using the WUP on the SBC, or more specifically SBC WAKE1 input on the SBC.&lt;/P&gt;&lt;P&gt;No matter what we do we cannot see anything on the CAN bus, even when using a sniffer, so apparently, we have missed something fundamental.&lt;/P&gt;&lt;P&gt;The manual states:&lt;/P&gt;&lt;P&gt;“Vehicle control unit CAN (VCU CAN) is the main CAN interface equipped with high-speed TJA1145ATK/FD partial networking transceiver. This transceiver supports CAN partial networking by means of a selective wake-up function. The transceiver inhibit pin is connected to the SBC wake1 signal, which wakes up the system when the wake-up command is received on the VCU CAN port. To configure VCU CAN transceiver, use LPSPI5 PCS2.”&lt;/P&gt;&lt;P&gt;The last sentence is what I do not get, I understand that it is an onboard SPI node (node name: VCU CAN TJA1145A, IC Reference: U20, SPI Instance: LPSPI5, Peripheral chip selects: PCS2, Max Clk Speed: 2.5), but how should it be used and how do I get CAN communication going?&lt;/P&gt;&lt;P&gt;Thanks in advance for your help and guidance!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;JWA74&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="MC33665A" id="MC33665A"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 15 Apr 2024 08:04:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/How-to-enable-CAN-on-MC33665A/m-p/1846904#M3433</guid>
      <dc:creator>JWA74</dc:creator>
      <dc:date>2024-04-15T08:04:23Z</dc:date>
    </item>
    <item>
      <title>Re: How to enable CAN on MC33665A?</title>
      <link>https://community.nxp.com/t5/Power-Management/How-to-enable-CAN-on-MC33665A/m-p/1847882#M3436</link>
      <description>&lt;P&gt;Hi Jimmie,&lt;/P&gt;
&lt;P&gt;Here are some hints:.&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;The DBC files are meant to be used with the CAN-based CMU board directly. We actually have an example with documentation (based on the MC33775) published on the &lt;A href="https://www.nxp.com/products/power-management/battery-management/battery-communication-ics/general-purpose-bms-communication-tpl-transceiver-and-can-fd-gateway:MC33665A" target="_blank"&gt;MC33665 webpage&lt;/A&gt;.&lt;/LI&gt;
&lt;LI&gt;There is a CAN-based example code for the BMU available at:&amp;nbsp;&lt;A href="https://nxp.flexnetoperations.com/control/frse/product?child_plneID=860927" target="_blank"&gt;https://nxp.flexnetoperations.com/control/frse/product?child_plneID=860927&lt;/A&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture.jpg" style="width: 657px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/273963i9FCC6A062D79E94E/image-dimensions/657x229?v=v2" width="657" height="229" role="button" title="Capture.jpg" alt="Capture.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope it helps.&lt;/P&gt;
&lt;P&gt;BR, Tomas&lt;/P&gt;</description>
      <pubDate>Tue, 16 Apr 2024 08:33:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/How-to-enable-CAN-on-MC33665A/m-p/1847882#M3436</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2024-04-16T08:33:38Z</dc:date>
    </item>
  </channel>
</rss>