<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MWCT1000 input power limit configuration in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/MWCT1000-input-power-limit-configuration/m-p/1793153#M3252</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;The MWCT1000 datasheet states the following in section 3.5 Dynamic Input Power Limit:&lt;/P&gt;&lt;P&gt;"When Tx is powered by a limited power supply, such as USB power, WCT1000 can limit the Tx output&lt;BR /&gt;power and provide necessary margin relative to the input power supply capability...&amp;nbsp;The input voltage level for DIPL control can be configured in the WCT1000 example project."&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Question:&amp;nbsp;&lt;/STRONG&gt;Where in the&amp;nbsp;WCT1000_A11_V3.3 example project is the input current limit defined?&lt;/P&gt;&lt;P&gt;I have tried setting&amp;nbsp;IN_CURR_HIGH_TO_LIMIT to 500 and the MWCT1000 is still pulling 2+ amps. Our goal is to limit the input current into the MWCT1000 to 1 amp or less based on our power supply capabilities.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Derek&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 22 Jan 2024 17:39:13 GMT</pubDate>
    <dc:creator>droberson</dc:creator>
    <dc:date>2024-01-22T17:39:13Z</dc:date>
    <item>
      <title>MWCT1000 input power limit configuration</title>
      <link>https://community.nxp.com/t5/Power-Management/MWCT1000-input-power-limit-configuration/m-p/1793153#M3252</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;The MWCT1000 datasheet states the following in section 3.5 Dynamic Input Power Limit:&lt;/P&gt;&lt;P&gt;"When Tx is powered by a limited power supply, such as USB power, WCT1000 can limit the Tx output&lt;BR /&gt;power and provide necessary margin relative to the input power supply capability...&amp;nbsp;The input voltage level for DIPL control can be configured in the WCT1000 example project."&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Question:&amp;nbsp;&lt;/STRONG&gt;Where in the&amp;nbsp;WCT1000_A11_V3.3 example project is the input current limit defined?&lt;/P&gt;&lt;P&gt;I have tried setting&amp;nbsp;IN_CURR_HIGH_TO_LIMIT to 500 and the MWCT1000 is still pulling 2+ amps. Our goal is to limit the input current into the MWCT1000 to 1 amp or less based on our power supply capabilities.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Derek&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Jan 2024 17:39:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/MWCT1000-input-power-limit-configuration/m-p/1793153#M3252</guid>
      <dc:creator>droberson</dc:creator>
      <dc:date>2024-01-22T17:39:13Z</dc:date>
    </item>
    <item>
      <title>Re: MWCT1000 input power limit configuration</title>
      <link>https://community.nxp.com/t5/Power-Management/MWCT1000-input-power-limit-configuration/m-p/1795712#M3266</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;This is wireless charging team reply:&lt;/P&gt;
&lt;P&gt;"&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The Dynamic Input Power limitation function is to stop response to the positive CEP from the PRX, input voltage level will be detected and can be configured by customer.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;But please notice PTX can only guess that power supply reach the limitation, but didn&lt;/SPAN&gt;’&lt;SPAN&gt;t have the ability to limit the input current of power supply, and the receiver still can drive more power.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;"&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Hope it can help you&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;XiangJun Rong&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Jan 2024 02:12:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/MWCT1000-input-power-limit-configuration/m-p/1795712#M3266</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-01-26T02:12:21Z</dc:date>
    </item>
  </channel>
</rss>