<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC33771C balancing 1 cell but other cells are affected in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/MC33771C-balancing-1-cell-but-other-cells-are-affected/m-p/1788405#M3231</link>
    <description>&lt;P&gt;Please read AN12084 Page14 for ----8 Cell balancing&lt;/P&gt;
&lt;P&gt;There is the setting flow chart for reference.&lt;/P&gt;</description>
    <pubDate>Mon, 15 Jan 2024 02:15:02 GMT</pubDate>
    <dc:creator>guoweisun</dc:creator>
    <dc:date>2024-01-15T02:15:02Z</dc:date>
    <item>
      <title>MC33771C balancing 1 cell but other cells are affected</title>
      <link>https://community.nxp.com/t5/Power-Management/MC33771C-balancing-1-cell-but-other-cells-are-affected/m-p/1788209#M3229</link>
      <description>&lt;P&gt;hello,&lt;/P&gt;&lt;P&gt;i'm using the MBDT and the &lt;SPAN class=""&gt;RD33771CDSTEVB&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;+ 33664 TPL evb to balancing a 14 cell string with matlab toolbox. in the program, i choose to enable the balancing on 1 cell (the one at max cell voltage) only but i noticed that other cells voltages are affected as well. i checked the documents it says the balancing would be disabled during sampling in the MBDT default setting so i wonder if this behavior is to do with the internal hw of the MC33771C? or is there other steps that i've missed?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="leonggz_0-1705086952761.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/258053i8C897DE13540220F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="leonggz_0-1705086952761.png" alt="leonggz_0-1705086952761.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 12 Jan 2024 19:19:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/MC33771C-balancing-1-cell-but-other-cells-are-affected/m-p/1788209#M3229</guid>
      <dc:creator>leonggz</dc:creator>
      <dc:date>2024-01-12T19:19:14Z</dc:date>
    </item>
    <item>
      <title>Re: MC33771C balancing 1 cell but other cells are affected</title>
      <link>https://community.nxp.com/t5/Power-Management/MC33771C-balancing-1-cell-but-other-cells-are-affected/m-p/1788405#M3231</link>
      <description>&lt;P&gt;Please read AN12084 Page14 for ----8 Cell balancing&lt;/P&gt;
&lt;P&gt;There is the setting flow chart for reference.&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jan 2024 02:15:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/MC33771C-balancing-1-cell-but-other-cells-are-affected/m-p/1788405#M3231</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2024-01-15T02:15:02Z</dc:date>
    </item>
  </channel>
</rss>