<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックRe: TEA2016 RINGO execute in WINDOWS11</title>
    <link>https://community.nxp.com/t5/Power-Management/TEA2016-RINGO-execute-in-WINDOWS11/m-p/1756976#M3102</link>
    <description>&lt;P&gt;Dear Jeff,&lt;/P&gt;
&lt;P&gt;The Ringo GUI should be compatible with Windows 11.&lt;/P&gt;
&lt;P&gt;Maybe there is an issue with the FTDI-drivers. The latest drivers can be downloaded from:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://ftdichip.com/wp-content/uploads/2021/08/CDM212364_Setup.zip" target="_blank"&gt;https://ftdichip.com/wp-content/uploads/2021/08/CDM212364_Setup.zip&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Tomas&lt;/P&gt;</description>
    <pubDate>Tue, 14 Nov 2023 14:15:38 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2023-11-14T14:15:38Z</dc:date>
    <item>
      <title>TEA2016 RINGO execute in WINDOWS11</title>
      <link>https://community.nxp.com/t5/Power-Management/TEA2016-RINGO-execute-in-WINDOWS11/m-p/1756267#M3100</link>
      <description>&lt;P&gt;Dear Sir:&lt;BR /&gt;HI…I’m Future FAE Jeff Yu and sorry to bother you.&lt;BR /&gt;Our customer reflect he can’t execute any version(v135 or v141) since his computer from WINDOWS 10 upgrade to WINDOW11.&lt;BR /&gt;(Doesn’t connect to USB-I2C Programming kit…offline execute Ringo).&lt;BR /&gt;His others senior colleague which used WINDOWS 10 base or my computer(also as WINDOWS 10) can execute Ringo even off-line.&lt;BR /&gt;Since he upgrade to WINDOWS 11 the will happen “unexpectedly close” during execute RINGO.exe.&lt;BR /&gt;Have you met this situation or others customer feedback this question.&lt;BR /&gt;Should we update driver or NXP have newest RINGO can support WINDOW11?&lt;BR /&gt;If you have any question or suggestion, please kindly advise.&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;Best Regards&lt;BR /&gt;Jeff Yu&lt;/P&gt;</description>
      <pubDate>Mon, 13 Nov 2023 12:19:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/TEA2016-RINGO-execute-in-WINDOWS11/m-p/1756267#M3100</guid>
      <dc:creator>JeffYu-FUTURE</dc:creator>
      <dc:date>2023-11-13T12:19:31Z</dc:date>
    </item>
    <item>
      <title>Re: TEA2016 RINGO execute in WINDOWS11</title>
      <link>https://community.nxp.com/t5/Power-Management/TEA2016-RINGO-execute-in-WINDOWS11/m-p/1756976#M3102</link>
      <description>&lt;P&gt;Dear Jeff,&lt;/P&gt;
&lt;P&gt;The Ringo GUI should be compatible with Windows 11.&lt;/P&gt;
&lt;P&gt;Maybe there is an issue with the FTDI-drivers. The latest drivers can be downloaded from:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://ftdichip.com/wp-content/uploads/2021/08/CDM212364_Setup.zip" target="_blank"&gt;https://ftdichip.com/wp-content/uploads/2021/08/CDM212364_Setup.zip&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Tomas&lt;/P&gt;</description>
      <pubDate>Tue, 14 Nov 2023 14:15:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/TEA2016-RINGO-execute-in-WINDOWS11/m-p/1756976#M3102</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2023-11-14T14:15:38Z</dc:date>
    </item>
    <item>
      <title>Re: TEA2016 RINGO execute in WINDOWS11</title>
      <link>https://community.nxp.com/t5/Power-Management/TEA2016-RINGO-execute-in-WINDOWS11/m-p/1760265#M3121</link>
      <description>&lt;P&gt;Dear Sir:&lt;/P&gt;&lt;P&gt;roger that...very appreciation your kindly help.&lt;/P&gt;&lt;P&gt;we will feedback to customer and try it.&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jeff Yu&lt;/P&gt;</description>
      <pubDate>Tue, 21 Nov 2023 02:39:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/TEA2016-RINGO-execute-in-WINDOWS11/m-p/1760265#M3121</guid>
      <dc:creator>JeffYu-FUTURE</dc:creator>
      <dc:date>2023-11-21T02:39:05Z</dc:date>
    </item>
    <item>
      <title>TEA2016 LLC Half-Bridge Damage  Fails During Use</title>
      <link>https://community.nxp.com/t5/Power-Management/TEA2016-RINGO-execute-in-WINDOWS11/m-p/1995723#M3917</link>
      <description>&lt;P&gt;Hi&amp;nbsp; Sir：&lt;/P&gt;&lt;P&gt;I have a Li-ion battery charger project that uses the TEA2016 . It need to outputs 28V to 42V.&lt;/P&gt;&lt;P&gt;The scenarios that need to be applied are 28V to 41.5V constant 5A current .&lt;/P&gt;&lt;P&gt;when battery is 42V ,It need&amp;nbsp; constant voltage.&lt;/P&gt;&lt;P&gt;At present, 42V constant voltage output, current 0A to 5A adjustable, the test is OK.&lt;/P&gt;&lt;P&gt;But, when the constant current 5A output and the voltage is adjusted from 28V to 41.5V, It happen a&amp;nbsp; question&amp;nbsp; LLC-GANMOS&amp;nbsp; Half bridge damaged .&lt;/P&gt;&lt;P&gt;lower bridge and the half-bridge&amp;nbsp; damaged.&lt;/P&gt;&lt;P&gt;I tested a report that the voltage can be output from 28V to 42V when the current loop is limited to a constant 2A output.&lt;/P&gt;&lt;P&gt;But, TEA2016 will automatically adjust the HP-LP mode, and the resonant current waveform and half-bridge voltage waveform in LP mode are confused.&lt;/P&gt;&lt;P&gt;At present, it is speculated that the 5A output in LP mode will disturb GANMOS-GS.（see pg1）&lt;/P&gt;&lt;P&gt;There is also a case where the current loop limits 5A constant current output, and when the load machine adjusts 7Ω in CR mode, the theoretical output voltage is at this moment: 5A*7Ω=35V. In reality, however, the TEA2016 chip stopped working. （see pg2）&lt;/P&gt;&lt;P&gt;See attachment for pictures of current loop 2A limitation（see pg3-pg6）&lt;/P&gt;&lt;P&gt;SCH see PDF,During the test, in order to avoid the instability of the operation amplifier power supply, 13V is an independent power supply&lt;/P&gt;&lt;P&gt;I have asked for the technical support of the agent, but there is no solution at present. I was hoping you could help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 16 Nov 2024 06:00:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/TEA2016-RINGO-execute-in-WINDOWS11/m-p/1995723#M3917</guid>
      <dc:creator>JuVen</dc:creator>
      <dc:date>2024-11-16T06:00:43Z</dc:date>
    </item>
  </channel>
</rss>