<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックRe: TEA2209T Resistive Load</title>
    <link>https://community.nxp.com/t5/Power-Management/TEA2209T/m-p/1745471#M3038</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;DIV&gt;1. &amp;nbsp; &amp;nbsp;The 4 MOSFETs that still need to be added, should they be 4 n-MOSFETs, or should it be a combination of 2 n-MOSFETs and 2 p-MOSFETs? My intuition tells me that they should all be n-MOSFETs, but why is this the case?&lt;/DIV&gt;
&lt;DIV&gt;&lt;SPAN&gt;4 MOSFETs are n type which has lower Rdson (lower power loss) than p type in general.&lt;/SPAN&gt;&lt;/DIV&gt;
&lt;DIV&gt;&lt;BR /&gt;2. &amp;nbsp; &amp;nbsp;If I use this active full-bridge rectifier with a filter capacitor as indicated in all the figures in the datasheet/demo board files, and if I have a resistive load of around 35 Ohms that serves as a heater (with a relatively large mass, making it slow to respond to changes in power), can this TEA2209T be used without a PFC circuit between it and the load still functioning optimally?&lt;/DIV&gt;
&lt;DIV&gt;&lt;SPAN&gt;For a resistor heater, TEA2209T is not needed + not cost effective. You can tie the resistor directly to the AC line to generate heat, but it’ll varies at different AC line voltages, i.e. at 90Vac, heat/loss=90*90/35=231(W); at 264Vac, heat/loss=264*264/35=1991(W)…&lt;/SPAN&gt;&lt;/DIV&gt;</description>
    <pubDate>Tue, 24 Oct 2023 21:29:58 GMT</pubDate>
    <dc:creator>ErikaC</dc:creator>
    <dc:date>2023-10-24T21:29:58Z</dc:date>
    <item>
      <title>TEA2209T</title>
      <link>https://community.nxp.com/t5/Power-Management/TEA2209T/m-p/1744613#M3035</link>
      <description>&lt;P&gt;posted accidentally in the wrong thread.&lt;/P&gt;&lt;P&gt;please remove it&lt;/P&gt;</description>
      <pubDate>Fri, 27 Oct 2023 07:52:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/TEA2209T/m-p/1744613#M3035</guid>
      <dc:creator>Fornito</dc:creator>
      <dc:date>2023-10-27T07:52:03Z</dc:date>
    </item>
    <item>
      <title>Re: TEA2209T Resistive Load</title>
      <link>https://community.nxp.com/t5/Power-Management/TEA2209T/m-p/1745471#M3038</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;DIV&gt;1. &amp;nbsp; &amp;nbsp;The 4 MOSFETs that still need to be added, should they be 4 n-MOSFETs, or should it be a combination of 2 n-MOSFETs and 2 p-MOSFETs? My intuition tells me that they should all be n-MOSFETs, but why is this the case?&lt;/DIV&gt;
&lt;DIV&gt;&lt;SPAN&gt;4 MOSFETs are n type which has lower Rdson (lower power loss) than p type in general.&lt;/SPAN&gt;&lt;/DIV&gt;
&lt;DIV&gt;&lt;BR /&gt;2. &amp;nbsp; &amp;nbsp;If I use this active full-bridge rectifier with a filter capacitor as indicated in all the figures in the datasheet/demo board files, and if I have a resistive load of around 35 Ohms that serves as a heater (with a relatively large mass, making it slow to respond to changes in power), can this TEA2209T be used without a PFC circuit between it and the load still functioning optimally?&lt;/DIV&gt;
&lt;DIV&gt;&lt;SPAN&gt;For a resistor heater, TEA2209T is not needed + not cost effective. You can tie the resistor directly to the AC line to generate heat, but it’ll varies at different AC line voltages, i.e. at 90Vac, heat/loss=90*90/35=231(W); at 264Vac, heat/loss=264*264/35=1991(W)…&lt;/SPAN&gt;&lt;/DIV&gt;</description>
      <pubDate>Tue, 24 Oct 2023 21:29:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/TEA2209T/m-p/1745471#M3038</guid>
      <dc:creator>ErikaC</dc:creator>
      <dc:date>2023-10-24T21:29:58Z</dc:date>
    </item>
  </channel>
</rss>