<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックRD33771-48VEVM Max Load Current?</title>
    <link>https://community.nxp.com/t5/Power-Management/RD33771-48VEVM-Max-Load-Current/m-p/1716114#M2910</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hello I purchased and am using RD33771-48VEVM. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The load motor we are currently using is of the high current (70-100[A]) class, so I would like to know how far it can be used. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I want to know what the maximum load current is. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;#RD33771&lt;/P&gt;&lt;P&gt;#BMS&lt;/P&gt;</description>
    <pubDate>Mon, 04 Sep 2023 02:10:36 GMT</pubDate>
    <dc:creator>Choist</dc:creator>
    <dc:date>2023-09-04T02:10:36Z</dc:date>
    <item>
      <title>RD33771-48VEVM Max Load Current?</title>
      <link>https://community.nxp.com/t5/Power-Management/RD33771-48VEVM-Max-Load-Current/m-p/1716114#M2910</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello I purchased and am using RD33771-48VEVM. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The load motor we are currently using is of the high current (70-100[A]) class, so I would like to know how far it can be used. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I want to know what the maximum load current is. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;#RD33771&lt;/P&gt;&lt;P&gt;#BMS&lt;/P&gt;</description>
      <pubDate>Mon, 04 Sep 2023 02:10:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/RD33771-48VEVM-Max-Load-Current/m-p/1716114#M2910</guid>
      <dc:creator>Choist</dc:creator>
      <dc:date>2023-09-04T02:10:36Z</dc:date>
    </item>
    <item>
      <title>Re: RD33771-48VEVM Max Load Current?</title>
      <link>https://community.nxp.com/t5/Power-Management/RD33771-48VEVM-Max-Load-Current/m-p/1716269#M2912</link>
      <description>&lt;P&gt;This BMS part use the shunt resistor 100uΩ which can support test&amp;nbsp;−1500 A to&lt;BR /&gt;1500 A (the actual range is in terms of voltage and is given by min and max of VIND) with&lt;BR /&gt;a 6.0 mA resolution.&lt;/P&gt;</description>
      <pubDate>Mon, 04 Sep 2023 07:11:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/RD33771-48VEVM-Max-Load-Current/m-p/1716269#M2912</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2023-09-04T07:11:42Z</dc:date>
    </item>
    <item>
      <title>Re: RD33771-48VEVM Max Load Current?</title>
      <link>https://community.nxp.com/t5/Power-Management/RD33771-48VEVM-Max-Load-Current/m-p/1716355#M2913</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;So, is this model capable of using a motor load of up to +-1500[A]?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I'm afraid the cable might burn out.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 04 Sep 2023 08:37:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/RD33771-48VEVM-Max-Load-Current/m-p/1716355#M2913</guid>
      <dc:creator>Choist</dc:creator>
      <dc:date>2023-09-04T08:37:58Z</dc:date>
    </item>
  </channel>
</rss>