<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power Management中的主题 Single Phase AC Induction Motor Control Reference Design</title>
    <link>https://community.nxp.com/t5/Power-Management/Single-Phase-AC-Induction-Motor-Control-Reference-Design/m-p/1714061#M2904</link>
    <description>&lt;P&gt;Hi to everybody,&lt;/P&gt;&lt;P&gt;I'm using the circuit suggest by the Motorola application note DRM039 (circuit of page 23); everything works fine but during the product certification I found that the 2KV surge disturb destroys the circuit!!&amp;nbsp;&lt;/P&gt;&lt;P&gt;Transil diodes D11 and D18 aren't able to protect the IGBTs. Also a varistor S10K300 at the AC line input is not sufficient to stop the surge transient. I tried to use strong IGBTs (IXYH8N250CHV) without positive results. The load is a 45W fan motor.&lt;/P&gt;&lt;P&gt;Anybody use that circuit? Suggestions to solve my problem?&lt;/P&gt;&lt;P&gt;Thanks a lot.&lt;/P&gt;</description>
    <pubDate>Wed, 30 Aug 2023 14:03:53 GMT</pubDate>
    <dc:creator>Lorenzo_Ziliotto</dc:creator>
    <dc:date>2023-08-30T14:03:53Z</dc:date>
    <item>
      <title>Single Phase AC Induction Motor Control Reference Design</title>
      <link>https://community.nxp.com/t5/Power-Management/Single-Phase-AC-Induction-Motor-Control-Reference-Design/m-p/1714061#M2904</link>
      <description>&lt;P&gt;Hi to everybody,&lt;/P&gt;&lt;P&gt;I'm using the circuit suggest by the Motorola application note DRM039 (circuit of page 23); everything works fine but during the product certification I found that the 2KV surge disturb destroys the circuit!!&amp;nbsp;&lt;/P&gt;&lt;P&gt;Transil diodes D11 and D18 aren't able to protect the IGBTs. Also a varistor S10K300 at the AC line input is not sufficient to stop the surge transient. I tried to use strong IGBTs (IXYH8N250CHV) without positive results. The load is a 45W fan motor.&lt;/P&gt;&lt;P&gt;Anybody use that circuit? Suggestions to solve my problem?&lt;/P&gt;&lt;P&gt;Thanks a lot.&lt;/P&gt;</description>
      <pubDate>Wed, 30 Aug 2023 14:03:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Single-Phase-AC-Induction-Motor-Control-Reference-Design/m-p/1714061#M2904</guid>
      <dc:creator>Lorenzo_Ziliotto</dc:creator>
      <dc:date>2023-08-30T14:03:53Z</dc:date>
    </item>
  </channel>
</rss>